Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is November 24th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Robotics J501 carrier board Hardware and Getting Started​

pir

This document introduces the Robotics J501-Mini carrier board and explains how to flash JetPack OS and use its hardware interfaces, including M.2, Ethernet, USB, LEDs and other I/O ports, with step-by-step instructions and test commands for robotics and edge AI applications.

Getting Started with XIAO Debug Mate​

pir

Seeed Studio XIAO Debug Mate is an open-source ESP32-S3 multi-tool that simplifies embedded system debugging with visual feedback. This all-in-one device features a standalone 2.01 inch TFT LCD display, LED status matrix, and native Seeed Studio XIAO support, delivering essential debugging functions: DAPLink chip-level debugging, built-in serial monitoring with UART passthrough, and accurate power consumption measurement. Plug-and-play design eliminates complex wiring for streamlined development.

pir

This comprehensive guide is designed to help both beginners and advanced users unlock the full potential of their XIAO Debug Mate for professional debugging tasks. Here, you will learn how to connect, configure, and operate the DAPLink debugger, understand essential software tools, and follow best practices to ensure a smooth and productive debugging experience with a wide range of XIAO series development boards. Whether you are troubleshooting complex firmware or streamlining your development workflow, this document provides clear step-by-step instructions, tips, and in-depth technical explanations to support your projects from start to finish.

XIAO Debug Mate Power Meter​

pir

The Power Meter feature of the XIAO Debug Mate transforms your device into a versatile, high-precision tool for measuring voltage, current, and power consumption. With an intuitive graphical interface and real-time data updates, you can easily monitor the power draw of your XIAO board or other connected hardware throughout all stages of development.

XIAO Debug Mate UART Monitor​

pir

This page provides clear guidance on how to use the Debug Mate for serial data monitoring. You will find step-by-step instructions for hardware setup, recommended software tools, and explanations of relevant concepts to help you make the most of the UART monitoring features in development and debugging scenarios.

Getting started for n8n with reCamera​

pir

This tutorial introduces how to push the information recognized by reCamera in text form to n8n, enabling it to serve as the trigger source for the workflow. In this way, users can easily integrate camera detection events into their own automation systems, achieving basic functions such as message alerts, log recording, and third-party service calls, laying the foundation for more complex business logic in the future.

Getting started in Telegram with reCamera​

pir

This tutorial introduces a simple and efficient integration method: the recognition results of reCamera are pushed in text form to n8n, and then n8n automatically sends them to the user-built Telegram personal Bot via API. Through this link, any recognition event can be immediately pushed to the mobile device, thus building a lightweight notification system that spans multiple devices and platforms. The entire process does not require writing complex code; it only requires completing the necessary node configuration to quickly achieve the goal.

Coupling reCamera Home Assistant Enterprise WeChat​

pir

This document explains how to integrate reCamera with Enterprise WeChat using Home Assistant and Node-RED, guiding you through environment setup, webhook and automation configuration, and data flow so that AI detection events from reCamera can trigger real-time alerts in your WeChat workgroup.

AI remote wireless monitoring system based on reCamera and Wifi Halow​

pir

This document shows how to build an AI-powered remote wireless monitoring system using reCamera and Wi-Fi HaLow, including hardware setup, static IP and HaLow configuration, Node-RED workflows, and streaming AI detection results and video to a remote terminal over a long-range, low-power link.

FashionStar Servo Motors Documents Hub​

pir

This document serves as a central hub for FashionStar servo motors, providing quick access to model datasheets, multi-platform SDKs, 3D dimensions, debugging tools, detailed technical documentation, and channels for technical support and product discussion.

Extending the MCP of SenseCAP Watcher with Grove​

pir

This guide explains how to deploy a face-recognition workflow using SenseCAP Watcher (Xiaozhi) together with a reComputer Raspberry Pi system. The Watcher captures images and sends them to the reComputer for face matching against a local database using the internal MCP tool.

HighTorque Motor Control Complete Guide​

This document provides a concise guide to setting up and controlling a high-torque BLDC motor, including hardware wiring, power and CAN configuration, Linux environment setup, and example code in multiple languages to achieve precise speed, position, and torque control.

RobStride Control Library - Complete Technical Documentation​

This document provides a complete technical guide to the RobStride motor control library, covering supported motor models, architecture and CAN protocol details, multi-mode control (MIT, position, speed), environment setup, and example implementations in Python, C++, Rust, and Arduino for real-time, cross-platform motor control.

Quectel RM520N Module for Jetson​

The RM520N is a series of 5G IoT modules specially optimized for IoT/eMBB applications, designed in an M.2 form factor in accordance with the 3GPP Release 16 specification, which supports both 5G NSA and SA modes. The RM520N is compatible with Quectel’s 5G module series RM50xQ, LTE-A Cat 6 module EM06, Cat 12 module series EM12/EM12xR/EM120K, and Cat 16 module EM160R-GL, facilitating migration from LTE-A to 5G.

Existing Wiki Updated​

How to establish communication between Jetson and EtherCAT devices​

We have added the Controlling an EtherCAT Motor on Jetson (MyActuator X4) example.

reComputer R1000 Getting Started​

We have added the Connect to 4G Module by QMI Mode example.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...