Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is December 1st, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Getting Started with XIAO ePaper Display EN04​

pir

Powered by XIAO nRF52840 Plus, the display board EN04 supports both 24-pin and 50-pin ePaper displays. It features a JST 2.0 mm battery connector with power switch, built-in charging IC, NFC function and comes with one reset and three user buttons. Well-suited for low-power ePaper projects such as digital signage, electronic labels, and portable information boards.

SenseCAP T2000 Tracker Introduction​

pir

SenseCAP T2000, an industrial-grade LoRaWAN® asset tracker, supports GNSS, Bluetooth and Wi-Fi positioning for reliable tracking across indoor and outdoor environments. It features IP67 protection, a built-in 3-axis accelerometer that detects the motion status, and an anti-tamper button that triggers a top-priority alarm if the device is removed.

Deploying AI Models on SenseCAP A1102 Using SenseCraft AI​

pir

The SenseCAP A1102 is a powerful sensor device that combines advanced AI capabilities with ease of deployment. This guide will walk you through deployingofficial or custom AI models on the A1102 using the SenseCraft AI website, offering step-by-step instructions for pairing, configuration, and testing.

Play Subway Surfers with body sensor control​

pir

The reCamera is an AI camera equipped with powerful edge computing capabilities. This demo showcases its ability to run the YOLO11n-Pose model in real-time at the device level - without relying on the cloud, it can accurately identify the key points and postures of the human body.

Deploy Facial Recognition on reComputer​

This wiki will guide you through using a reComputer equipped with a Hailo NPU to implement real-time facial recognition. In this project, we use SCRFD-10G for efficient face detection, capable of quickly and accurately detecting faces of various scales, including small faces, ensuring real-time performance.

MCP Integration with External Systems​

pir

This guide demonstrates how to integrate your existing business systems with SenseCAP Watcher through MCP (Model Context Protocol). Unlike the basic calculator example, this tutorial focuses on a industrial use case: voice-controlled warehouse management.

WHEELTEC IMU IMU Sensor Getting Start​

pir

The WHEELTEC H30 is a high-precision attitude sensor designed to accurately measure key data of carriers, including 3D attitude angles, acceleration, angular velocity, and magnetic field strength. Engineered with industrial-grade reliability, this sensor integrates a 3-axis MEMS gyroscope, a 3-axis MEMS accelerometer, and a 3-axis magnetic sensor—delivering robust performance for professional applications.

Stackforce X Series Motors Getting Start​

pir

This article will introduce how to get started with Stackforce series motors and how to use them with C++ and Python on the reComputer Jetson Super.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...