Skip to main content

Weekly Wiki

Greetings

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is January 5th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched

Semtech LR2021 LoRa Plus™ Evaluation Kit

pir

The Semtech LR2021 LoRa Plus Evaluation Kit features a modular design that seamlessly integrates the powerful Seeed Studio XIAO nRF54L15 Core Board with the LoRa Plus Expansion Board. This compact and robust hardware platform is specifically engineered for evaluating full-scenario ground-to-satellite communication. Its compatibility with numerous mainstream IoT protocols ensures it meets development requirements across diverse application scenarios.

YOLOv11 for Speed Estimation and Loitering Detection

This wiki is a comprehensive real-time object detection, tracking, and speed estimation system optimized for Hailo AI accelerators use yolov11. This project enables efficient detection of objects (with focus on persons and vehicles) with simultaneous tracking and speed calculation capabilities.

Pin Multiplexing with Seeed Studio XIAO ESP32-C5

pir

The Seeed Studio XIAO ESP32-C5 is a powerful and versatile development board that features a variety of peripheral interfaces and GPIO pins. These pins can be used for various purposes, such as communicating with other devices, reading analog sensors, controlling LEDs, and more. In this tutorial, we will guide you on how to use the multiplexed pins of the XIAO ESP32-C5.

AI Parking Management Demo with reCamera

pir

This project provides an out-of-the-box demo for parking management scenarios such as commercial parking lots, residential garages, industrial parks, and campuses. It detects the occupancy status of each parking slot from camera views, applies stabilization to reduce visual jitter and short-term fluctuations, automatically summarizes parking availability, and visualizes the results directly on the preview interface for quick verification and demonstration.

Creating a Custom BSP Package from Jetson Development Environment

This wiki guide demonstrates how to clone a complete development environment from an existing Jetson device and create a flashable BSP (Board Support Package) that can be used to replicate the same environment on other Jetson devices. The BSP created using this method enables complete environment cloning when flashed to other Jetson devices. This guide uses JetPack 6.2 as an example.

Existing Wiki Updated

Deploying AI Models on SenseCAP A1102 Using SenseCraft AI

We have added a Custom AI Model Deploying Process.

The Efforts of Contributor

Past Weekly wiki

Click here
Loading Comments...