Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is February 2nd, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Develop reComputer Jetson using Clawdbot​

pir

Traditionally, developing on a Jetson edge device required a physical setup with a monitor, keyboard, and mouse. Even with remote SSH access, developers still depended on terminal-based workflows and additional tools for monitoring and deployment. With Clawdbot, development becomes much simpler. Developers can now interact with the reComputer Jetson directly through a chat app like WhatsApp — sending messages to check device status, run commands, and debug scripts in a more convenient way. This wiki shows how to deploy and use Clawdbot on reComputer Jetson.

Getting Started with reTerminal E1004​

pir

reTerminal E1004 is a 13.3 inch open-source full color ePaper display with up to 3-month battery life. Powered by ESP32-S3, it natively supports our SenseCraft HMI no-code UI platform for effortless dashboard creation, while supporting Home Assistant, Arduino and ESP-IDF for further development. With the E Ink® Spectra™ 6 full-color ePaper Display, it's perfect for digital frame, colorful dashboard visulization.

Deploying Espectre on Seeed Studio XIAO ESP32 Series with ESPHome​

pir

ESPectre is a motion detection system based on Wi-Fi spectre analysis (CSI), with native Home Assistant integration via ESPHome. When someone moves in a room, they "disturb" the Wi-Fi waves traveling between the router and the sensor. It's like when you move your hand in front of a flashlight and see the shadow change. The XIAO ESP32 board "listens" to these changes and understands if there's movement.

YOLOv26 Dual USB Camera Image Processing System on Jetson​

pir

This wiki demonstrates how to build a dual USB camera image processing system based on YOLOv26 model and TensorRT acceleration from scratch.

Seeed Studio XIAO nRF54L15 Sense Zigbee​

pir

This tutorial guides you through implementing Zigbee applications on the Seeed Studio XIAO nRF54L15 development board, this board combines Wi-Fi, Bluetooth Low Energy (BLE), and Zigbee connectivity, making it perfect for IoT applications. The examples in this guide use the NCS to bring Zigbee functionality to life.

AI Human Detection and Meshtastic Notification Demo​

pir

This demo showcases a powerful Edge AI solution integrating the reCamera with a Meshtastic LoRa mesh network. By running a local YOLO11n model, the reCamera identifies humans in real-time and triggers a GPIO signal. This physical signal prompts a XIAO ESP32S3 node to broadcast a "Human detected" alert across the decentralized network. This setup allows for autonomous, off-grid monitoring and security without relying on internet infrastructure. The guide covers hardware assembly for the PoE baseboard, C++ deployment, and Mesh node configuration to bridge AI vision with long-range communication.

Deploy your cloud AI Xiaozhi voice assistant using ESP32S3 + reSpeaker​

pir

reSpeaker XVF3800 is a professional 4-microphone circular array based on the XMOS XVF3800 chip. It provides reliable voice pickup in noisy environments with features including dual modes, 360° far-field pickup (up to 5 m), acoustic echo cancellation (AEC), automatic gain control (AGC), direction of arrival (DoA), dereverberation, beamforming and noise suppression. With its robust capture and denoising abilities, Xiaozhi gets a much better "ear".

Existing Wiki Updated​

Getting Started with XIAO ePaper Display Board - EE02​

We have added an example demonstrating how to operate the EE02 using Arduino.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...