Skip to main content

Weekly Wiki

Greetings

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is March 9th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched

Getting Started with Sound Event Detection Module

pir

A compact edge audio board delivers real-time sound detection with strong local data privacy protection. It detects five abnormal sound events — Baby Cry, Glass Break, Gunshot, T3/T4 Alarms, and Snore, enabling immediate response and reliable early warning. Designed for native ESPHome integration with seamless compatibility for Home Assistant with XIAO series, ideal for home security monitoring or responsive automation triggers.

Get Started with Meshhcore on SenseCAP T1000-E

pir

This wiki explains how to set up and use the SenseCAP T1000-E with MeshCore firmware, including how to flash the firmware via Web Flasher or drag-and-drop, connect the device to the mobile app, and configure LoRa region, GPS, and messaging features. It also covers basic device operation and troubleshooting to help users start communicating over a LoRa mesh network.

Get Started with Meshhcore on Wio Tracker L1 Pro

pir

This wiki explains how to get started with MeshCore or other mesh firmware on the Wio Tracker L1 Pro, including how to flash the firmware using WebUSB or drag-and-drop. It also covers basic setup steps such as configuring the LoRa region, enabling GPS, and sending messages through the mesh network.

Get Started with MeshCore on SenseCAP Solar Node

pir

This wiki explains how to set up and deploy a MeshCore-based SenseCAP Solar Node, including flashing the firmware, activating the device, and connecting it to apps or web tools for configuration. It also covers hardware setup such as installing batteries, mounting the solar node, and configuring LoRa and GPS for outdoor mesh communication.

Setting up an MQTT Gateway with XIAO ESP32S3 & Wio-SX1262 Kit

pir

This wiki explains how to send LoRa data to an MQTT broker using the XIAO ESP32S3 & Wio-SX1262 Kit. It demonstrates how to set up the hardware, configure the firmware, and transmit sensor data through LoRa and publish it to an MQTT server for IoT applications.

Home Assistant and Sound Event Detection Module

pir

A compact edge audio board provides real-time sound detection with strong local data privacy protection. It can detect five abnormal sound events—Baby Cry, Glass Break, Gunshot, T3/T4 alarms, and Snore—enabling immediate response and reliable early warning. In this tutorial, we will learn how to compile and upload the firmware to a XIAO ESP32 board.

Lerobot Dataset Tool

pir

This wiki introduces tools for editing, managing, and visualizing LeRobot datasets. It explains how to remove episodes or features, split or merge datasets, convert image datasets to video format, and preview datasets locally or on Hugging Face.

The Efforts of Contributor

Past Weekly wiki

Click here
Loading Comments...