Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is March 16th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Getting Started with reTerminal D1001​

pir

reTerminal D1001 is an intelligent large-screen interaction terminal powered by Espressif's latest high-performance ESP32-P4 chip. Designed for AIoT application scenarios requiring high-performance graphics display, video processing, and voice interaction, it leverages the ESP32-P4's powerful 400MHz dual-core RISC-V processor and rich multimedia peripheral interfaces to easily handle complex edge computing and multimedia tasks.

Control SO-Arm by OpenClaw on Jetson Thor​

OpenClaw is an AI agent framework that can orchestrate local tools and models. In this project, OpenClaw is used as the high-level control interface, while LeRobot provides the low-level motor communication and calibration utilities for SO-Arm.

Object Detection with YOLOv11 on reComputer-RK​

This project provides industrial-grade, high-performance Computer Vision (CV) application solutions for Rockchip series development boards (RK3588 and RK3576). It features deep integration of the YOLOv11 object detection model, leveraging NPU acceleration for low-latency, high-frame-rate real-time inference.

Existing Wiki Updated​

Get Started with Wio Tracker L1​

We have added an example of the NodeDB Reset operation.

Getting started with SO-ARM100 and SO-ARM101 robotic arm with LeRobot​

We have added a tutorial on Asynchronous Inference in Train And Evaluate.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...