Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is April 13th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Getting Started with XIAO ePaper Display EE05​

pir

Powered by XIAO ESP32-S3 Plus, the display board EE05 is a compact ePaper driver board supporting 24-Pin ePaper displays. It features a JST 2.0 mm battery connector with a power switch, built-in battery level detection circuitry, and comes with one reset button and three user-programmable buttons. Well-suited for low-power ePaper projects such as digital signage, electronic labels, and portable information boards.

Getting Started with XIAO ePaper Display EN05​

pir

Powered by XIAO nRF52840 Plus, the display board EN05 is an ultra-low-power ePaper driver board specifically designed for 24-Pin ePaper displays. With a hardware power switch, it is ideal for battery-powered projects like electronic shelf labels, smart badges, and portable IoT information boards.

reSpeaker Flex with XIAO ESP32S3​

pir

The reSpeaker Flex ESP32 version integrates a pre-soldered XIAO ESP32S3 module on the core board, providing built-in Wi-Fi and Bluetooth connectivity for wireless control and edge processing. Powered by the XMOS XVF3800 voice processor, the system maintains the same modular architecture where the microphone array board connects to the core board through a flexible 24-pin FPC cable, allowing flexible placement inside device enclosures.

reSpeaker Flex control with Python​

In this section, we are going to talk about how to control your reSpeaker Flex using the Python SDK. It makes development more convenient for users who want to build their own applications. For instance, you can detect where the voice is coming from, perform voice activity detection (VAD), control LEDs, and much more.

Existing Wiki Updated​

Meshtastic Firmware Source Code Practical Tutorial​

We have added a new project: Project B – XIAO ESP32S3 Environmental Telemetry Node.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...