Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is June 1st, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Seeed Jetson DevelopTool Overview​

pir

Seeed Jetson DevelopTool is an all-in-one AI development workbench designed for Seeed Studio Jetson products. It consolidates the most common Jetson development workflows — from first-time firmware flashing to AI app deployment — into a single desktop GUI application.

ROS2 Voice Pipeline on reSpeaker XVF3800​

pir

This project turns your voice into TurtleSim control using a reSpeaker XVF3800 microphone array and ROS2. Say “Hey Jarvis” followed by a command, and Jarvis records audio, transcribes it with Groq Whisper, interprets intent with Groq LLaMA, and responds with Groq Orpheus TTS. It is designed for fast setup with Ubuntu and ROS2 Humble, making voice-driven robot experiments easy to run.

ROS2 Voice Pipeline on reSpeaker Flex​

pir

This project turns your voice into TurtleSim control using a reSpeaker Flex microphone array and ROS2. Say “Hey Jarvis” followed by a command, and Jarvis records audio, transcribes it with Groq Whisper, interprets intent with Groq LLaMA, and responds with Groq Orpheus TTS. It is designed for fast setup with Ubuntu and ROS2 Humble, making voice-driven robot experiments easy to run.

Arduino Cookbook: RTC, Low Power, Audio & Touch (reTerminal E Series)​

pir

This document explains how to use Arduino peripheral features on the reTerminal E Series, including RTC setup, low-power mode, PDM microphone recording, and E1003 touch screen examples, with hardware compatibility notes and sample code.

Using Stream Deck to Control reCamera Gimbal​

pir

This wiki demonstrates how to control the reCamera Gimbal using a Stream Deck. By sending commands via the HTTP protocol from the Stream Deck, you can control the reCamera Gimbal to rotate to specific angles, turn the fill light on/off, play audio, and perform other operations.

How to Install Antenna for reComputer Super and Classic​

pir

This guide walks you through installing antennas on the reComputer Super series and the reComputer Classic series. The procedures differ between the two product lines, so please follow the section that matches your device.

reSpeaker Flex with XIAO Feature Updates​

pir

We updated a series of documents for reSpeaker Flex with XIAO, covering audio testing, streaming, and device control features. The new guides include I2S record and playback, UDP/HTTP/MQTT streaming, DoA and VAD examples, and volume control, helping users quickly validate device capabilities and build connected audio applications.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...