Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is June 29th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

reComputer Mini J501 WiFi Module Installation​

pir

In this document, you will learn how to disassemble the reComputer Mini J501 and install or replace a Wi-Fi module (M.2 Key E).

Local Deployment of Picoclaw on reCamera​

pir

We believe many people want to implement their own ideas on reCamera but are unable to do so due to a lack of programming skills. To address these needs, we offer a case of locally deploying Picoclaw on reCamera. With Picoclaw, you can let it write code and debug devices for you—no need to do it yourself. Of course, it can not only help you write code but also directly control the onboard hardware modules. There are more ways to play waiting for you to explore!!

Porting the MediaPipe Hand Gesture Recognition Model to reCamera​

pir

This project demonstrates how to fully port the official Google MediaPipe hand gesture recognition suite onto the reCamera to perform real-time gesture recognition, and to stream the video and recognition results to a PC for visualization via UDP.

Robotics J601 carrier board Hardware Interfaces Usage​

pir

The reComputer Robotics J601 is a high-performance robotics carrier board designed for the NVIDIA Jetson AGX Thor module, targeting advanced embodied AI and robotic control applications. Equipped with extensive connectivity options — including high-speed Ethernet, M.2 slots for 5G and Wi-Fi/BT modules, USB 3.2 ports, 4x CAN (with CAN FD support), RS-232/485, I2C, I2S, UART, GMSL2 expansion (up to 8 cameras), and wide-range DC input — it serves as a powerful robotic brain capable of processing complex data from various sensors.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...