Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is July 6th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

CodeCraft Quick Start & Support​

pir

CodeCraft is an AI programming assistant designed specifically for hardware scenarios. You only need to describe what you want in natural language, and CodeCraft can generate executable hardware programs for you. It is suitable for users who want to quickly complete hardware creation without setting up a development environment from scratch.

Building a Long-Range Security System with reCamera and Meshtastic​

pir

This tutorial provides a highly geeky "network-free security" solution: leverage the powerful edge AI computing power of reCamera PoE for real-time human detection. Once a target is detected, immediately trigger the XIAO ESP32S3 + Wio-SX1262 module (transmitter) via the underlying hardware pins. The alert signal is converted into low-frequency radio waves, traversing kilometers of complex terrain to be captured by the indoor Wio-SX1262 receiver, and seamlessly translated into MQTT messages pushed to your local Home Assistant (HA) system.

Steering Gear Debugging Tool for SO-ARM in Lerobot​

pir

The Steering Gear Debugging Tool (Seeed_RoboController) is a graphical debugging tool for Lerobot/SO-ARM robotic arms. With this tool, you can quickly detect servo status, recalibrate servo IDs, write neutral values, control individual servos, and manage robotic arm calibration files, making it easier to assemble, debug, and maintain the leader and follower arms.

reSpeaker Clip Control with Python​

pir

This document explains how to use Python to control the reSpeaker Clip device, covering connection setup, recording control, file synchronization, and CLI/Web UI usage.

EM12-G GNSS Module Setup Guide for reComputer Robotics J3011​

pir

The EM12-G is a multi-constellation GNSS receiver module designed for positioning applications. It uses a standard M.2 Key B form factor and is compatible with embedded computing platforms such as NVIDIA Jetson and Raspberry Pi. This guide uses the J401 carrier board on reComputer Robotics J3011 as an example to show how to install, power on, and configure the EM12-G GNSS positioning module.

Flash a PREEMPT_RT Linux Real-Time Kernel on Seeed reComputer Jetson with JetPack 6.2.1​

pir

A real-time kernel, also known as a PREEMPT_RT kernel, is a Linux kernel variant with enhanced real-time scheduling capabilities. Its main purpose is to reduce scheduling latency and improve task execution determinism, rather than increase raw computing performance. This guide is based on the official NVIDIA Jetson Linux R36.4.4 BSP. It merges the Seeed R36.4.4 BSP, cross-compiles the PREEMPT_RT kernel, and flashes the system to the NVMe SSD of a Seeed Jetson device.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...