Skip to main content

Weekly Wiki

Greetings​

This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.

✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.

Today is September 7th, and a brand new week has begun! Check out what Seeed Studio did last week!

Latest Wiki Launched​

Wio Tracker L2 Introduction​

Wio Tracker L2

The Wio Tracker L2 Series is a highly extensible Meshtastic® node featuring LoRa (862–930 MHz), the ESP32S3 for efficient processing, and an L76K GPS module for accurate location tracking. Designed for flexibility, it supports QSPI touch screen, E-Ink displays, TF Card, as well as solar panels and battery power, making it ideal for a wide range of IoT and off-grid applications.

More Wio Tracker L2 guides updated this week:

Microduck RL on Jetson​

pir

This demo builds a complete robot-learning workflow for Microduck on a Seeed reComputer powered by NVIDIA Jetson Orin NX 16GB. It covers GPU environment deployment, PPO training with MuJoCo, visualization of local checkpoints, keyboard-controlled inference with official ONNX policies, and the development of new custom motions.

reBot Arm B601-RS Embodied Agent Design Framework​

pir

This tutorial is the operation guide for the wrc_demo project. Follow the steps in this guide to go from zero cloning to a running demo in 1-2 hours. wrc_demo is a visual grasping demo for the reBot Arm B601-RS (RobStride bus), running on Ubuntu 22.04 + Python 3.10 + conda wrc-demo environment. The demo receives natural language instructions (e.g. "pick up the red block"), automatically plans the grasp and executes it.

reSpeaker Clip AI Chat System Architecture​

pir

This document introduces the architecture of the reSpeaker Clip AI chat system, including its core components, workflow, tool calling, and memory mechanism.

Flash the Debian 13 Image to reCamera Pro​

pir

reCamera Pro is powered by the RV1126B chip and is available with 2 GB or 4 GB of memory. It ships with Buildroot firmware for a quick start with AI inference. This page provides a Debian 13 image for users who need more flexibility for development and deployment.

The Efforts of Contributor​

Past Weekly wiki​

Click here
Loading Comments...