Weekly Wiki ✨

Greetings
This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is October 23th and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
Getting Started with Scailable on reComputer J4012 (NVIDIA Jetson Orin NX)
Scailable provides a platform for creating and managing Edge AI solutions at scale. With Scailable, you can simply configure any supported edge device (such as a router, gateway, or IPC) to turn it into a "smart" device. This wiki will walkthrough how you can easily install Scailable AI Manager on the NVIDIA Jetson platform and use Scailable Platform to remotely configure and manage your AI solution at scale.
RS485 Air Temperature, Humidity and Barometric Pressure Sensor(S-THP-01A)
This Wiki describes IP56 RS485 Air Temp, Humi and Barometric pressure sensor. It has a wide operating range of 0-100% RH, -40 to 125°C, and 300-1100 hPa. It is ideal for applications such as smart agriculture, weather monitoring, calculating evapotranspiration, mold prevention and more. By integrating this sensor with the SenseCAP S2100 data logger, users can achieve seamless data collection and management.

E5 Bluetooth Location Beacon for SenseCAP Tracker
A BLE (Bluetooth Low Energy) Location Beacon is a small wireless device that transmits Bluetooth signals at regular intervals. These signals can be detected by Bluetooth-enabled devices, such as SenseCAP T1000 Tracker, allowing them to determine their proximity to the beacon, building a location-based solution for indoor positioning, asset tracking and other applications.
Automatically integrate all your SenseCAP Sensors to Home Assistant
This wiki constitutes the complete step-by-step tutorial for integrating SenseCAP into the Home Assistant platform. Home Assistant has the capability to seamlessly integrate different types of devices from various platforms into a single ecosystem, facilitating cross-platform interoperability. This holds profound significance for the comprehensiveness of the smart home ecosystem.

Existed Wiki Updated
Drivers to support Jetpack 5.1.2 for A603
We have updated the drivers to support Jetpack 5.1.2 for the Jetson Orin NX 8GB/16GB and Jetson Orin Nano 4GB/8GB modules.
Using Wi-Fi technology to enable geolocation for your tracker
We updated the use of Google Geolocation to get location over Wi-Fi.
Hardware Preparation for XIAO IO Expander
This wiki recommand three main ways to use this expansion board
XIAO ESP32C3 and XIAO ESP32S3 Strapping Pins Clarification
These two wikis recommand XIAO ESP32C3 and XIAO ESP32S3 Strapping pins clarification
Flashing methods for reServer Industrial
We have updated flashing methods for reServer Industrial.
More flashing methods for reComputer Industrial
We have updated more flashing methods for reComputer Industrial.
The Efforts of Contributor✨
reRouter Collection Page
Thanks our contributor Kasun Thushara to update the collection page for reRouter under the Contributor Program
Correction for SGP41(raw) measurement dependent on humidity and temperature
Thanks our contributor Hans coming up with a correction concept for SGP41(raw) measurement dependent on humidity and temperature. We are so welcome anyone sharing your thoughts with us!
Speech Recognition based on Edge Impulse using XIAO nRF52840
Thanks our contributor Bruno to make this wiki, using Edge Impulse with the ML capabilities of the Seeed Studio XIAO nRF52840 for Speech Recognition. He will use the Microphone which is already on the XIAO nRF52840 Sense.

EdgeBox 200 Ignition Edge Getting Started
Thanks our contributor Corey to develop the Ignition Edge deploying on EdgeBox 200. This is under the Contributor Program

Past Weekly wiki
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th