Weekly Wiki ✨

Greetings
This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is November 20th and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
Seeed Studio 24GHz mmWave for XIAO
24GHz mmWave Sensor for XIAO - Human Static Presence is a expansion board for Seeed Studio XIAO series. It is an antenna-integrated, high-sensitivity mmwave radar sensor that is based on the FMCW principle. Combined with radar signal processing and accurate human body sensing algorithms, it can identify human bodies in motion and stationary states.

Development of 24GHz mmWave in XIAO and Arduino
This section describes how to use the library and secondary development of mmWave for XIAO.

Object Detection with reTerminal and Pi camera
Object detection on edge computers has become a pivotal field in computer vision, enabling devices to autonomously perceive and respond to their surroundings. EfficientDet, a state-of-the-art object detection model, takes center stage in this domain. Designed to be resource-efficient, it strikes a balance between accuracy and computational demands, making it particularly well-suited for deployment on edge devices with limited processing power. Its ability to identify and locate multiple objects in real-time makes it a key enabler for enhancing the autonomy and intelligence of edge computing systems.

Existed Wiki Updated
SenseCAP T1000 Tracker FAQ - Network Related, Battery Related and Cache Data
We have updated some FAQ in the wiki of SenseCAP T1000 Tracker:
Flash Raspberry Pi OS which is newest version - Bookworm
We have prepared an image with the latest Bookworm OS, the newest release from Raspberry Pi officials. If you encounter any issues, especially those discussed above, we highly recommend following these steps for a smoother experience.

reTerminal - Application of Computer Vision
We'll show the Computer Vision application for reTerminal here.
The Efforts of Contributor✨
Creating XIAO Components on Flux.ai
Thanks our contributor Gokul to create XIAO Components on Flux.ai.
Flux is a browser-based PCB design tool that enables seamless collaboration between electronics teams. The tool's intuitive interface allows users to create schematics and layouts quickly and easily, while its built-in simulation capabilities help to ensure that designs are accurate and error-free.
In this section we are going to cover Creating Seeed Studio XIAO series Components on Flux.ai.
Past Weekly wiki
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th
- weekly wiki on 10.23th
- weekly wiki on 10.30th
- weekly wiki on 11.06th
- weekly wiki on 11.13th