Weekly Wiki

Greetings
This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is February 19th and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
Wio Terminal - FAQ
Currently, we have added a FAQ for Wio-Terminal, where we regularly update questions that come up more often.
Q1: How to avoid the program loss after restarting Wio Terminal multiple times
How to Use Arduino Uno R4 with LoRa Module
This wiki will guide you on how to use the Arduino UNO R4, Grove-Wio-E5, and Grove-Temperature & Humidity Sensor for LoRa communication. This tutorial is designed to provide comprehensive instructions for beginners and intermediate enthusiasts on setting up and implementing wireless communication based on LoRa. It aims to help you master the skills of using Arduino UNO R4 for LoRa communication. Finally, through ChirpStack, we will display the data in Home Assistant.

Grove - Wio-E5 with XIAO-ESP32-S3 via Arduino
The integration of Wio-E5 with XIAO-ESP32-S3 through Arduino presents a robust platform for IoT project development. This guide is designed to assist you in establishing a seamless connection between Wio-E5 and XIAO-ESP32-S3, enabling a wide range of applications and functionalities.

Shape Detection with reTerminal and Pi camera with OpenCV
Shape detection using OpenCV is a computer vision technique that involves identifying and analyzing geometric shapes within images. OpenCV provides a comprehensive set of tools for this task, including contour detection, edge detection, and polygonal approximation. The process typically begins with image preprocessing steps such as grayscale conversion, blurring, and thresholding to enhance shape visibility. The contours extracted from the processed image are then analyzed, and the number of vertices in each contour is used to classify shapes such as circles, triangles, and rectangles. OpenCV's versatility in shape detection makes it a powerful tool for applications ranging from object recognition in robotics to quality control in manufacturing.

Existed Wiki Updated
Grove - Sunlight Sensor
The Grove - Sunlight Sensor has two versions: one is SI1145, and the other is Si1151. We have currently developed Arduino and Raspberry Pi applications for both versions.
Grove Vision AI Module - Resources
We've updated to add the resources for Grove Vision AI
reServer X86 - Pin information
Here, we have listed the pin information for the 8-Pin Power Connector, 28-Pin Arduino Pinout, 9-Pin COM Pinout, 9-Pin USB2.0 Pinout, and 9-Pin Front Panel Pinout in reServer X86 for everyone's reference.
The Efforts of Contributor✨
XIAO ESP32C3 Prism Display
Thanks our contributor Tim to create XIAO ESP32C3 Prism Display.
This project uses the ESP32C3 to create a three-dimensional display using a splitter prism. This guide works to explain the steps required to build the enclosure, attach associated electronics, and install the firmware.

Past Weekly wiki
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th
- weekly wiki on 10.23th
- weekly wiki on 10.30th
- weekly wiki on 11.06th
- weekly wiki on 11.13th
- weekly wiki on 11.20th
- weekly wiki on 11.27th
- weekly wiki on 12.04th
- weekly wiki on 12.11th
- weekly wiki on 12.18th
- weekly wiki on 12.25th
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th