Weekly Wiki✨

Greetings
This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is March 25th and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
Deploying Models from Datasets to Grove Vision AI V2
Welcome to this comprehensive tutorial where we'll embark on a journey to turn your dataset into a fully functional model for deployment on the Grove Vision AI V2. In this guide, we'll navigate through the initial steps of labeling our dataset with Roboflow's intuitive tools, progressing to model training within the collaborative environment of Google Colab.

reTerminal DM - Connect AWS IoT Core with N3uron
We have outlined the process of transmitting data from your reTerminal DM device to AWS IoT Core using the MQTT protocol. This tutorial will seamlessly integrate with the aforementioned process. In this tutorial, we will delve into the intricacies of interfacing between the N3uron Edge IIoT platform and AWS IoT Core.

Seamless Asset Tracking with Amazon Sidewalk and LoRaWAN Networks
Existed Wiki Updated
reTerminal - add adaptation for Bookworm kernel 6.6
we have officially packaged the latest kernel version 6.6.20 into an image package, which includes both 64-bit and 32-bit versions. After conducting thorough testing, by flashing this image, you can resolve the issue of the LCD screen not turning on.
The Efforts of Contributor✨
XIAO ESP32S3(sense) With Zephyr(RTOS)
Thanks our contributor Tim to create XIAO ESP32S3(sense) With Zephyr(RTOS).
The Zephyr OS is based on a small-footprint kernel designed for use on resource-constrained and embedded systems: from simple embedded environmental sensors and LED wearables to sophisticated embedded controllers, smart watches, and IoT wireless applications.
For each supported device Zephyr has a devicetree file that describes the board and its features. The Xiao ESP32S3 Zephyr board page describes the supported features currently available which is defined by the board's dts file.

Past Weekly wiki
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th
- weekly wiki on 10.23th
- weekly wiki on 10.30th
- weekly wiki on 11.06th
- weekly wiki on 11.13th
- weekly wiki on 11.20th
- weekly wiki on 11.27th
- weekly wiki on 12.04th
- weekly wiki on 12.11th
- weekly wiki on 12.18th
- weekly wiki on 12.25th
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th
- weekly wiki on 2024.2.19th
- weekly wiki on 2024.2.26th
- weekly wiki on 2024.3.04th
- weekly wiki on 2024.3.11th
- weekly wiki on 2024.3.18th