Weekly Wiki

Greetings
This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is May 13th and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
reComputer R1000
The reComputer R1000 edge IoT controller is built on the high-performance Raspberry Pi CM4 platform, featuring a quad-core A72 processor with a maximum support of 8GB RAM and 32GB eMMC. Equipped with dual Ethernet interfaces that can be flexibly configured, it also includes 3 isolated RS485 channels supporting BACnet, Modbus RTU, Modbus TCP/IP ,and KNX protocols. With robust IoT network communication capabilities, the R1000 series supports multiple wireless communication options including 4G, LoRa®, Wi-Fi/BLE, allowing for flexible configurations to serve as corresponding wireless gateways. This controller is well-suited for remote device management, energy management, and various other scenarios in the field of smart buildings.
To get you started with the reComputer R1000, we have provided you with the following Wikis:
reComputer R1000 Getting Started

Intelligent IP Camera With AI Function
Grove Vision AI V2 can be advanced surveillance devices that integrate artificial intelligence to enhance security and operational efficiency. These cameras can perform real-time video analysis to detect and alert for unusual activities, recognize faces, and monitor crowd density, making them ideal for applications in areas such as public safety, retail management, and smart home security. By automating surveillance tasks, AI IP cameras reduce the need for constant human monitoring, enabling quicker responses to potential security threats and improving overall safety.

Edge Box RPi 200 - Connect N3uron with MQTT and Modbus Support Devices
In industrial automation, Modbus stands out as one of the most common protocols. MQTT has emerged as the leading protocol for IoT in industrial automation due to many characteristics. Its lightweight design, efficiency, scalability, and support for asynchronous messaging are notable. In MQTT, devices communicate only when there's a reportable event, contrasting with constant update checks. This event-driven approach, coupled with reporting by exception—sending data only when it deviates from norms or on specific triggers—conserves bandwidth and resources, optimizing data transmission for critical IoT applications.
The potent pairing of Edge Box RPi 200 and N3uron Duo facilitates efficient plant management by providing robust connectivity and data manipulation capabilities. This Wiki emphasizes the significance of Modbus TCP in industrial settings, highlighting the seamless integration of MQTT devices to further enhance connectivity.
J401 carrier board Hardware and Interfaces Usage
reComputer J401 carrier board supports NVIDIA Jetson Orin Nano/NX(Orin Nano 4GB/Orin Nano 8GB, Orin NX 8GB/Orin NX 16GB) bringing exceptional performance and being engineered to tackle tough edge computing tasks with ease. It's the perfect choice for developing industrial automation systems, building powerful AI applications, and more.
The Efforts of Contributor
- Check on GitHub for more information.
- We will be really appreciate if you can share your ideas with us!
Past Weekly wiki
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th
- weekly wiki on 10.23th
- weekly wiki on 10.30th
- weekly wiki on 11.06th
- weekly wiki on 11.13th
- weekly wiki on 11.20th
- weekly wiki on 11.27th
- weekly wiki on 12.04th
- weekly wiki on 12.11th
- weekly wiki on 12.18th
- weekly wiki on 12.25th
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th
- weekly wiki on 2024.2.19th
- weekly wiki on 2024.2.26th
- weekly wiki on 2024.3.04th
- weekly wiki on 2024.3.11th
- weekly wiki on 2024.3.18th
- weekly wiki on 2024.3.25th
- weekly wiki on 2024.4.01st
- weekly wiki on 2024.4.08th
- weekly wiki on 2024.4.15th
- weekly wiki on 2024.4.22nd
- weekly wiki on 2024.4.29th
- weekly wiki on 2024.5.06th