Weekly Wiki
![](https://files.seeedstudio.com/wiki/IndexWiki/logo.png)
Greetings
This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is June 3rd and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
[Grove - ADC for Load Cell (HX711)](https://wiki.seeedstudio.com/grove_adc_for_load_cell_hx711 /)
The Grove - ADC for Load Cell (HX711) is a 24-bit A/D converter designed specifically for the load cell. It contains an on-chip low noise programmable amplifier with an optional gain of 32, 64 and 128. The HX711 chip integrates a regulated power supply, an on-chip clock oscillator, and other peripheral circuits, which have the advantages of high integration, fast response, and strong anti-interference.
![](https://files.seeedstudio.com/wiki/Grove-ADC-for-Load-Cell-HX711-/img/Grove-ADC-for-Load-Cell-HX711-wiki.jpg)
Grove Vision AI V2 Notifies You Via Telegram
This project combines the XIAO ESP32S3 and Grove Vision AI V2 to create a compact person detection device. The V2 module, equipped with a person detection model, identifies human presence and sends the results to the ESP32S3. The microcontroller then processes the information and forwards the detection alerts to a designated Telegram account, providing real-time notifications whenever a person is detected in the monitored area.
Quick start with Zigbee on XIAO ESP32C6
In this tutorial, we will embark on a journey to explore Zigbee application development using the XIAO ESP32C6 development board. The XIAO ESP32C6 is a compact yet powerful board that features the ESP32-C6 chip, which offers integrated Wi-Fi and Bluetooth Low Energy (BLE) connectivity. By leveraging the ESP Zigbee SDK, we can harness the full potential of the XIAO ESP32C6 and extend its capabilities to include Zigbee functionality.
![](https://files.seeedstudio.com/wiki/xiaoc6_zigbee/0.png)
The Efforts of Contributor
- Check on GitHub for more information.
- We will be really appreciate if you can share your ideas with us!
Past Weekly wiki
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th
- weekly wiki on 10.23th
- weekly wiki on 10.30th
- weekly wiki on 11.06th
- weekly wiki on 11.13th
- weekly wiki on 11.20th
- weekly wiki on 11.27th
- weekly wiki on 12.04th
- weekly wiki on 12.11th
- weekly wiki on 12.18th
- weekly wiki on 12.25th
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th
- weekly wiki on 2024.2.19th
- weekly wiki on 2024.2.26th
- weekly wiki on 2024.3.04th
- weekly wiki on 2024.3.11th
- weekly wiki on 2024.3.18th
- weekly wiki on 2024.3.25th
- weekly wiki on 2024.4.01st
- weekly wiki on 2024.4.08th
- weekly wiki on 2024.4.15th
- weekly wiki on 2024.4.22nd
- weekly wiki on 2024.4.29th
- weekly wiki on 2024.5.06th
- weekly wiki on 2024.5.13th
- weekly wiki on 2024.5.20th
- weekly wiki on 2024.5.27th