Weekly Wiki

Greetings
This is Seraphina in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is July 8th and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
Watcher to Node-RED Quick Start
Node-RED is a programming tool for wiring together hardware devices, APIs and online services in new and interesting ways.
It provides a browser-based editor that makes it easy to wire together flows using the wide range of nodes in the palette that can be deployed to its runtime in a single-click.

To make it easier for our users to connect data from the Watcher to various other Paas platforms for more in-depth data processing. For example. from Watcher to IFTTT, Telegram, Twilio etc. We will do a series of tutorials for Watcher & Node-RED.
This tutorial, the first in a series, will walk you through installing and using Node-red and calling the Watcher API to connect to Node-RED.
reComputer R1000 Walk Through
The reComputer R1000 edge IoT controller, powered by Raspberry Pi CM4, features a quad-core A72 processor, dual Ethernet, and multiple RS485 channels supporting BACnet, Modbus RTU, and Modbus TCP/IP. With versatile wireless options including 4G, LoRa®, and Wi-Fi/BLE, it ensures robust IoT network communication. Ideal for remote device and energy management, the R1000 is perfect for smart building applications.

reComputer R1000 with Node Red and MQTT
MQTT (Message Queuing Telemetry Transport) is a lightweight messaging protocol ideal for IoT (Internet of Things) applications due to its efficiency and low bandwidth requirements. It facilitates communication between devices in a publish-subscribe model, allowing for real-time data exchange over unreliable networks. With Node-RED, integrating MQTT enables seamless connectivity between edge devices and central servers or other devices, fostering efficient data transmission and processing reComputer R1000 Edge Controller, by supporting MQTT natively, eliminates the need for additional hardware gateways by allowing the installation of an MQTT broker directly on the reComputer R1000 itself. This reduces complexity, minimizes latency, and enhances reliability, as data can be processed and acted upon at the edge without relying on external intermediaries, thus optimizing IoT system architecture.

reCoputer R1000 with Node Red and InfluxDB
Deploying InfluxDB on an reComputer R1000 , a Raspberry Pi-powered edge controller, enables robust time-series data collection and analysis at the edge of your network. This setup is ideal for IoT applications, providing real-time insights and monitoring capabilities. By leveraging the lightweight yet powerful InfluxDB database, you can efficiently manage and analyze sensor data directly on the reComputer R1000. The following guide outlines the steps to install, configure, and use InfluxDB on your reComputer R1000 , ensuring a seamless integration into your data infrastructure.
reComputer R1000 with Grafana
Grafana is an open-source visualization and analytics software that enables you to query, visualize, alert on, and explore your metrics, logs, and traces from any storage location. It offers tools to transform your time-series database (TSDB) data into insightful graphs and visualizations. As a powerful monitoring solution, Grafana helps in making informed decisions, enhancing system performance, and streamlining troubleshooting. In this wiki, we will guide you through the installation of Grafana on a Raspberry Pi-powered reComputer R1000 , connect it to an existing InfluxDB database, and create an illustrative dashboard.

reComputer R1000 with fuxa to achieve SCADA
FUXA is a web-based Process Visualization (SCADA/HMI/Dashboard) software. With FUXA you can create modern process visualizations with individual designs for your machines and real-time data display.It supports Modbus RTU/TCP, Siemens S7 Protocol, OPC-UA, BACnet IP, MQTT, and other protocols.
This article mainly introduces how to use fuxa to achieve SCADA. In the article, fuxa receives data from node-red and OPC UA Simulator, and displays it using chart and Circular Gauge; at the same time, it draws a series of patterns to simulate industrial processes.
SenseCAP Watcher - 1# Concepts and Classification of Tasks
Watcher is a powerful tool that relies on user-issued commands to perform various monitoring and analysis tasks. By sending precise instructions to Watcher, you can direct it to focus on specific targets, collect data, and provide valuable insights.
In the following sections, we will dive into the details of task categorization, model selection, and pricing information. Our goal is to equip you with the knowledge and skills necessary to efficiently assign tasks to Watcher and make the most of its functionalities. We will explore the different types of tasks available, guide you in selecting the appropriate models for your requirements, and provide clarity on the associated costs.

reComputer R1000 install fin
FIN Framework (FIN) is a software framework with application suites that can integrate, control, manage, analyze, visualize and connect. Its capabilities can be integrated by OEMs into a range of products and services.

This article mainly introduces how to install Fin on reComputer R1000.
Finetune with Llama-Factory
🚀Finetune LLM by Llama-Factory on Jetson! Now you can tailor a custom private local LLM to meet your requirements.

Llama-Factory provides a highly convenient large language model fine-tuning tool that supports common large language models, datasets, and fine-tuning methods. With this platform, we can easily customize private large language models.
In this wiki, we will learn how to deploy Llama-Factory on Nvidia Jetson and use Llama-Factory to train a large language model that supports Chinese Q&A.
reComputer R1000 with N3uron
N3uron is a complete Industrial Edge Platform for IIoT & DataOps that enables seamless integration between the industrial plant floor and third-party applications, whether on-premise or in the cloud. With N3uron, you can easily create bidirectional data pipelines between OT and IT systems and decouple devices from applications by consolidating, modeling, processing and visualizing all your operational data in a single source of truth and ultimately making all this data available across the entire organization.

reComputer R1000 use bacnet MS/TP
This article mainly introduces how to perform functional testing of bacnet MS/TP protocol on reComputer R1000.We simulated a bacnet MS/TP server on reComputer R1000, and then used YABE on the W10 PC to check whether the device is present. If the device we simulated can be found normally, it means that the bacnet MS/TP communication is normal.
Existed Wiki Updated
reTerminal && reTerminal DM-FAQ - How to solve screen refresh rate is too low
Screen has noticeable refresh stutter stripes. If your situation is the same, you can follow this wiki to solve it.

recomputer J401 and industrial JetPack 6 Compatibility
We've now updated the method for flashing Jetpack 6 on recomputer J401 and industrial.
Installation to reTerminal DM Lorawan Module
We have updated packages installation to reterminal dm lorawan module.
Using Grove Vision AI V2 with AT Commands - Compatibility of different XIAO
We've added a table of how the Grove Vision AI V2 pairs with the XIAO
The Efforts of Contributor
- Check on GitHub for more information.
- We will be really appreciate if you can share your ideas with us!
Past Weekly wiki
Click here
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th
- weekly wiki on 10.23th
- weekly wiki on 10.30th
- weekly wiki on 11.06th
- weekly wiki on 11.13th
- weekly wiki on 11.20th
- weekly wiki on 11.27th
- weekly wiki on 12.04th
- weekly wiki on 12.11th
- weekly wiki on 12.18th
- weekly wiki on 12.25th
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th
- weekly wiki on 2024.2.19th
- weekly wiki on 2024.2.26th
- weekly wiki on 2024.3.04th
- weekly wiki on 2024.3.11th
- weekly wiki on 2024.3.18th
- weekly wiki on 2024.3.25th
- weekly wiki on 2024.4.01st
- weekly wiki on 2024.4.08th
- weekly wiki on 2024.4.15th
- weekly wiki on 2024.4.22nd
- weekly wiki on 2024.4.29th
- weekly wiki on 2024.5.06th
- weekly wiki on 2024.5.13th
- weekly wiki on 2024.5.20th
- weekly wiki on 2024.5.27th
- weekly wiki on 2024.6.03rd
- weekly wiki on 2024.6.10th
- weekly wiki on 2024.6.17th
- weekly wiki on 2024.6.24th
- weekly wiki on 2024.7.01st