Weekly Wiki

Greetings
This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is July 15th and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
Watcher To IFTTT Quick Start

IFTTT (If This Then That) is a web-based service that allows developers to create automations and integrations between various apps, devices, and services without complex programming. It enables users to define simple conditional statements called "applets" that trigger actions based on specific events. It provides a user-friendly interface and a vast library of pre-built applets, making it accessible for developers to create powerful automations and integrations efficiently.
Watcher To Telegram Quick Start

What is Telegram
Telegram is a popular messaging app that offers a wide range of features for users and developers alike. With its open API and protocol, developers can create custom Telegram clients, bots, and integrate Telegram's services into their own applications. Telegram provides a secure and reliable platform for real-time communication, supporting various media types, group chats, and end-to-end encryption. Its cloud-based infrastructure ensures seamless synchronization across devices and allows for easy scalability. Developers can leverage Telegram's features and tools to build innovative solutions and enhance user experiences within their projects.
AWS IoT Core Intergate With reComputer R1000
AWS IoT Core is a service that assists in securely connecting and managing Internet of Things (IoT) devices. It enables devices to communicate with each other and with the cloud, facilitating the development of smart and connected applications. AWS IoT Core streamlines the integration of IoT devices into the broader AWS ecosystem, offering a reliable and scalable platform for building IoT solutions. In this guide, we will discuss how to connect our reComputer R1000 to the AWS IoT cloud.
reComputer R1000 Connect AWS IoT Core with N3uron
We have outlined the process of transmitting data from your reComputer-R1000 device with AWS IoT Core using the MQTT protocol. This tutorial will seamlessly integrate with the aforementioned process. In this tutorial, we will delve into the intricacies of interfacing between the N3uron Edge IIoT platform and AWS IoT Core.
reComputer R1000 with FIN to use modbus TCP
FIN Framework (FIN) is a software framework with application suites that can integrate, control, manage, analyze, visualize and connect. Its capabilities can be integrated by OEMs into a range of products and services.
This article introduces how to use the Modbus Connector of FIN Framwork, which mainly includes three aspects: creating a FIN Framwork project, configuring the Modbus Connector, and adding data points to Equip.
Existed Wiki Updated
Flash the Sidewalk version to LoRaWAN version
We've added the Application Firmware.
Get Started with SenseCAP Indicator
We have added the RP2040 Datasheet and the ESP32-S3 Datasheet.
The Efforts of Contributor
- Check on GitHub for more information.
- We will be really appreciate if you can share your ideas with us!
Past Weekly wiki
Click here
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th
- weekly wiki on 10.23th
- weekly wiki on 10.30th
- weekly wiki on 11.06th
- weekly wiki on 11.13th
- weekly wiki on 11.20th
- weekly wiki on 11.27th
- weekly wiki on 12.04th
- weekly wiki on 12.11th
- weekly wiki on 12.18th
- weekly wiki on 12.25th
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th
- weekly wiki on 2024.2.19th
- weekly wiki on 2024.2.26th
- weekly wiki on 2024.3.04th
- weekly wiki on 2024.3.11th
- weekly wiki on 2024.3.18th
- weekly wiki on 2024.3.25th
- weekly wiki on 2024.4.01st
- weekly wiki on 2024.4.08th
- weekly wiki on 2024.4.15th
- weekly wiki on 2024.4.22nd
- weekly wiki on 2024.4.29th
- weekly wiki on 2024.5.06th
- weekly wiki on 2024.5.13th
- weekly wiki on 2024.5.20th
- weekly wiki on 2024.5.27th
- weekly wiki on 2024.6.03rd
- weekly wiki on 2024.6.10th
- weekly wiki on 2024.6.17th
- weekly wiki on 2024.6.24th
- weekly wiki on 2024.7.01st
- weekly wiki on 2024.7.08th