Weekly Wiki

Greetings
This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is August 12th and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
reComputer R1000 with Home Assistant

The reComputer r1000, designed for Building Automation Systems, features multiple isolated RS485 channels that support both high and low-speed communication. It is compatible with BACnet, Modbus RTU, and Modbus TCP/IP protocols, making it versatile for various automation needs. This guide provides a concise introduction to installing Home Assistant on the reComputer r1000, enabling seamless integration and control of your smart home devices.
reComputer R1000 and Modbus with Home Assistant
In modern building management systems (BMS), integrating various protocols and devices is crucial for efficient monitoring and control. This guide focuses on leveraging the capabilities of Modbus communication protocols (Modbus TCP and Modbus RTU) with Home Assistant OS, using the powerful reComputer R1000, a Raspberry Pi-powered solution. Whether you're setting up a new system or enhancing an existing one, this guide will walk you through the process of connecting your Modbus devices to Home Assistant, ensuring seamless integration and control.
Use the Raspberry Pi as a NAS (Network-Attached Storage)

The Raspberry Pi is a powerful microcomputer, popular among tech enthusiasts. It can be used for various DIY projects, including setting up a Network Attached Storage (NAS). In this , we will explore the following aspects:
- Is Raspberry Pi good for NAS?
- How to convert Raspberry Pi 5 to NAS?
- Common Issues and Solutions When Using Raspberry Pi as a NAS
Tutorial of AI Kit with Raspberry Pi 5 about YOLOv8n object detection
YOLOv8 (You Only Look Once version 8) is the popular most YOLO series of real-time pose estimation and object detection models. It builds upon the strengths of its predecessors by introducing several advancements in speed, accuracy, and flexibility. The Raspberry-pi-AI-kit is used to accelerate inference speed, featuring a 13 tera-operations per second (TOPS) neural network inference accelerator built around the Hailo-8L chip.
This wiki will guide you on how to use YOLOv8n for object detection with AI Kit on Raspberry Pi 5, from training to deployment.
Seeed Studio XIAO RP2350 with C/C++ SDK
The Pico SDK represents a comprehensive software development kit tailored for the Raspberry Pi RP-family of microcontrollers, with a particular focus on the XIAO RP2350 board. This SDK incorporates a wide range of libraries and tools designed to facilitate the development of advanced applications, serving both novice enthusiasts and experienced professionals. The SDK functions as a foundational platform for exploiting the extensive capabilities of the RP2350 microcontroller across various projects.
Seeed Studio XIAO RP2350 with MicroPython
Welcome to the guide on using MicroPython with the Seeed Studio XIAO RP2350! This guide will help you get started with setting up MicroPython, writing and running your first script, and exploring the capabilities of the XIAO RP2350 using the Thonny IDE.
Existed Wiki Updated
Flash JetPack OS to A608 Carrier Board (NVIDIA Jetson Orin NX/Nano supported)
We have added an example of installing JetPack 6.0 on an A608 carrier board with a Jetson Orin NX module using NVIDIA L4T 36.3.
The Efforts of Contributor
- Check on GitHub for more information.
- We will be really appreciate if you can share your ideas with us!
Past Weekly wiki
Click here
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th
- weekly wiki on 10.23th
- weekly wiki on 10.30th
- weekly wiki on 11.06th
- weekly wiki on 11.13th
- weekly wiki on 11.20th
- weekly wiki on 11.27th
- weekly wiki on 12.04th
- weekly wiki on 12.11th
- weekly wiki on 12.18th
- weekly wiki on 12.25th
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th
- weekly wiki on 2024.2.19th
- weekly wiki on 2024.2.26th
- weekly wiki on 2024.3.04th
- weekly wiki on 2024.3.11th
- weekly wiki on 2024.3.18th
- weekly wiki on 2024.3.25th
- weekly wiki on 2024.4.01st
- weekly wiki on 2024.4.08th
- weekly wiki on 2024.4.15th
- weekly wiki on 2024.4.22nd
- weekly wiki on 2024.4.29th
- weekly wiki on 2024.5.06th
- weekly wiki on 2024.5.13th
- weekly wiki on 2024.5.20th
- weekly wiki on 2024.5.27th
- weekly wiki on 2024.6.03rd
- weekly wiki on 2024.6.10th
- weekly wiki on 2024.6.17th
- weekly wiki on 2024.6.24th
- weekly wiki on 2024.7.01st
- weekly wiki on 2024.7.08th
- weekly wiki on 2024.7.16th
- weekly wiki on 2024.7.22th
- weekly wiki on 2024.7.29th
- weekly wiki on 2024.8.05th