Weekly Wiki

Greetings
This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is October 14th, and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
Clip Application on Raspberry Pi with AI Kit
CLIP(Contrastive Language-Image Pre-Training) is a neural network trained on a variety of (image, text) pairs. It can be instructed in natural language to predict the most relevant text snippet, given an image, without directly optimizing for the task, similarly to the zero-shot capabilities of GPT-2 and 3. We found CLIP matches the performance of the original ResNet50 on ImageNet “zero-shot” without using any of the original 1.28M labeled examples, overcoming several major challenges in computer vision.
This wiki will teach you how to deploy the clip application on a Raspberry Pi5 or Recomputer r1000, clip will inference on AI kit.
reCamera Getting Started
reCamera is a combination of a processor and a camera sensor.

This combination makes reCamera a standalone system that can handle basic detection and control tasks on its own.
How to install CODESYS for reComputer R1000

CODESYS is a popular automation software development platform widely used in industrial control and automation systems. Its full name is Controller Development System, which was first developed by the German company 3S-Smart Software Solutions. This article mainly introduces how to download and install CODESYS, and finally deploy the CODESYS project to reComputer R1000
How to use CODESYS to configure the Modbus rtu function of R1000

This article mainly introduces how to use the modbus rtu function of reComputer R1000 based on CODESYS. We will use the two rs485 ports of reComputer R1000, one port is used for Modbus master and the other port is used for Modbus slave. This article will detail how to configure Modbus master and Modbus slave on CODESYS and show how to deploy them on reComputer R1000.
Training Model for Watcher

This WiKi article will teach you how to use our SenseCraft to train your own AI model and deploy it on our Watcher. It will be a very interesting process. If you still don't know what SenseCraft is, please click here. This is a platform that allows us to deploy various open-source AI models on Seeed Studio devices.
Wio-SX1262 Introduction

The Wio-SX1262 is a low-cost, ultra-low-power, and ultra-compact LoRa® Pure RF module based on the high-performance Semtech SX1262 LoRa® wireless communication IC, supporting LoRa & LoRaWAN frequency from 868 to 915 MHz and up tp +22 dBm highly efficient transmitted power. Equipped with an onboard IPEX antenna connector and high-quality oscillator of the TCXO(Temperature Compensate Crystal Oscillator), it ensures stable operation at the high and low temperature environment of industry. It is designed for wireless sensor networks and other IoT devices, especially those requiring battery-powered, low-power consumption, and long-range connectivity. Ideal for applications such as wireless meter reading, agriculture sensor, LoRaWAN single channel gateway etc.
Wio-SX1262 with XIAO ESP32S3 Kit Introduction

This thumb-sized LoRa development kit, which consists of the XIAO ESP32S3 and the Wio-SX1262 LoRa module, is an ideal starter kit for Meshtastic and LoRa/LoRaWAN projects. Supporting WiFi, BLE, and LoRa, it includes a built-in power management chip and can be extended via IIC, UART, and other GPIO interfaces, and is compatible with Arduino development. The XIAO ESP32S3 with Wio-SX1262 is a single-channel LoRaWAN LoRa module with a low price and high cost performance. It is suitable for application scenarios with long distance, low power consumption, and small data volume. It supports more than 30 node devices (depending on upload interval, data payload, etc.).
Get Started for Meshtastic

Meshtastic is an open source, off-grid, decentralized, mesh network built to run on affordable, low-power devices. Seeed Studio provides a comprehensive range of ready-to-go Meshtastic devices for hobbyists and industrial users. Wio-SX1262 with XIAO ESP32S3 kit is flexible solution for meshtastic developer and maker.
How to Use Orbbec Depth Cameras on reComputer with ROS

This tutorial provides a step-by-step guide on how to use Orbbec Depth Camera through ROS on reComputer J30/J40 series devices. We will take Orbbec Gemini 2 as an example, obtain topic data of depth images and point clouds, and visualize them on rviz.
Getting Started ThingsBoard With reComputer R1000
ThingsBoard is an open-source IoT platform designed for rapid development, management, and scaling of IoT projects. It offers an out-of-the-box solution for both cloud and on-premises IoT infrastructure, enabling you to provision devices, manage assets, collect and visualize data, and analyze telemetry with ease. In this guide, we will walk through the installation of ThingsBoard Community Edition on a reComputer, providing a robust foundation for your IoT applications.
Existing Wiki Updated
Watcher to Node-RED Quick Start
We provide a method for Watcher to send messages to Node-RED using the HTTP protocol.
Usage of Seeed Studio XIAO ESP32S3 microphone
We provide an example of saving recorded sound to a microSD card in the ESP32 version 3.0.x.
The Efforts of Contributor
- Check on GitHub for more information.
- We will be really appreciate if you can share your ideas with us!
Past Weekly wiki
Click here
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th
- weekly wiki on 10.23th
- weekly wiki on 10.30th
- weekly wiki on 11.06th
- weekly wiki on 11.13th
- weekly wiki on 11.20th
- weekly wiki on 11.27th
- weekly wiki on 12.04th
- weekly wiki on 12.11th
- weekly wiki on 12.18th
- weekly wiki on 12.25th
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th
- weekly wiki on 2024.2.19th
- weekly wiki on 2024.2.26th
- weekly wiki on 2024.3.04th
- weekly wiki on 2024.3.11th
- weekly wiki on 2024.3.18th
- weekly wiki on 2024.3.25th
- weekly wiki on 2024.4.01st
- weekly wiki on 2024.4.08th
- weekly wiki on 2024.4.15th
- weekly wiki on 2024.4.22nd
- weekly wiki on 2024.4.29th
- weekly wiki on 2024.5.06th
- weekly wiki on 2024.5.13th
- weekly wiki on 2024.5.20th
- weekly wiki on 2024.5.27th
- weekly wiki on 2024.6.03rd
- weekly wiki on 2024.6.10th
- weekly wiki on 2024.6.17th
- weekly wiki on 2024.6.24th
- weekly wiki on 2024.7.01st
- weekly wiki on 2024.7.08th
- weekly wiki on 2024.7.16th
- weekly wiki on 2024.7.22th
- weekly wiki on 2024.7.29th
- weekly wiki on 2024.8.05th
- weekly wiki on 2024.8.12th
- weekly wiki on 2024.8.19th
- weekly wiki on 2024.8.26th
- weekly wiki on 2024.9.02nd
- weekly wiki on 2024.9.09th
- weekly wiki on 2024.9.16th
- weekly wiki on 2024.9.23th
- weekly wiki on 2024.9.30th
- weekly wiki on 2024.10.07th