Weekly Wiki

Greetings
This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is October 21th, and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
Enclosure Installation Guide with ReSpeaker Lite
This wiki will provide you with a detailed, easy-to-follow guide for enclosure installation, helping you safely assemble the ReSpeaker Lite voice kit setup.
SenseCAP Watcher Quick Start Guide
SenseCAP Watcher is an AI watcher to help you monitor anomalies within a space and then take actions. Simply speak to Watcher to give commands, and it will execute your desired tasks when the event occurs.

As a new comer for smart building / smart home system, SenseCAP Watcher is far more intelligent compared to current sensors and actuators. It understands what is happening within the space and then takes actions accordingly.
Hardware components of the SenseCAP Watcher

In this section of the Wiki, we will focus on the hardware components of the SenseCAP Watcher, its construction and the use of additional accessories.
Operation guideline of the SenseCAP Watcher
Inside this section of the Wiki, we will provide you with information on the SenseCAP Watcher's operating logic, tasking, and the use of the device's features.
Connect to Chirpstack with Wio-SX1262 with XIAO ESP32S3 Kit
LoRaWAN is a low-power, wide-area networking protocol built on top of the LoRa technique. It wirelessly connects devices to the internet and manages communication between end-node devices and network gateways. Followed the Get Started for Lora, we configured Wio-SX1262 with XIAO ESP32S3 as one channel hub lora gateway.

This wiki page explains how set up LoraWAN based on Wio-SX1262 with XIAO ESP32S3 kit as single channel gateway exchange data. And also connect the Sensecap S210x lora sensor node to Wio-SX1262 with XIAO ESP32S3 kit and transmit the sensor data to Chirpstack.
Connect to TTN with Wio-SX1262 with XIAO ESP32S3 Kit
LoRaWAN is a low-power, wide-area networking protocol built on top of the LoRa technique. It wirelessly connects devices to the internet and manages communication between end-node devices and network gateways. Followed the Get Started for Lora, we configured Wio-SX1262 with XIAO ESP32S3 as one channel hub lora gateway.

This wiki page explains how set up LoraWAN based on Wio-SX1262 with XIAO ESP32S3 kit as single channel gateway exchange data with TTN. And also connect the Sensecap S210x lora sensor node to Wio-SX1262 with XIAO ESP32S3 kit and transmit the sensor data to TTN(The Things Network).
Lorawan Based on Wio SX1262 with XIAO ESP32S3 Module
The XIAO ESP32S3 as host MCU and Wio SX1262 LoRa radio kit can be configured to function as single channel gateway for connecting to The Things Network. This kit offers a practical solution for those interested in delving into LoRa technology and establishing connections to LNS(lora network server).
Existing Wiki Updated
Wio-SX1262 Introduction
We provide a link for Wio SX1262 symbol and package file.
The Efforts of Contributor
- Check on GitHub for more information.
- We will be really appreciate if you can share your ideas with us!
Past Weekly wiki
Click here
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.21st
- weekly wiki on 8.28th
- weekly wiki on 9.11st
- weekly wiki on 9.18th
- weekly wiki on 9.25th
- weekly wiki on 10.9th
- weekly wiki on 10.16th
- weekly wiki on 10.23th
- weekly wiki on 10.30th
- weekly wiki on 11.06th
- weekly wiki on 11.13th
- weekly wiki on 11.20th
- weekly wiki on 11.27th
- weekly wiki on 12.04th
- weekly wiki on 12.11th
- weekly wiki on 12.18th
- weekly wiki on 12.25th
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th
- weekly wiki on 2024.2.19th
- weekly wiki on 2024.2.26th
- weekly wiki on 2024.3.04th
- weekly wiki on 2024.3.11th
- weekly wiki on 2024.3.18th
- weekly wiki on 2024.3.25th
- weekly wiki on 2024.4.01st
- weekly wiki on 2024.4.08th
- weekly wiki on 2024.4.15th
- weekly wiki on 2024.4.22nd
- weekly wiki on 2024.4.29th
- weekly wiki on 2024.5.06th
- weekly wiki on 2024.5.13th
- weekly wiki on 2024.5.20th
- weekly wiki on 2024.5.27th
- weekly wiki on 2024.6.03rd
- weekly wiki on 2024.6.10th
- weekly wiki on 2024.6.17th
- weekly wiki on 2024.6.24th
- weekly wiki on 2024.7.01st
- weekly wiki on 2024.7.08th
- weekly wiki on 2024.7.16th
- weekly wiki on 2024.7.22th
- weekly wiki on 2024.7.29th
- weekly wiki on 2024.8.05th
- weekly wiki on 2024.8.12th
- weekly wiki on 2024.8.19th
- weekly wiki on 2024.8.26th
- weekly wiki on 2024.9.02nd
- weekly wiki on 2024.9.09th
- weekly wiki on 2024.9.16th
- weekly wiki on 2024.9.23th
- weekly wiki on 2024.9.30th
- weekly wiki on 2024.10.07th
- weekly wiki on 2024.10.14th