Weekly Wiki

Greetings
This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is March 31th, and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
ePaper Panel in Home Assistant
The XIAO ESP32C3-powered 7.5-inch E-Ink Display is a compact, energy-efficient solution for showcasing Home Assistant data. With seamless integration and crisp visuals, it's perfect for smart homes. Also compatible with Arduino for easy customization, it offers low power consumption and excellent readability in any light. Simplify your smart home setup with this versatile display.
ePaper Panel in Arduino

The 7.5 inch E-Ink display is a game-changer for Arduino users. It seamlessly integrates with Arduino, allowing you to easily showcase various data. With simple wiring and straightforward code, even beginners can get started quickly. It offers low power consumption and excellent readability in any light. Let's unlock endless creative projects with this accessible and versatile display ~
Distributed Inference of DeepSeek model on Raspberry Pi

This wiki explains how to deploy the DeepSeek model on Multiple Raspberry Pi AI Boxs with distributed-llama.In this wiki, I used a Raspberry Pi with 8GB of RAM as the root node and three Raspberry Pis with 4GB of RAM** as worker nodes to run the DeepSeek 8B model. The inference speed reached 6.06 tokens per second.
Flash JetPack to J401-Mini Carrier Board

This article explains how to flash JetPack 6.0 on the J401-Mini Carrier Board, covering device overview, preparation, entering Force Recovery mode, and using a one-click script for flashing, helping users quickly deploy NVIDIA Jetson Orin devices.
reCamera Gimbal Overview

This wiki introduces the features, specifications, hardware interface, and part list of the Recamera Gimbal.
Existing Wiki Updated
Flash JetPack OS to A608 Carrier Board (NVIDIA Jetson Orin NX/Nano supported)
We have added the CAD file resources for A608.
The Efforts of Contributor
Seeed Studio XIAO RA4M1 with NuttX(RTOS)
This wiki introduces setting up NuttX RTOS on the Seeed Studio XIAO RA4M1 board. NuttX is a lightweight, scalable real-time operating system known for its small footprint and broad hardware support. The guide walks through installing necessary tools, configuring the board, building the system, and flashing firmware. It includes examples for using NuttShell (NSH), USBNSH, and JUMBO applications, with a focus on practical tasks like GPIO and LED control.
T1000-E Arduino Examples
This wiki provides Arduino examples for the T1000-E Tracker, covering basic GPIO control, sensor data reading, GNSS positioning, and LoRaWAN communication, along with setup and upload instructions.
- Check on GitHub for more information.
- We will be really appreciate if you can share your ideas with us!
Past Weekly wiki
Click here
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th
- weekly wiki on 2024.2.19th
- weekly wiki on 2024.2.26th
- weekly wiki on 2024.3.04th
- weekly wiki on 2024.3.11th
- weekly wiki on 2024.3.18th
- weekly wiki on 2024.3.25th
- weekly wiki on 2024.4.01st
- weekly wiki on 2024.4.08th
- weekly wiki on 2024.4.15th
- weekly wiki on 2024.4.22nd
- weekly wiki on 2024.4.29th
- weekly wiki on 2024.5.06th
- weekly wiki on 2024.5.13th
- weekly wiki on 2024.5.20th
- weekly wiki on 2024.5.27th
- weekly wiki on 2024.6.03rd
- weekly wiki on 2024.6.10th
- weekly wiki on 2024.6.17th
- weekly wiki on 2024.6.24th
- weekly wiki on 2024.7.01st
- weekly wiki on 2024.7.08th
- weekly wiki on 2024.7.16th
- weekly wiki on 2024.7.22th
- weekly wiki on 2024.7.29th
- weekly wiki on 2024.8.05th
- weekly wiki on 2024.8.12th
- weekly wiki on 2024.8.19th
- weekly wiki on 2024.8.26th
- weekly wiki on 2024.9.02nd
- weekly wiki on 2024.9.09th
- weekly wiki on 2024.9.16th
- weekly wiki on 2024.9.23th
- weekly wiki on 2024.9.30th
- weekly wiki on 2024.10.07th
- weekly wiki on 2024.10.14th
- weekly wiki on 2024.10.21th
- weekly wiki on 2024.10.28th
- weekly wiki on 2024.11.04th
- weekly wiki on 2024.11.11th
- weekly wiki on 2024.11.18th
- weekly wiki on 2024.11.25th
- weekly wiki on 2024.12.02nd
- weekly wiki on 2024.12.09th
- weekly wiki on 2024.12.16th
- weekly wiki on 2024.12.23th
- weekly wiki on 2024.12.30th
- weekly wiki on 2025.1.06th
- weekly wiki on 2025.1.13th
- weekly wiki on 2025.1.20th
- weekly wiki on 2025.1.27th
- weekly wiki on 2025.2.10th
- weekly wiki on 2025.2.17th
- weekly wiki on 2025.2.24th
- weekly wiki on 2025.3.03rd
- weekly wiki on 2025.3.10th
- weekly wiki on 2025.3.17th
- weekly wiki on 2025.3.24th