Weekly Wiki

Greetings
This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is April 14th, and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
XIAO RP2040 with PlatformIO

PlatformIO is a development platform that integrates many types of development boards and has good scalability. If the platform does not have the type you need, you can manually add the type of development board yourself. The code you write on Arduino can use it, just add the corresponding library.
In this wiki, we will introduce how to install PlatformIO for the XIAO RP2040 and run the sample code. In addition, we have also updated the tutorials for the XIAO RA4M1, XIAO RP2350, and XIAO SAMD21.
Getting started with XIAO 2-Channel Wi-Fi AC Energy Meter In Home Assistant

The XIAO 2-Channel Wi-Fi AC Energy Meter is a smart device from Seeed Studio designed to detect the electricity usage of AC-powered appliances. Its dual-channel configuration supports independent detect of up to two loads, making it an excellent choice for automating a variety of devices in smart home environments. This guide provides a detailed walkthrough, including setup, integration, and advanced configuration for users ranging from beginners to smart-home enthusiasts.
Getting Started with Seeed Studio IoT Button

The IoT Button is a versatile smart switch offering dual Home Assistant integrations through ESPHome and Zigbee. Powered by ESP32-C6, it features customizable RGB LED indicators, programmable event triggers, USB-C charging, and flexible mounting options - everything you need for intuitive smart home control.
Existing Wiki Updated
Getting Started with ODYSSEY – STM32MP135D
We have provided a precompiled package for the ODYSSEY STM32MP135D.
Voice Assistant System for Home Assitant
We have updated the .yaml example for adding the XIAO ESP32S3 to ESPHome.
ePaper Panel in Home Assistant
We have added an example of displaying a screenshot of Home Assistant.
The Efforts of Contributor
Seeed Studio XIAO ESP32S3 with NuttX(RTOS)
This wiki introduces setting up NuttX RTOS on the Seeed Studio XIAO ESP32S3 board. NuttX is a lightweight, scalable real-time operating system known for its small footprint and broad hardware support. The guide walks through installing necessary tools, configuring the board, building the system, and flashing firmware. It includes examples for using NuttShell (NSH), USBNSH, and JUMBO applications, with a focus on practical tasks like GPIO and LED control.
- Check on GitHub for more information.
- We will be really appreciate if you can share your ideas with us!
Past Weekly wiki
Click here
- weekly wiki on 2024.1.08th
- weekly wiki on 2024.1.15th
- weekly wiki on 2024.1.22nd
- weekly wiki on 2024.1.29th
- weekly wiki on 2024.2.19th
- weekly wiki on 2024.2.26th
- weekly wiki on 2024.3.04th
- weekly wiki on 2024.3.11th
- weekly wiki on 2024.3.18th
- weekly wiki on 2024.3.25th
- weekly wiki on 2024.4.01st
- weekly wiki on 2024.4.08th
- weekly wiki on 2024.4.15th
- weekly wiki on 2024.4.22nd
- weekly wiki on 2024.4.29th
- weekly wiki on 2024.5.06th
- weekly wiki on 2024.5.13th
- weekly wiki on 2024.5.20th
- weekly wiki on 2024.5.27th
- weekly wiki on 2024.6.03rd
- weekly wiki on 2024.6.10th
- weekly wiki on 2024.6.17th
- weekly wiki on 2024.6.24th
- weekly wiki on 2024.7.01st
- weekly wiki on 2024.7.08th
- weekly wiki on 2024.7.16th
- weekly wiki on 2024.7.22th
- weekly wiki on 2024.7.29th
- weekly wiki on 2024.8.05th
- weekly wiki on 2024.8.12th
- weekly wiki on 2024.8.19th
- weekly wiki on 2024.8.26th
- weekly wiki on 2024.9.02nd
- weekly wiki on 2024.9.09th
- weekly wiki on 2024.9.16th
- weekly wiki on 2024.9.23th
- weekly wiki on 2024.9.30th
- weekly wiki on 2024.10.07th
- weekly wiki on 2024.10.14th
- weekly wiki on 2024.10.21th
- weekly wiki on 2024.10.28th
- weekly wiki on 2024.11.04th
- weekly wiki on 2024.11.11th
- weekly wiki on 2024.11.18th
- weekly wiki on 2024.11.25th
- weekly wiki on 2024.12.02nd
- weekly wiki on 2024.12.09th
- weekly wiki on 2024.12.16th
- weekly wiki on 2024.12.23th
- weekly wiki on 2024.12.30th
- weekly wiki on 2025.1.06th
- weekly wiki on 2025.1.13th
- weekly wiki on 2025.1.20th
- weekly wiki on 2025.1.27th
- weekly wiki on 2025.2.10th
- weekly wiki on 2025.2.17th
- weekly wiki on 2025.2.24th
- weekly wiki on 2025.3.03rd
- weekly wiki on 2025.3.10th
- weekly wiki on 2025.3.17th
- weekly wiki on 2025.3.24th
- weekly wiki on 2025.3.31th
- weekly wiki on 2025.4.07th