Weekly Wiki

Greetings
This is Frank in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is June 23rd, and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
Connect SenseCAP S210X to Datacake via TTN

This guide walks you through how to connect the SenseCAP S210X LoRaWAN® sensors to Datacake via The Things Network (TTN). It covers everything from setting up your Datacake account and adding your device to TTN, to configuring webhooks, generating API tokens, and setting up downlinks and payload decoders. Perfect for anyone looking to integrate SenseCAP sensors into a low-code IoT platform.
Get Started with Wio Tracker L1
![]()
This guide shows you how to get started with the Meshtastic-enabled Wio Tracker L1. It walks you through flashing the latest firmware using the Meshtastic Web Flasher, entering DFU mode, setting up the device over USB, and connecting via Bluetooth (iOS/Android apps). It also explains how to configure the correct LoRa region to begin mesh communication.
HEXFELLOW Y200 IMU Sensor Getting Start

The Y200 is a 9-axis gyroscope specifically developed for robots. The device supports a maximum power supply of 60V and uses a standard XT30 CAN interface for quick integration into a robot network. It features an internal potting process for excellent shock resistance, and its casing is designed with a reinforced structure for stable and reliable installation.
AI-Powered Control of the Robotic Arm via GR00T

This article demonstrates how NVIDIA's GR00T AI platform enables advanced, autonomous control of StarAI Robotic Arm. Combining real-time perception and adaptive decision-making, GR00T bridges AI and robotics for precision tasks in industrial and research applications.
Real-time OCR with reComputer AI box

OCR, or Optical Character Recognition, can be applied to various scenarios such as sign recognition and invoice processing. In this project, the PGNet model is deployed on the reComputer R2000 or reComputer R2000 produced by Seeed Studio to enable accelerated and real-time OCR detection.
Frigate NVR and Hailo on reComputer R2000 connect with Home Assistant

In this guide, we'll walk you through how to install Frigate on a reComputer AI box equipped with Hailo PCIe, and how to connect it to your existing Home Assistant setup using MQTT with minimal hassle.
Existing Wiki Updated
Get Started with SenseCAP Solar Node
We added an example of the Flash Firmware operation.
Getting Started with reComputer Super
We added an example of the Flash JetPack OS operation.
The Efforts of Contributor
- Check on GitHub for more information.
- We will be really appreciate if you can share your ideas with us!
Past Weekly wiki
Click here
- weekly wiki on 2024.4.01st
- weekly wiki on 2024.4.08th
- weekly wiki on 2024.4.15th
- weekly wiki on 2024.4.22nd
- weekly wiki on 2024.4.29th
- weekly wiki on 2024.5.06th
- weekly wiki on 2024.5.13th
- weekly wiki on 2024.5.20th
- weekly wiki on 2024.5.27th
- weekly wiki on 2024.6.03rd
- weekly wiki on 2024.6.10th
- weekly wiki on 2024.6.17th
- weekly wiki on 2024.6.24th
- weekly wiki on 2024.7.01st
- weekly wiki on 2024.7.08th
- weekly wiki on 2024.7.16th
- weekly wiki on 2024.7.22nd
- weekly wiki on 2024.7.29th
- weekly wiki on 2024.8.05th
- weekly wiki on 2024.8.12th
- weekly wiki on 2024.8.19th
- weekly wiki on 2024.8.26th
- weekly wiki on 2024.9.02nd
- weekly wiki on 2024.9.09th
- weekly wiki on 2024.9.16th
- weekly wiki on 2024.9.23rd
- weekly wiki on 2024.9.30th
- weekly wiki on 2024.10.07th
- weekly wiki on 2024.10.14th
- weekly wiki on 2024.10.21th
- weekly wiki on 2024.10.28th
- weekly wiki on 2024.11.04th
- weekly wiki on 2024.11.11th
- weekly wiki on 2024.11.18th
- weekly wiki on 2024.11.25th
- weekly wiki on 2024.12.02nd
- weekly wiki on 2024.12.09th
- weekly wiki on 2024.12.16th
- weekly wiki on 2024.12.23rd
- weekly wiki on 2024.12.30th
- weekly wiki on 2025.1.06th
- weekly wiki on 2025.1.13th
- weekly wiki on 2025.1.20th
- weekly wiki on 2025.1.27th
- weekly wiki on 2025.2.10th
- weekly wiki on 2025.2.17th
- weekly wiki on 2025.2.24th
- weekly wiki on 2025.3.03rd
- weekly wiki on 2025.3.10th
- weekly wiki on 2025.3.17th
- weekly wiki on 2025.3.24th
- weekly wiki on 2025.3.31st
- weekly wiki on 2025.4.07th
- weekly wiki on 2025.4.14th
- weekly wiki on 2025.4.21st
- weekly wiki on 2025.4.28th
- weekly wiki on 2025.5.05th
- weekly wiki on 2025.5.12th
- weekly wiki on 2025.5.19th
- weekly wiki on 2025.5.26th
- weekly wiki on 2025.6.02nd
- weekly wiki on 2025.6.09th
- weekly wiki on 2025.6.16th