Weekly Wiki

Greetings!
This is Matthew in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
Today is April 17th and a brand new week has begun! Check out what Seeed did last week!
Latest Wiki Launched
File System and XIAO ESP32S3 Sense

In this tutorial, we will focus on the use of the file system of XIAO ESP32S3, mainly on the use of the microSD card slot for the Sense version. At the same time, we will introduce the official ESP file system SPIFFS, the chip's built-in Flash, etc.
SenseCraft Model Assistant Getting Start with Seeed Studio XIAO ESP32S3

SenseCraft Model Assistant is an open-source project focused on embedded AI. We have optimized excellent algorithms from OpenMMLab for real-world scenarios and made implemention more user-friendly, achieving faster and more accurate inference on embedded devices.
How to use 40-Pin GPIO on reComputer Jetson Boards(NVIDIA)

This wiki demonstrates how to access and control the 40-pin GPIO of reComputer Jetson Boards. For this wiki, we have used reComputer J4012 as an example. However, the steps will be similar for other reComputer Jetson boards as well.
Getting Started with SenseCAP S2120 8-in-1 LoRaWAN Weather Sensor

We added this will for you getting started with SenseCAP S2120 8-in-1 LoRaWAN Weather Sensor.
RS485 750cm Ultrasonic Level Sensor

The RS485 750cm Ultrasonic Level Sensor utilizes ultrasonic sensing technology to measure distances with a measuring range of 28-750cm.
Existed Wiki Updated
SenseCAP Sensor Hub Data Logger

Sensor Hub Data logger is an easy-to-deploy cellular station, 2 power source options are available: Solar power with a rechargeable battery and power adapter power.
We have updated the wiki contents for better browsing.
SenseCAP S2100 LoRaWAN Data Logger

The SenseCAP S2100 Data Logger is a versatile device that can connect to MODBUS-RTU RS485/Analog/GPIO sensors, allowing for easy transmission of data to the LoRaWAN network.
We have updated the wiki contents for better browsing.
Getting S2100 started with 12V RS485 Sensor

Let's get started on learning how to use the S2100 with a 12V RS485 sensor. Once we've got that down, we'll move on to the basics of S2100's application. This will give you a good idea of how to connect your own customized sensor in the future.
We have updated the wiki contents for better browsing.
XIAO ESP32C3 accesses Home Assistant via ESPHome service

We have added an FAQ:
My XIAO ESP32C3 is connected to network, but why don't I see the sensor data refreshed?
If you have the same issue, you can refer to here and check it.