Weekly Wiki

Greetings
This is Matthew in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
Today is June 12th and a brand new week has begun! Check out what Seeed did last week!
Latest Wiki Launched
Grove - VOC Gas Sensor (SGP40)
The Grove - VOC Gas Sensor (SGP40) is an innovative environmental sensing module developed for a wide array of Volatile Organic Compound (VOC) detection applications. Based on the advanced Sensirion SGP40 sensor, it excels in transforming raw sensor signals into standardized digital signals for seamless integration into existing systems.

XIAO CAN Bus Expansion Board
The XIAO CAN Bus Expansion Board is specifically designed to work with the Seeed Studio XIAO development board, providing an easy and convenient way to add CAN bus communication functionality to your projects. CAN bus (Controller Area Network) is a widely used communication protocol in automotive, industrial, and other embedded systems, allowing for reliable and robust data exchange between different nodes.

Grove - D7S Vibration Sensor
The Grove - D7S Vibration Sensor is a powerful earthquake detection module that provides real-time monitoring of seismic activities. It is based on the advanced D7S module developed by Omron Corporation, a leading manufacturer of sensing technology.

Grove Lightning Sensor AS3935
The Grove Lightning Sensor is a highly sensitive sensor that detects electric fields free in air and using an internal proprietary algorithm determines if it is caused by the front end of a storm with lightning events. It is very easy to be used as a plug and play device using the Grove standard cable can accept several adjustments to be optimized for the application environment, both indoor or outdoor.

Getting Started with reComputer Industrial
reComputer industrial series offers full systems including NVIDIA Jetson™ Xavier NX/ Orin Nano/Orin NX/ modules, ranging from 20 TOPS to 100 TOPS AI performance. Preinstalled with Jetpack 5.1.1, reComputer industrial simplifies development, ideal for bulding applications of video analytics, object detection, natural language processing, medical imaging, and robots, which brings digital transformantion across industries of smart cities, security, industrial automation, smart factories.

reComputer Industrial J20 Hardware and Interfaces Usage
This wiki introduces the various different hardware and interfaces on the reComputer Industrial J2012, J2011 and how to use them to expand your project ideas.
reComputer Industrial J40, J30 Hardware and Interfaces Usage
This wiki introduces the various different hardware and interfaces on the reComputer Industrial J4012, J4011, J3011, J3010 and how to use them to expand your project ideas.
Streamlining Web Development The Perfect Duo - Linkstar and WordPress
This wiki will guide you through the installation process of WordPress using Docker and how to access the WordPress dashboard. Embrace the transformative power of Linkstar as you customize your local host website, captivating customers and driving sales. Prepare to experience unparalleled growth, efficiency, and technical prowess with the cutting-edge capabilities of Linkstar.
Existed Wiki Updated
XIAO ESP32C3 accesses Home Assistant via ESPHome service
We have added FAQ5: I used the Jlink flash firmware, but I got the error "Programming of range @address 0x08000000 failed (block verification error) Program failed Failed to program and verify target"
FAQs for reTerminal Usage
We have updated the steps for Connect to STM32 using CM4 and flash the firmware.