Weekly Wiki

Greetings
This is Matthew in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
Today is July 24th and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
Deploy YOLOv8 on NVIDIA Jetson using TensorRT
This wiki guide explains how to deploy a YOLOv8 model into NVIDIA Jetson Platform and perform inference using TensorRT. Here we use TensorRT to maximize the inference performance on the Jetson platform.
Different computer vision tasks will be introduced here such as:
- Object Detection
- Image Segmentation
- Image Classification
- Pose Estimation
- Object Tracking

EdgeBox RPi 200 Balena OS Setup
Balena is an Internet of Things (IoT) platform designed to help developers build, deploy, and manage IoT applications across a fleet of devices. It supports a wide range of device architectures and includes features for containerized application deployment, making it possible to easily update your IoT software and HostOS, fix bugs and introduce new features on your IoT applications.

TinyML Topic Page
TinyML is a field of study in Machine Learning and Embedded Systems that explores machine learning on small, low-powered microcontrollers, enabling secure, low-latency, low-power and low-bandwidth machine learning inferencing on edge devices. If you're excited about TinyML but not sure where to start, our one-stop guide is perfect for you. This guide provides an overview of what TinyML is, the opportunities it offers, and step-by-step instructions on how to get started. Join this exciting field and start your TinyML journey today!

Existed Wiki Updated
Add IMX219 and IMX477 camera usages to reComputer Industrial J20 Series
Add IMX219 and IMX477 camera usages to reComputer Industrial J20 Series
Add IMX219 and IMX477 camera usages to reComputer Industrial J40, J30 Series
Add IMX219 and IMX477 camera usages to reComputer Industrial J40, J30 Series
Add 4G module usage on reterminal DM
Add 4G module usage on reterminal DM

Update sensecraft edge OS download link and add tips about 32-bit driver
Update sensecraft edge OS download link and add tips about 32-bit driver
XIAO Canbus Expansion board
Thanks for the notices, we have changed pin promopt to the correct ones:

- GND
- CAN-H
- CAN-L
- LED Indicators for RX/TX
- SN65NVD230
Add reTerminal DM DI/DO wiring samples
Upload PCB Source file for reTermianl Bridge
Add Wio 1110 libraries Installation steps
The Efforts of Contributor
Past Weekly wiki
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th