Weekly Wiki ✨

Greetings
This is Matthew in Seeed Studio and welcome to the Seeed Studio weekly wiki! Each Monday, I will introduce you our latest wiki, including the ones related to our new products, the interesting projects published by Seeed Studio, and the tutorials, introductions, etc... You name it.
✨ For each week, when a collaborator contributes a project or fixes something important, we put the stars at the end of title of "Weekly Wiki" for more people be able to see their efforts👍.
Today is August 21st and a brand new week has begun! Check out what Seeed Studio did last week!
Latest Wiki Launched
SenseCAP T1000 Tracker
SenseCAP T1000 is a compact LoRaWAN® tracker that utilizes GNSS/Wi-Fi/Bluetooth for precise indoor & outdoor location tracking. It boasts self-geo-adaptive capabilities, local data storage, and an impressive months of battery life. Additionally, it is equipped with temperature, light, and motion sensors, making it ideal for a variety of location-based applications.
SenseCAP Indicator x LoRa Application Development
We have published a wiki about using SenseCAP Indicator for peer-to-peer data transfer under the LoRa network.
This demonstration showcases how to establish a basic LoRa communication between the SenseCAP Indicator and the XIAO board using the Wio-E5 as an intermediary. The SenseCAP Indicator retrieves sensor data from the XIAO, which is then transmitted via Wio-E5. The transmitted payload is subsequently received by the SenseCAP Indicator, which deciphers and outputs. the result and displays the data on its screen.
Existed Wiki Updated
Andanced OV5640 camera Sensor for XIAO ESP32S3 Sense
We now have a new fully XIAO ESP32S3 Sense-compatible powerful camera, the OV5640, on our shelves, and if you purchase it, you can replace the camera to use it.

Update Indicator flash firmware
We have updated the firmware for SenseCAP Indicator(both ESP32S3 and RP2040 chip)
Flash TinyML model on XIAO ESP32S3 Sense using SenseCraft Model Assistant function
We flash the SenseCraft Model Assistant program in advance for all XIAO ESP32S3 Sense participating in the Workshop, and pre-set the model for face recognition. Simply connect the XIAO ESP32S3 Sense to your PC via a data cable to instantly display face recognition.

The Efforts of Contributor✨
MicroPython for ESP32C3
Thanks our contributor - Zachary for adding a wiki page about connecting XIAO ESP32C3 and Seeed Studio Expansion Board to build a Wi-Fi signal strength tracker, which proves invaluable when establishing a high-speed, high-quality family network, programming with MicroPython.

Thanks our contributor for organizing tinyML workshop page
Thanks our contributor - Salman for organizing tinyML workshop page to make the course more logical.
Past Weekly wiki
- weekly wiki on 2.27th
- weekly wiki on 3.06th
- weekly wiki on 3.13th
- weekly wiki on 3.20th
- weekly wiki on 3.27th
- weekly wiki on 4.03rd
- weekly wiki on 4.10th
- weekly wiki on 4.17th
- weekly wiki on 4.24th
- weekly wiki on 5.15th
- weekly wiki on 5.22nd
- weekly wiki on 5.29th
- weekly wiki on 6.05th
- weekly wiki on 6.12th
- weekly wiki on 6.19th
- weekly wiki on 7.03th
- weekly wiki on 7.10th
- weekly wiki on 7.17th
- weekly wiki on 7.24th
- weekly wiki on 7.31th
- weekly wiki on 8.07th
- weekly wiki on 8.14th ✨