SenseCAP Indicator X DALL·E
DALL-E is an advanced AI model developed by OpenAI that can generate images from textual descriptions. DALL-E has been trained on a massive dataset of images and their corresponding textual descriptions.
Given a textual prompt, DALL-E can generate a unique image that matches the description. The model has demonstrated impressive capabilities, such as generating images of fictional creatures, objects, and scenes that do not exist in the real world. DALL-E has potential applications in various fields, including art, design, and advertising.
Please follow the Step 1 and Step 2 to set the Wi-Fi and API Key.
Given a text description and create your own image!


Click on image for full view, click it again to return.

In addition to the demonstrated functionality, SenseCAP provides fully open source code and detailed tutorials,click here for more details.
FAQ
The device is connected to WIFi but still prompts "Please check the wifi connection"
- Please try connecting to another Wi-Fi, or check your router settings.
Please set the Open AI API key first
- The API Key is not set, or the setting fails, please set it again.
Request fail
- Check if the API Key is correct.
Tech Support
Need help with your SenseCAP Indicator? We're here to assist you!