How to Create your own UI
LvGL
LvGL is an open-source graphics library providing everything you need to create an embedded GUI with easy-to-use graphical elements, beautiful visual effects, and a low memory footprint.
Example Code
We provide the demo code of the UI interface, and lvGL example file are many sample codes for drawing UI for reference, you can modify the sample code or customize your own UI.
#include "freertos/FreeRTOS.h"
#include "freertos/task.h"
#include "esp_log.h"
#include "bsp_board.h"
#include "lv_demos.h"
#include "lv_port.h"
#include "ui_demo1.h"
#include "ui_demo2.h"
#define LOG_MEM_INFO 1
static const char *TAG = "app_main";
void app_main(void)
{
ESP_LOGI("TAG", "system start");
ESP_ERROR_CHECK(bsp_board_init());
lv_port_init();
#if CONFIG_LCD_AVOID_TEAR
ESP_LOGI(TAG, "Avoid lcd tearing effect");
#if CONFIG_LCD_LVGL_FULL_REFRESH
ESP_LOGI(TAG, "LVGL full-refresh");
#elif CONFIG_LCD_LVGL_DIRECT_MODE
ESP_LOGI(TAG, "LVGL direct-mode");
#endif
#endif
lv_port_sem_take();
lv_demo_widgets(); /* A widgets example. This is what you get out of the box */
//lv_demo_music(); /* A modern, smartphone-like music player demo. */
//lv_demo_stress(); /* A stress test for LVGL. */
//lv_demo_benchmark(); /* A demo to measure the performance of LVGL or to compare different settings. */
// ui_demo1_init(); /* A demo to show virtual printer (must be 800*480)*/
//ui_demo2_init(); /* A demo to show virtual tuner
/* (must be 480*800, set LCD_EVB_SCREEN_ROTATION_90 in menuconfig)*/
lv_port_sem_give();
#if LOG_MEM_INFO
static char buffer[128]; /* Make sure buffer is enough for `sprintf` */
while (1) {
sprintf(buffer, " Biggest / Free / Total\n"
"\t DRAM : [%8d / %8d / %8d]\n"
"\t PSRAM : [%8d / %8d / %8d]",
heap_caps_get_largest_free_block(MALLOC_CAP_INTERNAL),
heap_caps_get_free_size(MALLOC_CAP_INTERNAL),
heap_caps_get_total_size(MALLOC_CAP_INTERNAL),
heap_caps_get_largest_free_block(MALLOC_CAP_SPIRAM),
heap_caps_get_free_size(MALLOC_CAP_SPIRAM),
heap_caps_get_total_size(MALLOC_CAP_SPIRAM));
ESP_LOGI("MEM", "%s", buffer);
vTaskDelay(pdMS_TO_TICKS(10000));
}
#endif
}
Squareline Studio(Optional)
Squareline Studio is a multi-platform design tool that uses a visual interface to help designers and developers work quickly and efficiently. SquareLine Studio makes it possible by creating the perfect code for your projects. Whether you use C or Python, you can export code for both.
If you need to create a more complex or advanced UI interface, it‘s recommended that you use Squareline Studio for development.
Squareline Studio Installation
We provide a demo project for the UI page:
SenseCAP Indicator/squareline_project
Replace with your own UI
- Step 1:You can make changes in our demo project, or create a new UI page
Open the demo project and make changes:

Create a new project:
Note:The resolution of the screen is 480*480.

- Step 2:Export your finished page as UI files

- Step 3:Remove all the original UI files and copy your onw UI files to this direct.

- Step 4:Build and Flash the project
Run the following command to build, flash and monitor the project:
idf.py -p PORT build flash monitor
Tech Support
Need help with your SenseCAP Indicator? We're here to assist you!