Buzzer
The built-in buzzer of SenseCAP Indicator is a passive buzzer, meaning that it requires an AC signal(PWM) to trigger and output a sound, you can generate various tones and effects.
Basic
#include <Arduino.h>
#define Buzzer 19 //Buzzer GPIO
void setup() {
digitalWrite(Buzzer, OUTPUT); //Set Buzzer as an output
analogWrite(Buzzer, 127); //Generates pwm of 50% duty cycle
}
void loop() {
delay(1000);
digitalWrite(Buzzer, LOW); //Turn off the Buzzer
}
Example Code 1
This example use a buzzer to play melodies. It sends a square wave of the appropriate frequency to the buzzer, generating the corresponding tone. " Twinkle Twinkle Little Start..."
#include <Arduino.h>
#define Buzzer 19 //Buzzer GPIO
int length = 15; /* the number of notes */
char notes[] = "ccggaagffeeddc ";
int beats[] = { 1, 1, 1, 1, 1, 1, 2, 1, 1, 1, 1, 1, 1, 2, 4 };
int tempo = 300;
void setup() {
//set buzzer pin as output
pinMode(19, OUTPUT);
}
void loop() {
for(int i = 0; i < length; i++) {
if(notes[i] == ' ') {
delay(beats[i] * tempo);
} else {
playNote(notes[i], beats[i] * tempo);
}
delay(tempo / 2); /* delay between notes */
}
}
//Play tone
void playTone(int tone, int duration) {
for (long i = 0; i < duration * 1000L; i += tone * 2) {
digitalWrite(19, HIGH);
delayMicroseconds(tone);
digitalWrite(19, LOW);
delayMicroseconds(tone);
}
}
void playNote(char note, int duration) {
char names[] = { 'c', 'd', 'e', 'f', 'g', 'a', 'b', 'C' };
int tones[] = { 1915, 1700, 1519, 1432, 1275, 1136, 1014, 956 };
// play the tone corresponding to the note name
for (int i = 0; i < 8; i++) {
if (names[i] == note) {
playTone(tones[i], duration);
}
}
}
Example Code 2
This example demonstrates an alarm when the CO2 value is greater than 1000ppm.
#include <Arduino.h>
#include <Wire.h>
#include <SPI.h>
#include <SD.h>
#include <SensirionI2CScd4x.h>
#define Buzzer 19 //Buzzer GPIO
SensirionI2CScd4x scd4x;
String SDDataString = "";
void sensor_power_on(void) {
pinMode(18, OUTPUT);
digitalWrite(18, HIGH);
}
void sensor_scd4x_init(void) {
uint16_t error;
char errorMessage[256];
scd4x.begin(Wire);
// stop potentially previously started measurement
error = scd4x.stopPeriodicMeasurement();
if (error) {
Serial.print("Error trying to execute stopPeriodicMeasurement(): ");
errorToString(error, errorMessage, 256);
Serial.println(errorMessage);
}
// Start Measurement
error = scd4x.startPeriodicMeasurement();
if (error) {
Serial.print("Error trying to execute startPeriodicMeasurement(): ");
errorToString(error, errorMessage, 256);
Serial.println(errorMessage);
}
}
void sensor_scd4x_get(void) {
uint16_t error;
char errorMessage[256];
Serial.print("sensor scd4x: ");
// Read Measurement
uint16_t co2;
float temperature;
float humidity;
error = scd4x.readMeasurement(co2, temperature, humidity);
if (error) {
Serial.print("Error trying to execute readMeasurement(): ");
errorToString(error, errorMessage, 256);
Serial.println(errorMessage);
} else if (co2 == 0) {
Serial.println("Invalid sample detected, skipping.");
} else {
Serial.print("Co2:");
Serial.print(co2);
Serial.print("\t");
Serial.print("Temperature:");
Serial.print(temperature);
Serial.print("\t");
Serial.print("Humidity:");
Serial.println(humidity);
}
if( co2 > 1000 ) {
analogWrite(Buzzer, 10);
} else {
analogWrite(Buzzer, 0);
}
}
int cnt = 0;
void setup() {
Serial.begin(115200);
sensor_power_on();
Wire.setSDA(20);
Wire.setSCL(21);
Wire.begin();
sensor_scd4x_init();
digitalWrite(Buzzer, OUTPUT);
}
void loop() {
delay(5000);
sensor_scd4x_get();
}
Tech Support
Don't worry, we've got you covered! Please visit our Seeed Official Discord Channel to ask your questions!
If you have large order or customization requirement, please contact iot@seeed.cc