Introduction
SenseCAP T1000 is a compact LoRaWAN® tracker that utilizes GNSS/Wi-Fi/Bluetooth for precise indoor & outdoor location tracking. It boasts self-geo-adaptive capabilities, local data storage, and an impressive months of battery life. Additionally, it is equipped with temperature, light, and motion sensors, making it ideal for a variety of location-based applications.
![]()
| Compatible Network | Temperature | Light | Accelerometer | |
|---|---|---|---|---|
| SenseCAP T1000-A |
| ✅ | ✅ | ✅ |
| SenseCAP T1000-B |
| |||
| SenseCAP T1000-E |
| ✅ | ✅ | ✅ |
Features
Accurate Positioning
GNSS, Wifi, BLE, 3 positioning technologies for both indoor and outdoor solutions.
GNSS Positioning (Outdoor)
The tracker will get location outdoor via satellite system (GPS/BeiDou/more), then uploads the data to server by LoRa wireless.
![]()
Wi-Fi / Bluetooth Positioning (Indoor)
Tracker scan the MAC address and RSSI of nearby Wi-Fi/Bluetooth and upload it through LoRaWAN. The application server needs to calculate the real geographical location based on the MAC address and signal strength (RSSI).
![]()
Offline Data Storage
Capable of storing 1000+ records locally. The storage capacity of 1 hour upload interval exceeds 40 days.
When the LoRaWAN signal coverage is weak or there is no network coverage, the data will be saved and entered in the next cycle. When the device returns to an area with the LoRaWAN network coverage, it will send the offline data automatically.
![]()
Cross-Regional Adaptability
T1000 provides seamless global LoRaWAN® region switching, automatically adjusting to the appropriate LoRaWAN® frequency plan based on detected location coordinates, ensuring optimal performance across Europe, pan-America, and beyond.
![]()
Months of Battery Life
Powered by the LR1110 and featuring low power consumption, most of the models can lasts for over 3 months of battery life with 1 hour upload interval in GNSS only mode, with the motion sensor disabled. (Battery life may vary with configuration parameters such as frequency band, positioning mode, and data upload interval. Please refer to the Battery Life Calculation for detailed reference)
![]()
Temp, Light, Motion Sensors
Temperature & light sensors are included to keep track of the environmental data on the go. For example, temp data can be used to inference the possibility if the food / vaccine goes bad. Light data shows if it is seen by unwanted eyes.
![]()
Decentralized Gateway Network for location Provenance
Helium’s decentralized network is built on a trust mechanism where every gateway shares its location, and Helium validates the authenticity of these locations. When using Helium with T1000, by cross-checking the gateway’s location, you can have a approximate location of T1000. This provides an additional layer of validation, increasing the data’s validity compared to other networks.
![]()
Emergency Report
Motion sensor to detect anomaly, SOS button for emergency reporting and automatically switch to high-frequency data transmission

Architecture
![]()
Applications
- International Asset Tracing
- Search And Rescue
- Equipment Monitoring
![]()
Specification
Model Specification
We provide two different solutions for users, and comes in three versions: A, B and E.
-
T1000-A/T1000-B: These two versions are designed for LoRaWAN network, supporting indoor (Wi-Fi + Bluetooth) + outdoor positioning (GNSS). T1000-A is equipped with essential features, including a temperature sensor, light sensor, motion sensor, while T1000-B comes without these sensors.
-
T1000-E: It features open-source software and is available in two separate versions: one for LoRaWAN and the other for Meshtastic. Both offer full source code, enabling developers to customize and expand their functions freely.

General Parameters
Location
| GNSS Constellation | GPS/GLONASS/Galileo/BeiDou/QZSS |
|---|---|
| GNSS Sensitivity | -145dBm cold start / -160 dBm Tracking |
| GNSS Location Accuracy | 2.5m CEP 50% |
| Wi-Fi Positioning | Passive scanning, uploads the scanned 4 MAC addresses |
| Bluetooth Positioning | uploads the scanned 3 best signal MAC addresses of Beacon |
| Data Cache | Cache 1000 data when there is no LoRaWAN network |
Battery