Skip to main content

Datacake Integrated(via TTS)

Datacake is a multi-purpose IoT platform, which provides the possibility of building custom IoT applications, without requiring programming skills.

To meet the growing need for building IoT applications, we’ve been working with Datacake to create templates to enable the community to add SenseCAP T1000 Tracker to Datacake through The Things Network conveniently and easily.

pir

Before starting the setup, please check Connect SenseCAP T1000 to TTS to connect your SenseCAP T1000 Tracker to TTS first.

Configure The Datacake​

To begin, register an account on Datacake.

Create a Workspace​

First, create a Workspace on Datacake by navigating to the Create Workspace button in the upper left corner.

pir

Add Device​

Click Devices on the left hand menu. To add a new device, click the Add Device button on the right.

pir

Choose LoRaWAN to add LoRaWAN devices.

pir

We uploaded a template for users, you only need to select the product model and paste your device EUI to quickly set up.

info

Device Template: Seeed SenseCAP T1000

pir

Get a API Token​

Navigate to Account Settings on your Datacake workspace, and copy your API Token.

pir

Configure The Things Stack​

On The Things Stack, navigate to Integrations → Webhooks, and click Add Webhook.

pir

Choose the Datacake Webhook template.

pir

Name your integration by filling in the Webhook ID and paste the API token from Datacake for the authorization.

pir

Datacake Dashboard​

Then you can check your devcie data on the Dashboard.

pir

Loading Comments...