Qubitro Integrated(via TTS)
Qubitro is a Device Data Platform (DDP) for developers that provides the tools, workflows, and infrastructure you need to develop solutions faster, without the need of manual integration of multiple services. Qubitro supports popular data sources out-of-the-box and provides tools for real-time collaboration on your projects combined with scalable infrastructure.
The content of this chapter will guide users how to connect the SenseCAP T1000 Tracker to Qubitro through TTN.
![]()
Before starting the setup, please check Connect SenseCAP T1000 to TTS to connect your SenseCAP T1000 Tracker to TTS first.
Configure The Qubitro
To get started, create an account with Qubitro. By creating an account, you’ll automatically be on a Starter plan.
Get credentials from Qubitro Dashboard
Create a new project.
![]()
Click on the New source button and click on The Things Stack in the list.
![]()
![]()
Then you will get the Project ID and Webhook Signing Keys.
![]()
Configure The Things Stack
Navigate to TTS Console to configure the webhook integration.
On The Things Stack, navigate to Integrations → Webhooks, and click Add Webhook.
![]()
Choose the Qubitro Webhook template.
![]()
Name your integration by filling in the Webhook ID, and paste the values provided in the first step on Qubitro Portal.
![]()
Click on the Create Qubitro Webhook button and go back to the Qubitro Portal.
Device status
Click on the Go to project button and then the Refresh button to verify that the devices are listed successfully.
Once the integration is configured, all devices connected to the same project on The Things Stack will be synchronized automatically.
![]()
Configure the decoder on Qubitro
Navigate to your device page, and click Create function button.
![]()
Choose the Decoder function, and click Get started.
![]()
We uploaded a template for users,you only need to select the product model to quickly set up.
Formatter type: Device template
Manufacturer Brand: Seeed Studio
Model: SenseCAP_T1000
Then click Save and complete.
![]()
Check the data
Navigate to the device and click on the Data tab to verify the incoming data.
![]()
Customize the dashboard(optional)
Location Dashboard
Navigate to your dashbaord page, and click Create new.
![]()
Name your dashboard and click Create.
![]()
Choose Map for the widget type.
![]()
Choose your device and coordinates value.
![]()
Then you can check you location on the dashbaord. You can also customize your other widgets.
![]()