Connect to The Things Network
The Things Stack(TTS) is a LoRaWAN® Network Server stack which is the critical component for any LoRaWAN solution. In this chapter we will guide users to connect the SenseCAP T100 Tracker to the Things Network.
Device Configuration
Before connecting to the TTS, you need to configure the basic parameters of your device on SenseCAP Mate APP, check Get Started for more details.
- Set the platform to TTN, and then copy the Device EUI/APP EUI/APP Key.
![]()
The Things Network
The Things Stack(TTS) is an enterprise grade LoRaWAN network server, built on an open-source core. The Things Stack allows you to build and manage LoRaWAN networks on your own hardware or in the cloud.
To begin, register an account on The Things Network.

Step 1: Create an application
Navigate to Applications page, click "+Create application".

Enter an Application ID, click Create Application to save your changes.

Step 2: Register the Device
We uploaded a template for users,you only need to select the product model to quickly set up. Select the input method to 'Select the end device in the LoRaWAN Device Repository'
End device brand:SenseCAP
Model:SenseCAP T1000 Tracker A/B
Select the frequency plan according to your device.
![]()
Paste the Device EUI/APP EUI/APP Key from the SenseCraft App, and then click Register end device.
![]()
![]()
The "JoinEUI" above is simliar to "AppEUI".
Step 3: Check the data
When the device tries to connect to the network, the breathing light will flash. If the device joins the network successfully, the breathing light will flash quickly, and there will be a light and cheerful melody.
Then you can check the data on the TTS console.
![]()