edit

Sensor health

This article is mainly introducing sensors that are able to provide body health advice via measuring heart rate, fingerprint, GSR and EMG. We offer various types of sensors about humanbeings' body feature on our website and reading this illustration may help you have an in-depth knowledge about our products.

Principles

Category of Sensors Content
GSR GSR sensors help us measure sweat gland activity related to emotional agitation. We use the electrical properties of the skin to measure GSR. In other words, the skin resistance changes with sweat gland activity, which is, sweat gland activity occurs, the more sweating, the smaller the skin resistance.
EMG EMG detector is a bridge connects human body and electrical, the sensor gathers small muscle signal then process with 2th amplify and filter, the output signal can be recognized by Arduino.
Heart Rate The heart rate sensor uses optical technology to detect the amount of blood oxygen in the subcutaneous capillaries to detect the corresponding human heart rate, so that the module can easily and conveniently measure the heart rate. The heart rate sensor uses optical technology to detect the heart rate of the human body through changes in the amount of blood oxygen in the subcutaneous capillaries. Heart rate detection can be widely used in scenarios such as wearable devices and fitness auxiliary equipment.
Fingerprint A fingerprint sensor is a sensing device, which belongs to an optical fingerprint sensor and a semiconductor fingerprint sensor, and is a key device for automatic fingerprint collection.

Field of Applicaitons

There are a numerous use of these health-related sensors. Particularly, using these kinds of sensors, human beings can be monitored and saved from potential dangers. Hence the health sensors play important roles in various sectors, which include industry, medical, social applications, and domestic applications for monitoring body feature of people.

Field of application Function Examples of detected sensors
Hospital Monitoring heart rate of patients in avoidance of being in danger and give advice for health. Heart rate, EMG, GSR
Gym Supervising the heart rate of people who are doing exercises for fitness and body health advice. Heart rate, EMG, GSR
Asylum for lunatic Monitoring heart rate, emotional behaviours and body health. Heart rate, EMG, GSR
Indoor Entrance ( Bank, government, firm, private land and etc. ) Providing stable methods for security. Fingerprint
Laboratory Gathering and analyzing experimental data to offer helpful advice for humanbeings and social development. Heart rate, EMG, GSR

Seeed Health Sensors

For all the products in our bazaar, please click Products in Bazaar to check.

Name Thumbnail image Operate voltage Input interface Click to buy
Grove - Fingerprint Sensor 3.6V-6V TTL Serial Buy Now
Grove - Ear-clip Heart Rate Sensor 3V-5.25V TTL Serial Buy Now
Grove - Chest Strap Heart Rate Sensor 3V-5.5V TTL Serial Buy Now
Grove - Finger-clip Heart Rate Sensor 5V I2C Buy Now
Grove - Finger-clip Heart Rate Sensor with shell 5V I2C Buy Now
Grove - GSR sensor 3.3-5V Analog Buy Now
Grove - EMG Detector 3.3-5V Analog Buy Now

Tech Support

if you have any technical issue. submit the issue into our forum.