Skip to main content

Troubleshooting BIOS-Related Issues

Some issues with Odyssey can be resolved by configuring BIOS settings. Below are some problems that can be addressed using BIOS settings. First, we will describe how to access the BIOS setup.

How to access the BIOS setup​

Press the Power Button and keep pressing DEL key until you see the BIOS Setup.

How to solve the problem of being unable to connect to Wi-Fi and Bluetooth​

Check BIOS settings and enable Wi-Fi and Bluetooth from BIOS.

Is the built-in fan controllable​

Currently the fan is controlled by BIOS, and not controlled by user. The fan speed is set according to the CPU temperature. Check Chipset -> FAN Contorl in the BIOS setup screen for more information.

How to set the ODYSSEY - X86J41x5 to auto power on when power plugged in​

This also need to be configured in the BIOS. Enter BIOS settings by pressing DEL key. Navigate to Chipset -> Restore on AC Power Loss and change settings to Last State.

pir

Does ODYSSEY board have Boot Guard for Secure Boot​

Yes, you can enable the Security Boot option in the BIOS. When this is enabled, the BIOS will disable booting from unauthenticated devices.

Why is GPIO still working after Odyssey is Shut down​

To set this up, you need to update to the latest BIOS we provide. In the latest BIOS, you can change enable to disable here to turn off both GPIO and ODYSSEY.

pir

Loading Comments...