Audio Features
This wiki introduces how to set the Audio for Wio Terminal using with ReSpeaker 2-Mic Hats.
Please visit the Audio Overview for the Hardware Connection.
Playing Audio from SD Card
This example plays a music file from MicroSD card using ReSpeaker 2-Mic Hat.
-
You will need a MicroSD card for Wio Terminal.
-
Save your music file in the
.wavformat and save it into your MicroSD card. In this example, you will need to name the music file asSDTEST2.WAV. -
Insert the MicroSD card to Wio Terminal, upload the following code to Wio Terminal.
-
Make sure that ReSpeaker 2-Mic is connected with Wio Terminal correctly, and a speaker is plugged into the JST2.0 Speaker pin on the ReSpeaker 2-Mic.
You may also find this example in the github page.
You may configure the wm8960.volume(0.7) to adjust the volume of the speaker! Furthermore, you can also uncomment wm8960.outputSelect(HEADPHONE) to have audio jack as the output!
#include <Audio.h>
#include <Wire.h>
#include <Seeed_FS.h>
#include "SD/Seeed_SD.h"
AudioPlaySdWav playSdWav1;
AudioOutputI2S i2s1;
AudioConnection patchCord1(playSdWav1, 0, i2s1, 0);
AudioConnection patchCord2(playSdWav1, 1, i2s1, 1);
AudioControlWM8960 wm8960;
void setup() {
Serial.begin(9600);
AudioMemory(8);
while (!Serial) {};
wm8960.enable();
// wm8960.outputSelect(HEADPHONE);
wm8960.volume(0.7);
while (!SD.begin(SDCARD_SS_PIN,SDCARD_SPI,10000000UL)) {
Serial.println("Card Mount Failed");
return;
}
delay(1000);
}
void loop() {
if (playSdWav1.isPlaying() == false) {
Serial.println("Start playing");
playSdWav1.play("SDTEST2.WAV");
delay(10); // wait for library to parse WAV info
}
// do nothing while playing...
}
Recording Sound and Playback
This example records sound using the mic on ReSpeaker 2-Mic Hat, stores the raw data to MicroSD card and plays it back through the Speaker.
-
You will need a MicroSD card for Wio Terminal.
-
Upload the code to Wio Terminal.
-
Press the right button on the top of Wio Terminal (
WIO_KEY_A) and it will start recording. Speak to the mic of ReSpeaker 2-Mic Hat. It saves the recording to the MicroSD card asRECORD.WAV.
While recording, press one of any other two buttons to stop recording.
-
Press the left button on the top of Wio Terminal (
WIO_KEY_C) and it will play theRECORD.WAVthat just recorded. -
Press the middle button on the top of Wio Terminal (
WIO_KEY_B) will stop playing the recording.
You may also find this example in the github page.
// Record sound as raw data to a SD card, and play it back.
#include <Bounce.h>
#include <Audio.h>
#include <Wire.h>
#include <Seeed_FS.h>
#include "SD/Seeed_SD.h"
// GUItool: begin automatically generated code
AudioInputI2S i2s2; //xy=105,63
AudioAnalyzePeak peak1; //xy=278,108
AudioRecordQueue queue1; //xy=281,63
AudioPlaySdRaw playRaw1; //xy=302,157
AudioOutputI2S i2s1; //xy=470,120
AudioConnection patchCord1(i2s2, 0, queue1, 0);
AudioConnection patchCord2(i2s2, 0, peak1, 0);
AudioConnection patchCord3(playRaw1, 0, i2s1, 0);
AudioConnection patchCord4(playRaw1, 0, i2s1, 1);
AudioControlWM8960 wm8960;
// GUItool: end automatically generated code
Bounce buttonRecord = Bounce(WIO_KEY_A, 8);
Bounce buttonStop = Bounce(WIO_KEY_B, 8); // 8 = 8 ms debounce time
Bounce buttonPlay = Bounce(WIO_KEY_C, 8);
// which input on the audio shield will be used?
const int myInput = AUDIO_INPUT_MIC;
// Remember which mode we're doing
int mode = 0; // 0=stopped, 1=recording, 2=playing
// The file where data is recorded
File frec;
void setup() {
Serial.begin(9600);
// Configure the pushbutton pins
pinMode(WIO_KEY_A, INPUT_PULLUP);
pinMode(WIO_KEY_B, INPUT_PULLUP);
pinMode(WIO_KEY_C, INPUT_PULLUP);
// Audio connections require memory, and the record queue
// uses this memory to buffer incoming audio.
AudioMemory(60);
// Enable the audio shield, select input, and enable output
wm8960.enable();
wm8960.inputSelect(myInput);
wm8960.volume(1);
// Initialize the SD card
while (!SD.begin(SDCARD_SS_PIN,SDCARD_SPI,10000000UL)) {
Serial.println("Card Mount Failed");
return;
}
}
void loop() {
// First, read the buttons
buttonRecord.update();
buttonStop.update();
buttonPlay.update();
// Respond to button presses
if (buttonRecord.fallingEdge()) {
Serial.println("Record Button Press");
if (mode == 2) stopPlaying();
if (mode == 0) startRecording();
}
if (buttonStop.fallingEdge()) {
Serial.println("Stop Button Press");
if (mode == 1) stopRecording();
if (mode == 2) stopPlaying();
}
if (buttonPlay.fallingEdge()) {
Serial.println("Play Button Press");
if (mode == 1) stopRecording();
if (mode == 0) startPlaying();
}
// If we're playing or recording, carry on...
if (mode == 1) {
continueRecording();
}
if (mode == 2) {
continuePlaying();
}
// when using a microphone, continuously adjust gain
if (myInput == AUDIO_INPUT_MIC) adjustMicLevel();
}
void startRecording() {
Serial.println("startRecording");
if (SD.exists("RECORD.RAW")) {
// The SD library writes new data to the end of the
// file, so to start a new recording, the old file
// must be deleted before new data is written.
SD.remove("RECORD.RAW");
}
frec = SD.open("RECORD.RAW", FILE_WRITE);
if (frec) {
queue1.begin();
mode = 1;
}
}
void continueRecording() {
if (queue1.available() >= 2) {
byte buffer[512];
// Fetch 2 blocks from the audio library and copy
// into a 512 byte buffer. The Arduino SD library
// is most efficient when full 512 byte sector size
// writes are used.
memcpy(buffer, queue1.readBuffer(), 256);
queue1.freeBuffer();
memcpy(buffer+256, queue1.readBuffer(), 256);
queue1.freeBuffer();
// write all 512 bytes to the SD card
elapsedMicros usec = 0;
frec.write(buffer, 512);
// Uncomment these lines to see how long SD writes
// are taking. A pair of audio blocks arrives every
// 5802 microseconds, so hopefully most of the writes
// take well under 5802 us. Some will take more, as
// the SD library also must write to the FAT tables
// and the SD card controller manages media erase and
// wear leveling. The queue1 object can buffer
// approximately 301700 us of audio, to allow time
// for occasional high SD card latency, as long as
// the average write time is under 5802 us.
Serial.print("SD write, us=");
Serial.println(usec);
}
}
void stopRecording() {
Serial.println("stopRecording");
queue1.end();
if (mode == 1) {
while (queue1.available() > 0) {
frec.write((byte*)queue1.readBuffer(), 256);
queue1.freeBuffer();
}
frec.close();
}
mode = 0;
}
void startPlaying() {
Serial.println("startPlaying");
playRaw1.play("RECORD.RAW");
mode = 2;
}
void continuePlaying() {
if (!playRaw1.isPlaying()) {
playRaw1.stop();
mode = 0;
}
}
void stopPlaying() {
Serial.println("stopPlaying");
if (mode == 2) playRaw1.stop();
mode = 0;
}
void adjustMicLevel() {
// TODO: read the peak1 object and adjust sgtl5000_1.micGain()
// if anyone gets this working, please submit a github pull request :-)
}
Peak Detection

This example plays a music file from the MicroSD card and detects peak value of both channels and display on the Serial Monitor.
-
Same configurations as the Playing Audio from SD Card from above.
-
Upload the code, and you should be able to see the peaks of both channels of on the Serial Monitor, whilst the music is playing via the speaker.
#include <Audio.h>
#include <Wire.h>
#include <SPI.h>
#include <Seeed_FS.h>
#include "SD/Seeed_SD.h"
// GUItool: begin automatically generated code
AudioPlaySdWav playSdWav1; //xy=422,359
AudioAnalyzePeak peak1; //xy=611,306
AudioAnalyzePeak peak2; //xy=612,396
AudioOutputI2S i2s1; //xy=792,365
AudioConnection patchCord1(playSdWav1, 0, peak1, 0);
AudioConnection patchCord2(playSdWav1, 0, i2s1, 0);
AudioConnection patchCord3(playSdWav1, 1, peak2, 0);
AudioConnection patchCord4(playSdWav1, 1, i2s1, 1);
AudioControlWM8960 wm8960;
// GUItool: end automatically generated code
void setup() {
Serial.begin(9600);
AudioMemory(10);
wm8960.enable();
// wm8960.outputSelect(HEADPHONE);
wm8960.volume(0.7);
while (!SD.begin(SDCARD_SS_PIN,SDCARD_SPI,10000000UL)) {
Serial.println("Card Mount Failed");
return;
}
delay(1000);
}
// for best effect make your terminal/monitor a minimum of 62 chars wide and as high as you can.
elapsedMillis msecs;
void loop() {
if (playSdWav1.isPlaying() == false) {
Serial.println("Start playing");
//playSdWav1.play("SDTEST1.WAV");
playSdWav1.play("SDTEST2.WAV");
//playSdWav1.play("SDTEST3.WAV");
//playSdWav1.play("SDTEST4.WAV");
delay(10); // wait for library to parse WAV info
}
if (msecs > 40) {
if (peak1.available() && peak2.available()) {
msecs = 0;
float leftNumber = peak1.read();
float rightNumber = peak2.read();
int leftPeak = leftNumber * 30.0;
int rightPeak = rightNumber * 30.0;
int count;
for (count=0; count < 30-leftPeak; count++) {
Serial.print(" ");
}
while (count++ < 30) {
Serial.print("<");
}
Serial.print("||");
for (count=0; count < rightPeak; count++) {
Serial.print(">");
}
while (count++ < 30) {
Serial.print(" ");
}
Serial.print(leftNumber);
Serial.print(", ");
Serial.print(rightNumber);
Serial.println();
}
}
}
Playing Audio with the LCD Display
This example also plays music file from the MicroSD card and displays both channels peak on the screen of Wio Terminal.
-
Same configurations as the Playing Audio from SD Card from above.
-
Upload the code, and you should be able to see the peaks of both channels of on the screen, whilst the music is playing via the speaker.
NOTE: Because we are using LCD graphics with the audio library, it has a bigger workload. It is recommended to Overclock the SAMD51 in this example. Under Arduino IDE, select Tools -> CPU Speed -> 200MHz. This will increase the overall graphics performance.
You may also find this example in the github page.
#include <TFT_eSPI.h> // Hardware-specific library
#include <Audio.h>
#include <Wire.h>
#include <Seeed_FS.h>
#include "SD/Seeed_SD.h"
// GUItool: begin automatically generated code
AudioPlaySdWav playSdWav1; //xy=512,375
AudioAnalyzePeak peak2; //xy=787,543
AudioAnalyzePeak peak1; //xy=790,488
AudioOutputI2S i2s1; //xy=827,334
AudioConnection patchCord1(playSdWav1, 0, peak1, 0);
AudioConnection patchCord2(playSdWav1, 0, i2s1, 0);
AudioConnection patchCord3(playSdWav1, 1, peak2, 0);
AudioConnection patchCord4(playSdWav1, 1, i2s1, 1);
AudioControlWM8960 wm8960;
// GUItool: end automatically generated code
TFT_eSPI tft_e = TFT_eSPI();
TFT_eSprite tft = TFT_eSprite(&tft_e);
void setup() {
Serial.begin(9600);
delay(500);
tft_e.begin();
tft_e.fillScreen(ILI9341_BLACK);
tft.createSprite(240, 320);
tft.fillSprite(TFT_BLACK);
tft.setTextColor(ILI9341_YELLOW);
//tft.setTextSize(3);
tft.setCursor(40, 8);
tft.println("Peak Meter");
AudioMemory(10);
wm8960.enable();
// wm8960.outputSelect(HEADPHONE);
wm8960.volume(0.7);
while (!SD.begin(SDCARD_SS_PIN,SDCARD_SPI,10000000UL)) {
Serial.println("Card Mount Failed");
return;
}
delay(1000);
}
elapsedMillis msecs;
void loop() {
if (playSdWav1.isPlaying() == false) {
Serial.println("Start playing");
playSdWav1.play("SDTEST2.WAV");
delay(10); // wait for library to parse WAV info
}
if (msecs > 15) {
if (peak1.available() && peak2.available()) {
msecs = 0;
float leftNumber = peak1.read();
float rightNumber = peak2.read();
Serial.print(leftNumber);
Serial.print(", ");
Serial.print(rightNumber);
Serial.println();
// draw the verticle bars
int height = leftNumber * 240;
tft.fillRect(60, 280 - height, 40, height, ILI9341_GREEN);
tft.fillRect(60, 280 - 240, 40, 240 - height, ILI9341_BLACK);
height = rightNumber * 240;
tft.fillRect(140, 280 - height, 40, height, ILI9341_GREEN);
tft.fillRect(140, 280 - 240, 40, 240 - height, ILI9341_BLACK);
// a smarter approach would redraw only the changed portion...
// draw numbers underneath each bar
tft.fillRect(60, 284, 40, 16, ILI9341_BLACK);
tft.setCursor(67, 284);
tft.print(leftNumber);
tft.fillRect(140, 284, 40, 16, ILI9341_BLACK);
tft.setCursor(147, 284);
tft.print(rightNumber);
tft.pushSprite(0, 0);
}
}
}
Example Demos
Audio Spectrum Visualizer
This is an example using the FFT function of the Audio Library to calculate and visualize Audio Spectrum.
Feature
-
Audio Spectrum of Music
-
Press buttons to increase/decrease volume
Complete Code
#include <Audio.h>
#include <Wire.h>
#include <Seeed_FS.h>
#include "SD/Seeed_SD.h"
#include <TFT_eSPI.h> // Hardware-specific library
#include <Bounce.h>
// The display size and color to use
const unsigned int matrix_width = 19;
const unsigned int matrix_height = 12;
// These parameters adjust the vertical thresholds
const float maxLevel = 0.5; // 1.0 = max, lower is more "sensitive"
const float dynamicRange = 10.0; // total range to display, in decibels
const float linearBlend = 0.4; // useful range is 0 to 0.7
// GUItool: begin automatically generated code
AudioPlaySdWav playSdWav1; //xy=260,184
AudioMixer4 mixer1; //xy=505,238
AudioOutputI2S i2s2; //xy=701,139
AudioAnalyzeFFT1024 fft1024_1; //xy=761,235
AudioConnection patchCord1(playSdWav1, 0, mixer1, 0);
AudioConnection patchCord2(playSdWav1, 0, i2s2, 0);
AudioConnection patchCord3(playSdWav1, 1, mixer1, 1);
AudioConnection patchCord4(playSdWav1, 1, i2s2, 1);
AudioConnection patchCord5(mixer1, fft1024_1);
AudioControlWM8960 wm8960;
// GUItool: end automatically generated code
const int lowerFFTBins[] = {0, 1, 2, 3, 4, 5, 6, 8, 10, 12, 15, 18, 22, 27, 32, 38, 45, 53, 63, 74, 87, 102, 119, 138, 160, 186, 216, 250, 289, 334, 385, 444};
const int upperFFTBins[] = {0, 1, 2, 3, 4, 5, 7, 9, 11, 14, 17, 21, 26, 31, 37, 44, 52, 62, 73, 86, 101, 118, 137, 159, 185, 215, 249, 288, 333, 384, 443, 511};
float thresholdVertical[matrix_height];
float thresholdVert[matrix_height];
float level;
unsigned int x, y;
const uint8_t gridSize = 10;
float val = 0.7;
Bounce buttonUp = Bounce(WIO_KEY_A, 8);
Bounce buttonDown = Bounce(WIO_KEY_C, 8);
TFT_eSPI tft = TFT_eSPI();
TFT_eSprite spr = TFT_eSprite(&tft);
void setup() {
Serial.begin(115200);
// while (!Serial);
pinMode(WIO_KEY_A, INPUT_PULLUP);
pinMode(WIO_KEY_C, INPUT_PULLUP);
tft.begin();
tft.fillScreen(TFT_BLACK);
tft.setRotation(3);
tft.setTextSize(2);
tft.drawString("Audio Spectrum Visualiser", 10, 10);
AudioMemory(20);
computeVerticalLevels();
for (int i = 0; i < 8; i++) {
Serial.print("thresholdVertical ");
Serial.print(i);
Serial.print(" = ");
Serial.println(thresholdVertical[i]);
}
for (unsigned int j = 0; j < matrix_height; j++) {
thresholdVert[j] = thresholdVertical[matrix_height - j - 1];
}
wm8960.enable();
// wm8960.outputSelect(HEADPHONE);
wm8960.volume(val);
while (!SD.begin(SDCARD_SS_PIN, SDCARD_SPI, 16000000UL)) {
Serial.println("Card Mount Failed");
return;
}
playSdWav1.play("SDTEST2.WAV");
delay(20);
fft1024_1.windowFunction(AudioWindowHanning1024);
spr.createSprite(180, 320);
spr.fillSprite(TFT_BLACK);
tft.setRotation(2);
}
void loop() {
buttonUp.update();
buttonDown.update();
if (buttonUp.fallingEdge() && val < 1.0) {
val += 0.1;
}
if(buttonDown.fallingEdge() && val >= 0.1) {
val -= 0.1;
}
wm8960.volume(val);
if (fft1024_1.available()) {
colorRainbow();
spr.pushSprite(0, 10);
}
}
void colorRainbow() {
for (x = 0; x < matrix_width; x++) {
level = fft1024_1.read(lowerFFTBins[x], upperFFTBins[x]);
for (y = 0; y < 12; y++) {
if (level >= thresholdVert[y]) {
spr.fillRect(y * 12, xy(x, y) * 2, gridSize, gridSize, Wheel(y * 24));
// Serial.println(xy(x, y));
}
else {
spr.fillRect(y * 12, xy(x, y) * 2, gridSize, gridSize, TFT_BLACK);
}
}
}
}
// Input a value 0 to 255 to get a color value.
// The colours are a transition r - g - b - back to r.
uint32_t Wheel(byte WheelPos) {
WheelPos = 255 - WheelPos;
if (WheelPos < 85) {
return color2color(255 - WheelPos * 3, 0, WheelPos * 3);
} else if (WheelPos < 170) {
WheelPos -= 85;
return color2color(0, WheelPos * 3, 255 - WheelPos * 3);
} else {
WheelPos -= 170;
return color2color(WheelPos * 3, 255 - WheelPos * 3, 0);
}
}
uint32_t color2color(uint8_t r, uint8_t g, uint8_t b) {
return ((uint32_t)r << 16) | ((uint32_t)g << 8) | b;
}
unsigned int xy(unsigned int x, unsigned int y) {
return x * 8;
}
void computeVerticalLevels() {
unsigned int y;
float n, logLevel, linearLevel;
for (y = 0; y < matrix_height; y++) {
n = (float)y / (float)(matrix_height - 1);
logLevel = pow(n * -1.0 * (dynamicRange / 20.0), 10);
linearLevel = 1.0 - n;
linearLevel = linearLevel * linearBlend;
logLevel = logLevel * (1.0 - linearBlend);
thresholdVertical[y] = (logLevel + linearLevel) * maxLevel;
}
}
Mic Spectrum Visualizer
This is an example using the Mics of ReSpeaker 2-Mic Hats and FFT calculations.
Feature
- Audio Spectrum of Mics
Complete Code
#include <Audio.h>
#include <Wire.h>
#include <Seeed_FS.h>
#include "SD/Seeed_SD.h"
#include <TFT_eSPI.h> // Hardware-specific library
// The display size and color to use
const unsigned int matrix_width = 19;
const unsigned int matrix_height = 12;
// These parameters adjust the vertical thresholds
const float maxLevel = 0.6; // 1.0 = max, lower is more "sensitive"
const float dynamicRange = 10.0; // total range to display, in decibels
const float linearBlend = 0.6; // useful range is 0 to 0.7
// GUItool: begin automatically generated code
AudioInputI2S i2s1; //xy=376,203
AudioMixer4 mixer1; //xy=608,235
AudioAnalyzeFFT1024 fft1024_1; //xy=770,200
AudioConnection patchCord1(i2s1, 0, mixer1, 0);
AudioConnection patchCord2(i2s1, 1, mixer1, 1);
AudioConnection patchCord3(mixer1, fft1024_1);
AudioControlWM8960 wm8960;
// GUItool: end automatically generated code
const int lowerFFTBins[] = {0, 1, 2, 3, 4, 5, 6, 8, 10, 12, 15, 18, 22, 27, 32, 38, 45, 53, 63, 74, 87, 102, 119, 138, 160, 186, 216, 250, 289, 334, 385, 444};
const int upperFFTBins[] = {0, 1, 2, 3, 4, 5, 7, 9, 11, 14, 17, 21, 26, 31, 37, 44, 52, 62, 73, 86, 101, 118, 137, 159, 185, 215, 249, 288, 333, 384, 443, 511};
float thresholdVertical[matrix_height];
float thresholdVert[matrix_height];
float level;
unsigned int x, y;
const uint8_t gridSize = 10;
TFT_eSPI tft = TFT_eSPI();
TFT_eSprite spr = TFT_eSprite(&tft);
void setup() {
Serial.begin(115200);
// while (!Serial);
tft.begin();
tft.fillScreen(TFT_BLACK);
tft.setRotation(3);
tft.setTextSize(2);
tft.drawString("Mic Spectrum Visualiser", 20, 10);
AudioMemory(20);
computeVerticalLevels();
for (int i = 0; i < 8; i++) {
Serial.print("thresholdVertical ");
Serial.print(i);
Serial.print(" = ");
Serial.println(thresholdVertical[i]);
}
for (unsigned int j = 0; j < matrix_height; j++) {
thresholdVert[j] = thresholdVertical[matrix_height - j - 1];
}
wm8960.enable();
while (!SD.begin(SDCARD_SS_PIN, SDCARD_SPI, 16000000UL)) {
Serial.println("Card Mount Failed");
return;
}
delay(20);
fft1024_1.windowFunction(AudioWindowHanning1024);
spr.createSprite(180, 320);
spr.fillSprite(TFT_BLACK);
tft.setRotation(2);
}
void loop() {
if (fft1024_1.available()) {
colorRainbow();
spr.pushSprite(0, 10);
}
}
void colorRainbow() {
for (x = 0; x < matrix_width; x++) {
level = fft1024_1.read(lowerFFTBins[x], upperFFTBins[x]);
for (y = 0; y < 12; y++) {
if (level >= thresholdVert[y]) {
spr.fillRect(y * 12, xy(x, y) * 2, gridSize, gridSize, Wheel(y * 24));
// Serial.println(xy(x, y));
}
else {
spr.fillRect(y * 12, xy(x, y) * 2, gridSize, gridSize, TFT_BLACK);
}
}
}
}
// Input a value 0 to 255 to get a color value.
// The colours are a transition r - g - b - back to r.
uint32_t Wheel(byte WheelPos) {
WheelPos = 255 - WheelPos;
if (WheelPos < 85) {
return color2color(255 - WheelPos * 3, 0, WheelPos * 3);
} else if (WheelPos < 170) {
WheelPos -= 85;
return color2color(0, WheelPos * 3, 255 - WheelPos * 3);
} else {
WheelPos -= 170;
return color2color(WheelPos * 3, 255 - WheelPos * 3, 0);
}
}
uint32_t color2color(uint8_t r, uint8_t g, uint8_t b) {
return ((uint32_t)r << 16) | ((uint32_t)g << 8) | b;
}
unsigned int xy(unsigned int x, unsigned int y) {
return x * 8;
}
void computeVerticalLevels() {
unsigned int y;
float n, logLevel, linearLevel;
for (y = 0; y < matrix_height; y++) {
n = (float)y / (float)(matrix_height - 1);
logLevel = pow(n * -1.0 * (dynamicRange / 20.0), 10);
linearLevel = 1.0 - n;
linearLevel = linearLevel * linearBlend;
logLevel = logLevel * (1.0 - linearBlend);
thresholdVertical[y] = (logLevel + linearLevel) * maxLevel;
}
}
Record and Play at Real Time
This is an example of real-time recording and playing.
Feature
- Recording and Playing at real-time
Complete Code
#include <Audio.h>
#include <Wire.h>
#include <Seeed_FS.h>
#include "SD/Seeed_SD.h"
// GUItool: begin automatically generated code
AudioInputI2S i2s1; //xy=274,186
AudioRecordQueue queue1; //xy=550,172
AudioPlayQueue queue2; //xy=550,220
AudioOutputI2S i2s2; //xy=769,208
AudioConnection patchCord1(i2s1, 0, queue1, 0);
AudioConnection patchCord2(queue2, 0, i2s2, 0);
AudioConnection patchCord3(queue2, 0, i2s2, 1);
AudioControlWM8960 wm8960;
// GUItool: end automatically generated code
const int myInput = AUDIO_INPUT_MIC;
void setup() {
Serial.begin(9600);
// while (!Serial);
AudioMemory(20);
wm8960.enable();
wm8960.inputSelect(myInput);
wm8960.volume(0.9);
// wm8960.outputSelect(HEADPHONE);
queue1.begin();
}
void loop() {
if (queue1.available() >= 2)
{
// Recording buffer
byte buffer[256];
memcpy(buffer, queue1.readBuffer(), 256);
queue1.freeBuffer();
// Playing buffer
queue2.getBuffer();
queue2.playBuffer();
}
}