Skip to main content

Deploy the Microduck RL Environment on Jetson

This chapter prepares the Jetson system, installs the project environment, explains the directory layout, and verifies that PPO training can execute on CUDA.

Hardware and Software​

The following platform was validated for this demo:

ItemVersion
DeviceSeeed reComputer with Jetson Orin NX 16GB
OSUbuntu 24.04 LTS, aarch64
JetPack / L4TJetPack 7.2 / L4T R39.2
System CUDA13.2
Python3.12
PyTorch2.9.1+cu130
MuJoCo3.10.0
Warp1.12.0

Use NVMe storage with at least 25GB free space. Active cooling, a stable power supply, and a reliable network connection are recommended.

warning

Do not independently replace the JetPack-provided CUDA driver or L4T packages. The Python project is isolated in .venv, while the system GPU stack remains managed by JetPack.

Project Directory​

~/microduck-jetson/
├── deploy_microduck_jetson.sh
├── microduck_rl/
│ ├── src/mjlab_microduck/tasks/
│ ├── scripts/
│ ├── pretrained/pollen-robotics/
│ ├── models/checkpoints/
│ └── logs/rsl_rl/
├── microduck_jetson_startup.md
├── microduck_jetson_training_guide.md
└── microduck_custom_action_training.md

The .venv directory is created locally on Jetson and is intentionally not included in the Git repository.

Clone the Repository​

mkdir -p ~/microduck-jetson
cd ~/microduck-jetson

git clone -b develop https://github.com/jjjadand/microduck_rl.git
cd microduck_rl

Run the Deployment Script​

cd ~/microduck-jetson/microduck_rl

SUDO_PASSWORD=<JETSON_PASSWORD> \
TARGET_DIR=$HOME/microduck-jetson/microduck_rl \
bash deploy_microduck_jetson.sh

The script installs the build and visualization dependencies, installs uv, creates Python 3.12 .venv, synchronizes the locked project dependencies, installs the compatible CUDA PyTorch wheel, and performs CUDA validation.

note

Passing a password through an environment variable is convenient for this reproducible lab setup. For a shared or production device, review the script and run privileged commands interactively instead.

Enter the Environment​

All project commands must run from the repository root:

cd ~/microduck-jetson/microduck_rl
export MUJOCO_GL=egl

Use uv run --no-sync for the commands in this guide. This prevents an unintended dependency re-sync from replacing the Jetson CUDA PyTorch installation.

Verify CUDA​

uv run --no-sync python3 - <<'PY'
import torch

print("PyTorch:", torch.__version__)
print("CUDA runtime:", torch.version.cuda)
print("CUDA available:", torch.cuda.is_available())
print("GPU:", torch.cuda.get_device_name(0))

left = torch.randn(512, 512, device="cuda")
right = torch.randn(512, 512, device="cuda")
result = left @ right
torch.cuda.synchronize()
print("CUDA matmul:", result.device)
PY

Expected results include CUDA available: True, an Orin GPU name, and CUDA matmul: cuda:0.

Run the Training Smoke Test​

uv run --no-sync train Mjlab-Velocity-Flat-MicroDuck \
--env.scene.num-envs 64 \
--agent.logger tensorboard \
--agent.max_iterations 5

A successful run creates a directory under logs/rsl_rl/velocity/ containing configuration files, TensorBoard events, and one or more .pt checkpoints.

When MuJoCo and the training managers start, the terminal prints the active termination, reward, curriculum, actor, and critic configuration:

Microduck MuJoCo and training managers starting in the terminal

After rollout collection begins, each learning iteration reports throughput, reward terms, episode length, curriculum values, and termination statistics:

Microduck PPO training iteration metrics on Jetson

Run 4096 Parallel Training Environments​

For the full training run used in this demo, the backend simulates 4096 independent Microduck environments in parallel:

uv run --no-sync train Mjlab-Velocity-Flat-MicroDuck \
--env.scene.num-envs 4096 \
--agent.logger tensorboard

jtop shows the GPU load and device state while the 4096-environment training process is running:

Jetson jtop output while training 4096 Microduck environments

If memory is insufficient, reduce the environment count using 4096 → 2048 → 1024 → 512.

Visualize the Training Environments​

The backend still trains all 4096 environments. Viewer settings only control how many robots are rendered for inspection and do not reduce the backend training batch unless --env.scene.num-envs is changed.

Render One Microduck​

Rendering one robot is the clearest way to inspect posture, contacts, and gait during training:

One Microduck visualized while the backend trains 4096 environments

Render Multiple Microducks​

Rendering many robots makes the parallel environment concept visible. The full backend run still contains 4096 environments even though only a subset is shown in the Viewer:

Multiple Microducks visualized while the backend trains 4096 environments

The Viewer is intended for short inspection runs. Long training runs normally use headless EGL rendering to avoid continuous drawing overhead.

Optional Performance Setup​

Check the supported power modes before selecting one:

sudo nvpmodel -q
sudo nvpmodel

Monitor the device while training:

tegrastats

Do not copy a power-mode number from another Jetson model. Select a supported high-performance mode for the exact device.

Next Step​

Loading Comments...