Skip to main content

Getting Started with reComputer Robotics J50 Mini

reComputer Mini J501 complete system

reComputer Robotics J50 Mini (reComputer Mini J501) is a compact edge AI computer for robotics and embedded AI development, available as J5011 with NVIDIA Jetson AGX Orin 32GB and J5012 with NVIDIA Jetson AGX Orin 64GB. Both GMSL configurations include a 128GB NVMe SSD and an eight-channel GMSL expansion board. The enclosure measures 119 × 119 × 100 mm and weighs 1325 g.

The platform can be used with NVIDIA Isaac ROS, ROS, PyTorch, and other Jetson-compatible software for multi-camera perception, sensor integration, and robotics development.

note

Available customization options: logo branding, packaging, and firmware flashing.

Features​

  • AGX Orin performance: Up to 275 TOPS with the 64GB module, supporting perception and edge AI workloads.
  • Compact enclosure: A 119 × 119 mm footprint for space-constrained robot integration.
  • Camera connectivity: The J5012 with GMSL includes the GMSL expansion board for up to eight GMSL2 cameras; use compatible cameras and drivers.
  • Wired and wireless expansion: 10GbE and 1GbE networking, plus M.2 Key E for Wi-Fi/Bluetooth expansion.
  • Robotics I/O: Isolated CAN and RS485, digital inputs/outputs, I2S, USB, and HDMI.
  • 48V system integration: XT30 power input with a specified 19–48V DC operating range and a 54V maximum input rating.

Specifications​

Jetson AGX Orin System on Module
SpecificationsreComputer Mini J5011reComputer Mini J5012
ModuleNVIDIA Jetson AGX Orin 32GBNVIDIA Jetson AGX Orin 64GB
AI PerformanceUp to 200 TOPSUp to 275 TOPS
GPU1792-core NVIDIA Ampere architecture GPU
56 Tensor Cores
2048-core NVIDIA Ampere architecture GPU
64 Tensor Cores
GPU Max Frequency930 MHz1.3 GHz
CPU8-core Arm Cortex-A78AE12-core Arm Cortex-A78AE
CPU Max Frequency2.2 GHz
Memory32GB 256-bit LPDDR5
204.8 GB/s
64GB 256-bit LPDDR5
204.8 GB/s
Module Storage64GB eMMC 5.1
Video Encoder1 × 4K60 / 3 × 4K30 (H.265)
6 × 1080p60 / 12 × 1080p30 (H.265)
2 × 4K60 / 4 × 4K30 (H.265)
8 × 1080p60 / 16 × 1080p30 (H.265)
Video Decoder1 × 8K30 / 2 × 4K60 / 4 × 4K30 (H.265)
9 × 1080p60 / 18 × 1080p30 (H.265)
1 × 8K30 / 3 × 4K60 / 7 × 4K30 (H.265)
11 × 1080p60 / 22 × 1080p30 (H.265)
Module Power15W / 40W15W / 60W
JetPackPreinstalled JetPack 6.2; supports JetPack 7.2
Carrier Board
Storage128GB NVMe SSD included
1 × M.2 Key M for NVMe 2280 SSD
NetworkingEthernet1 × RJ45 10GbE; 1 × RJ45 1GbE
Wireless Expansion1 × M.2 Key E for a Wi-Fi/Bluetooth module
I/OUSB2 × USB 3.2 Gen 2 Type-A (10Gbps)
1 × USB 2.0 Type-C (Debug)
1 × USB 3.0 Type-C (Recovery)
Display1 × HDMI 2.1
CAN2 × isolated CAN
RS4851 × isolated RS485
Digital I/O4 × GPI (3.3V); 4 × GPO (3.3V)
I2S1 × I2S (3.3V)
Fan1 × 4-pin fan connector (12V PWM)
RTC1 × 2-pin RTC header
IndicatorsPWR, ACT and USR LEDs
Buttons1 × Reset; 1 × Recovery
Power Input1 × XT30; 19–48V DC; maximum input 54V
GMSL Extension Board
GMSL ConnectivityIncluded in both with-GMSL configurations
2 × Mini-Fakra connectors for up to 8 GMSL2 cameras
Others
MechanicalDimensions (W × D × H)119 × 119 × 100 mm
Weight1325 g
InstallationDesktop
Operating Temperature−10°C to 60°C

Hardware Overview​

reComputer Mini J501 hardware overview 1
reComputer Mini J501 hardware overview 2
Mini J501 carrier board top view
Mini J501 carrier board side view
Mini J501 carrier board bottom view

Flash JetPack OS​

This section shows how to flash the Mini J501 system image to the NVMe SSD in reComputer Robotics J50 Mini.

Supported NVIDIA Jetson Modules​

Prerequisites​

  • Ubuntu host PC
  • reComputer Robotics J50 Mini with its Jetson AGX Orin module, NVMe SSD, and compatible power supply
  • USB Type-C data transmission cable
info

We recommend that you use physical ubuntu host devices instead of virtual machines. Please refer to the table below to prepare the host machine.

JetPack Version Ubuntu Version (Host Computer)
18.04 20.04 22.04 24.04
JetPack 6.x ✅ ✅
JetPack 7.2 ✅ ✅ ✅

Note: For JetPack 7.2, Ubuntu 24.04 is supported for flashing and target-side component installation only. Use Ubuntu 20.04 or 22.04 if you need host development components.

Prepare the JetPack Image​

Here, we need to download the system image to our Ubuntu PC corresponding to the Jetson module we are using:

Jetpack VersionJetson Module GMSL Download Link1SHA256
7.2 AGX Orin 64GB✅Download1cd0d7004f426a524a55761bf01dd22280829b9834cbd11d4094b29865f46fe9
AGX Orin 32GB✅Downloadc369b02c979a8d0e1bd926725e94eba19be0e1b6a1a145e03a1179e77b72c5fd
6.2.1 AGX Orin 64GB✅Download53859b314aba332c417c7295d9f6b6711bc7d8c4352dad55aa917af80757330c
AGX Orin 32GB✅Download16408ec8d3b8b0e01eb7edd81b0367357f7dddfdee09388da4c74591d31f917a
danger

The JetPack image files are large and may take around 60 minutes to download. Please wait for the download to complete.

info

To verify the integrity of the downloaded firmware, you can compare the SHA256 hash value.

On an Ubuntu host machine, open the terminal and run the command sha256sum <File> to obtain the SHA256 hash value of the downloaded file. If the resulting hash matches the SHA256 hash provided in the wiki, it confirms that the firmware you downloaded is complete and intact.

Enter Force Recovery Mode​

info

Before we can move on to the installation steps, we need to make sure that the board is in force recovery mode.

Step-by-Step

Step 1. Press and hold the REC button.

Step 2. Power up the carrier board by connecting the power cable, then release REC button .

Step 3. Connect the board to the Ubuntu host PC with a USB Type-C data transmission cable.

Step 4. On the Linux host PC, open a Terminal window and enter the command lsusb. If the returned content has one of the following outputs according to the Jetson SoM you use, then the board is in force recovery mode.

  • For AGX Orin 32GB: 0955:7223 NVidia Corp
  • For AGX Orin 64GB: 0955:7023 NVidia Corp

The below image is for AGX Orin 32GB:

Flash to Jetson Step by Step​

Step 1: Extract the downloaded image file:

cd <path-to-image>
sudo tar xpf mfi_xxxx.tar.gz
# For JetPack 7.2 example: sudo tar xpf mfi_recomputer-mini-agx-orin-j501x-32g-7.2.0-39.2.0-2026-06-25.tar.gz
# For JetPack 6.2.1 example: sudo tar xpf mfi_recomputer-mini-agx-orin-32g-j501-6.2.1-36.4.4-2026-02-11.tar.gz

Step 2: Execute the following command to flash jetpack system to the NVMe SSD:

cd mfi_xxxx
# For example: cd mfi_recomputer-mini-agx-orin-32g-j501-6.2.1-36.4.4-2026-02-11
sudo ./tools/kernel_flash/l4t_initrd_flash.sh --flash-only --massflash 1 --network usb0 --showlogs

You will see the following output if the flashing process is successful

note

The flash command may run for 2-10 minutes.

Step 3: Connect reComputer Robotics J50 Mini to a display through HDMI, then complete the initial system configuration:

info

Please complete the System Configuration according to your needs.

Step 4 (optional): Install the NVIDIA JetPack SDK. Open a terminal on the Jetson and run:

sudo apt update
sudo apt install nvidia-jetpack

Hardware Interfaces Usage​

Hardware Interface Guide

Click the button below to open the Mini J501 interface guide for connector pinouts, wiring, and step-by-step usage instructions.

Resources​

Tech Support & Product Discussion​

Thank you for choosing our products! For technical support and product discussions, use the following channels.

Loading Comments...