Skip to main content

Benchmark of Multistream Inference on Raspberrypi 5 with Hailo8

Introduction

YOLOv8 (You Only Look Once version 8) is the popular most YOLO series of real-time pose estimation and object detection models. It builds upon the strengths of its predecessors by introducing several advancements in speed, accuracy, and flexibility. The Hailo8 is used to accelerate inference speed, featuring a 26 TOPS AI performance.

This wiki showcases benchmarking of YOLOv8m for object detection on Raspberry Pi 5 with hailo8. All tests utilize the same model (YOLOv8m), quantized to int8, with an input size of 640x640 resolution, batch size set to 8.

Prepare Hardware

reComputer AI R2140reComputer Industrial R20xxreComputer Industrial R21xx

Install AI kit on RPi5

Please refer to this

Prepare software

update the system

sudo date -s "$(wget -qSO- --max-redirect=0 google.com 2>&1 | grep Date: | cut -d' ' -f5-8)Z"
sudo apt update
sudo apt full-upgrade

Download hailo software on hailo office web

Note: you need an official Hailo account and ensure you are logged in. Click this link download the necessary libs as follows:

pir

Install hailort_4.19.0_arm64.deb on respberrypi5

sudo dpkg -i hailort_4.19.0_arm64.deb 

sudo reboot

Install dkms

sudo apt-get install dkms

Install hailort-pcie-driver_4.19.0_all.deb

sudo dpkg -i hailort-pcie-driver_4.19.0_all.deb 
sudo reboot

Create and activate a Python virtual environment

python -m venv hailo_env
source hailo_env/bin/activate

Install hailort-4.19.0-cp311-cp311-linux_aarch64.whl

pip install hailort-4.19.0-cp311-cp311-linux_aarch64.whl 

Check if the software is installed

hailortcli fw-control identify

The result is show as bellow:

ain@pi5-hailo:~ $ hailortcli fw-control identify
Executing on device: 0000:01:00.0
Identifying board
Control Protocol Version: 2
Firmware Version: 4.19.0 (release,app,extended context switch buffer)
Logger Version: 0
Board Name: Hailo-8
Device Architecture: HAILO8
Serial Number: HLLWM2B225100548
Part Number: HM218B1C2FAE
Product Name: HAILO-8 AI ACC M.2 M KEY MODULE EXT TEMP

Set pcie to gen2/gen3(gen3 is faster than gen2)

Add following text to /boot/firmware/config.txt

#Enable the PCIe external connector

dtparam=pciex1

#Force Gen 3.0 speeds

dtparam=pciex1_gen=3

note

If you want to use gen2,please comment dtparam=pciex1_gen=3

Install Tapps

Install necessary libs

sudo apt-get install -y rsync ffmpeg x11-utils python3-dev python3-pip python3-setuptools python3-virtualenv python-gi-dev libgirepository1.0-dev gcc-12 g++-12 cmake git libzmq3-dev

sudo apt-get install -y libopencv-dev python3-opencv

sudo apt-get install -y libcairo2-dev libgirepository1.0-dev libgstreamer1.0-dev libgstreamer-plugins-base1.0-dev libgstreamer-plugins-bad1.0-dev gstreamer1.0-plugins-base gstreamer1.0-plugins-good gstreamer1.0-plugins-bad gstreamer1.0-plugins-ugly gstreamer1.0-libav gstreamer1.0-tools gstreamer1.0-x gstreamer1.0-alsa gstreamer1.0-gl gstreamer1.0-gtk3 gstreamer1.0-qt5 gstreamer1.0-pulseaudio gcc-12 g++-12 python-gi-dev

sudo apt install python3-gi python3-gi-cairo gir1.2-gtk-3.0

Set hailo_pci force_desc_page_size

sudo nano /etc/modprobe.d/hailo_pci.conf

And then input the following content.

options hailo_pci force_desc_page_size=4096

Finally, press Ctrl+X, type Y, and press Enter to save the file

And then reboot the raspberrypi5

sudo reboot

Download Tapps

git clone --depth 1 https://github.com/hailo-ai/tappas.git

Download hailort to tapps

cd tappas
mkdir hailort
git clone https://github.com/hailo-ai/hailort.git hailort/sources

Change common.py

nano downloader/common.py

And change the content like below, add RaspberryPI5 = 'rpi5'in common.py:

class Platform(Enum):
X86 = 'x86'
ARM = 'arm'
IMX8 = 'imx8'
Rockchip = 'rockchip'
RaspberryPI = 'rpi'
RaspberryPI5 = 'rpi5'

ANY = 'any'

def __str__(self):
return self.value

Install tappas

./install.sh --skip-hailort --target-platform rpi5

Change batch size to 8

cd ./apps/h8/gstreamer/general/multistream_detection/
nano multi_stream_detection.sh

Add readonly DEFAULT_BATCH_SIZE=8 to the 14 line as follows:

readonly DEFAULT_NETWORK_NAME="yolov5"
readonly DEFAULT_BATCH_SIZE=8
readonly MAX_NUM_OF_DEVICES=4

Add batch_size=$DEFAULT_BATCH_SIZE to the 19 line as follows:

network_name=$DEFAULT_NETWORK_NAME
batch_size=$DEFAULT_BATCH_SIZE
num_of_src=12

Add batch-size=$batch_size to the 154 line as follows:

queue name=hailo_pre_infer_q_0 leaky=no max-size-buffers=30 max-size-bytes=0 max-size-time=0 ! \
hailonet hef-path=$hef_path batch-size=$batch_size device-count=$device_count scheduling-algorithm=0 nms-score-threshold=0.3 nms-iou-threshold=0.45 output-format-type=HAILO_FORMAT_TYPE_FLOAT32 ! \
queue name=hailo_postprocess0 leaky=no max-size-buffers=30 max-size-bytes=0 max-size-time=0 ! \

Finally Ctrl+X and input Y to save the file.

Run multistream inference

sudo chmod +x multi_stream_detection.sh
./multi_stream_detection.sh --network yolov8 --num-of-sources 8 --show-fps

Result

All the results are based on inference with a model input size of 640x640, batch size is 8, and a video resolution of 1280x760, which is 720p.

Channel CountPCIE Gen2 PerformancePCIE Gen3 Performance
1 channel stream39.82FPS76.99FPS
2 channels streams19.86FPS38.21FPS
4 channels streams8.45FPS16.94FPS
8 channels streams3.85FPS8.15FPS
12 channels streams2.94FPS5.43FPS

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...