Welcome
· One min read
Docusaurus blogging features are powered by the blog plugin.
Simply add Markdown files (or folders) to the blog directory.
Regular blog authors can be added to authors.yml.
The blog post date can be extracted from filenames, such as:
2019-05-30-welcome.md2019-05-30-welcome/index.md
A blog post folder can be convenient to co-locate blog post images: