红外发射器入门指南
本教程演示如何在 Wio Terminal 中使用内置红外发射器组件。红外发射器是一个数字接口,可用于发送红外信号,就像遥控器一样!

为 Wio Terminal 安装红外库
-
访问 Seeed_Arduino_IR 仓库,将整个仓库下载到本地驱动器。
-
现在可以将红外库安装到 Arduino IDE 中。打开 Arduino IDE,点击
sketch->Include Library->Add .ZIP Library,选择刚刚下载的Seeed_Arduino_IR文件。

示例代码
导航到 Files -> Examples -> IRLib2 -> Send。发送示例将出现,应如下所示。要测试来自 Wio Terminal 的红外信号,您可以使用 Grove - 红外接收器。这可以轻松修改为使用 Wio Terminal 作为您的电视遥控器!
注意: WIO_IR 为内置红外发射器定义(已在此库的头文件中定义,因此无需在 ino 文件中定义)
/* send.ino Example sketch for IRLib2
* Illustrates how to send a code.
*/
#include <IRLibSendBase.h> // First include the send base
//Now include only the protocols you wish to actually use.
//The lowest numbered protocol should be first but remainder
//can be any order.
#include <IRLib_P01_NEC.h>
#include <IRLib_P02_Sony.h>
#include <IRLibCombo.h> // After all protocols, include this
// All of the above automatically creates a universal sending
// class called "IRsend" containing only the protocols you want.
// Now declare an instance of that sender.
IRsend mySender;
void setup() {
Serial.begin(9600);
delay(2000); while (!Serial); //delay for Leonardo
Serial.println(F("Every time you press a key is a serial monitor we will send."));
}
void loop() {
if (Serial.read() != -1) {
// send a code every time a character is received from the
// serial port. You could modify this sketch to send when you
// push a button connected to an digital input pin.
// Substitute values and protocols in the following statement
// for device you have available.
// mySender.send(SONY,0xa8bca, 20);//Sony DVD power A8BCA, 20 bits
mySender.send(NEC,0x61a0f00f,0);//NEC TV power button=0x61a0f00f
Serial.println(F("Sent signal."));
}
}
注意: 红外发射器位于 Wio Terminal 的背面,在 SD 卡槽的左侧。