Skip to main content

Seeed Studio XIAO SAMD21 上的 SPI 通信

SPI 通信接口​

硬件​

所需材料

硬件连接

  • 步骤 1. Grove-高精度压力传感器的 CSK 连接到 Seeed Studio XIAO 的 SCK。

  • 步骤 2. 传感器的 CS 连接到 Seeed Studio XIAO 的 D3。

  • 步骤 3. 传感器的 SDO 连接到 Seeed Studio XIAO 的 MISO。

  • 步骤 4. 传感器的 SDI 连接到 Seeed Studio XIAO 的 MOSI。

  • 步骤 5. 传感器的 GND 连接到 Seeed Studio XIAO 的 GND。

  • 步骤 6. 传感器的 3V3 连接到 Seeed Studio XIAO 的 3.3V。

  • 步骤 7. 通过 Type-C 数据线将 Seeed Studio XIAO 连接到 PC。

软件​

note

如果这是您第一次使用 Arduino,我们强烈建议您在开始之前先查看 Arduino 入门指南。

#include <Dps310.h>

// Dps310 Opject
Dps310 Dps310PressureSensor = Dps310();

void setup()
{
//pin number of your slave select line
//XMC2GO
int16_t pin_cs = 3;
//for XMC 1100 Bootkit & XMC4700 Relax Kit uncomment the following line
//int16_t pin_cs = 10;

Serial.begin(9600);
while (!Serial);


//Call begin to initialize Dps310
//The parameter pin_nr is the number of the CS pin on your Microcontroller
Dps310PressureSensor.begin(SPI, pin_cs);

//temperature measure rate (value from 0 to 7)
//2^temp_mr temperature measurement results per second
int16_t temp_mr = 2;
//temperature oversampling rate (value from 0 to 7)
//2^temp_osr internal temperature measurements per result
//A higher value increases precision
int16_t temp_osr = 2;
//pressure measure rate (value from 0 to 7)
//2^prs_mr pressure measurement results per second
int16_t prs_mr = 2;
//pressure oversampling rate (value from 0 to 7)
//2^prs_osr internal pressure measurements per result
//A higher value increases precision
int16_t prs_osr = 2;
//startMeasureBothCont enables background mode
//temperature and pressure ar measured automatically
//High precision and hgh measure rates at the same time are not available.
//Consult Datasheet (or trial and error) for more information
int16_t ret = Dps310PressureSensor.startMeasureBothCont(temp_mr, temp_osr, prs_mr, prs_osr);
//Use one of the commented lines below instead to measure only temperature or pressure
//int16_t ret = Dps310PressureSensor.startMeasureTempCont(temp_mr, temp_osr);
//int16_t ret = Dps310PressureSensor.startMeasurePressureCont(prs_mr, prs_osr);


if (ret != 0)
{
Serial.print("Init FAILED! ret = ");
Serial.println(ret);
}
else
{
Serial.println("Init complete!");
}
}


void loop()
{
uint8_t pressureCount = 20;
float pressure[pressureCount];
uint8_t temperatureCount = 20;
float temperature[temperatureCount];

//This function writes the results of continuous measurements to the arrays given as parameters
//The parameters temperatureCount and pressureCount should hold the sizes of the arrays temperature and pressure when the function is called
//After the end of the function, temperatureCount and pressureCount hold the numbers of values written to the arrays
//Note: The Dps310 cannot save more than 32 results. When its result buffer is full, it won't save any new measurement results
int16_t ret = Dps310PressureSensor.getContResults(temperature, temperatureCount, pressure, pressureCount);

if (ret != 0)
{
Serial.println();
Serial.println();
Serial.print("FAIL! ret = ");
Serial.println(ret);
}
else
{
Serial.println();
Serial.println();
Serial.print(temperatureCount);
Serial.println(" temperature values found: ");
for (int16_t i = 0; i < temperatureCount; i++)
{
Serial.print(temperature[i]);
Serial.println(" degrees of Celsius");
}

Serial.println();
Serial.print(pressureCount);
Serial.println(" pressure values found: ");
for (int16_t i = 0; i < pressureCount; i++)
{
Serial.print(pressure[i]);
Serial.println(" Pascal");
}
}

//Wait some time, so that the Dps310 can refill its buffer
delay(10000);
}
  • 步骤 4. 点击 工具 > 串口监视器,或同时按下 Ctrl+Shift+M,成功上传后打开串口监视器,输出如下所示:

pir

Loading Comments...