Skip to main content

使用 XIAO ESP32-S3 Plus 对 reSpeaker XVF3800 44mm 进行 UDP 流式传输

概述​

本项目通过 Wi-Fi 从 reSpeaker XVF3800 44mm 阵列实时流式传输音频。XIAO ESP32-S3 Plus 通过 I2S 捕获处理后的立体声输出,将其拆分为带编号的 UDP 数据包,并发送到你 PC 上的 Python 接收端,由其重新组装音频流并保存为 WAV 文件。

reSpeaker XVF3800 44mm with XIAO ESP32-S3 Plus

功能概览​

  • 以 station 模式将 XIAO 连接到 Wi-Fi 网络。
  • 通过 I2S 从 XVF3800 捕获 48 kHz、立体声、32 位音频。
  • 将 5 秒音频作为 UDP 数据包发送到 PC,每个数据包带有 8 字节头部(AUD0 魔数 + 序列号)。
  • Python 接收端重新组装音频流,检测丢包或重复包,为间隙插入静音,并写入 respeaker_recording.wav。
note

此示例要求 XVF3800 上烧录 I2S 固件,采样率为 48 kHz。如果板子仍在运行 USB 固件镜像,则不会产生 I2S 时钟。请参阅 Update Firmware。

开始之前​

  1. 将开发板与 PC 连接到同一网络。
  2. 在示例程序中设置你的 Wi-Fi 凭据以及 PC 的 IPv4 地址。
  3. 使用 ipconfig(Windows)或 ip addr(Linux/macOS)查找 PC 地址。
  4. 在防火墙中允许 UDP 端口 12345 的入站访问,否则数据包会被静默丢弃。

Arduino 代码​

在上传前先更新以下数值:

// WiFi credentials
const char* ssid = "Your-SSID";
const char* password = "Your-PASSWORD";

// Your PC's IP address and the UDP port the Python script listens on
IPAddress pcIP(192, 168, 1, 100);
const uint16_t udpPort = 12345;

完整代码(流式传输 5 秒音频)​

#include <WiFi.h>
#include <WiFiUdp.h>
#include "AudioTools.h"

// =====================================================
// WIFI CONFIGURATION
// =====================================================

const char* ssid = "Your-SSID";
const char* password = "Your-PASSWORD";

// Your Windows PC IP address
IPAddress pcIP(192, 168, 1, 100);

const uint16_t udpPort = 12345;

WiFiUDP udp;


// =====================================================
// I2S CONFIGURATION
// =====================================================

#define SAMPLE_RATE 48000
#define CHANNELS 2
#define BITS_PER_SAMPLE 32

#define I2S_BCK_PIN 8
#define I2S_WS_PIN 7
#define I2S_TX_PIN 44
#define I2S_RX_PIN 43

AudioInfo info(
SAMPLE_RATE,
CHANNELS,
BITS_PER_SAMPLE
);

I2SStream i2s;
I2SConfig i2sConfig;


// =====================================================
// RECORDING CONFIGURATION
// =====================================================

#define RECORD_SECONDS 5

#define BUFFER_SIZE 1024

#define FRAME_BYTES 8

#define BYTES_PER_SECOND \
(SAMPLE_RATE * CHANNELS * (BITS_PER_SAMPLE / 8))

#define TOTAL_BYTES \
(BYTES_PER_SECOND * RECORD_SECONDS)


// =====================================================
// UDP PACKET CONFIGURATION
// =====================================================

// Header: 4-byte magic + 4-byte sequence
#define HEADER_SIZE 8

#define PACKET_MAGIC "AUD0"

uint8_t audioBuffer[BUFFER_SIZE];

uint8_t packetBuffer[HEADER_SIZE + BUFFER_SIZE];

uint32_t sequenceNumber = 0;


// =====================================================
// WIFI CONNECTION
// =====================================================

bool connectWiFi() {

Serial.printf(
"Connecting to WiFi: %s\n",
ssid
);

WiFi.mode(WIFI_STA);

WiFi.begin(ssid, password);

unsigned long start = millis();

while (WiFi.status() != WL_CONNECTED) {

delay(500);
Serial.print(".");

if (millis() - start > 30000) {

Serial.println("\nWiFi connection timeout!");

return false;
}
}

Serial.println("\nWiFi connected!");

Serial.print("ESP32 IP: ");
Serial.println(WiFi.localIP());

Serial.print("PC destination: ");
Serial.println(pcIP);

Serial.print("UDP port: ");
Serial.println(udpPort);

return true;
}


// =====================================================
// I2S INITIALIZATION
// =====================================================

bool setupI2SInput() {

Serial.println("\nInitializing I2S...");

i2sConfig = i2s.defaultConfig(RX_MODE);

i2sConfig.copyFrom(info);

i2sConfig.pin_bck = I2S_BCK_PIN;
i2sConfig.pin_ws = I2S_WS_PIN;

i2sConfig.pin_data = I2S_TX_PIN;
i2sConfig.pin_data_rx = I2S_RX_PIN;

// XVF3800 supplies BCLK and LRCLK
i2sConfig.is_master = false;

if (!i2s.begin(i2sConfig)) {

Serial.println("I2S initialization failed!");

return false;
}

Serial.println("I2S initialized successfully");

Serial.println("Sample rate: 48000 Hz");
Serial.println("Channels: 2");
Serial.println("Bit depth: 32-bit");

return true;
}


// =====================================================
// SEND ONE UDP AUDIO PACKET
// =====================================================

bool sendAudioPacket(
const uint8_t* data,
size_t length
) {

if (length == 0 || length > BUFFER_SIZE) {
return false;
}

// Header magic
memcpy(
packetBuffer,
PACKET_MAGIC,
4
);

// Sequence number, little-endian
memcpy(
packetBuffer + 4,
&sequenceNumber,
4
);

// Audio payload
memcpy(
packetBuffer + HEADER_SIZE,
data,
length
);

if (!udp.beginPacket(pcIP, udpPort)) {
return false;
}

size_t headerWritten = udp.write(
packetBuffer,
HEADER_SIZE
);

size_t audioWritten = udp.write(
packetBuffer + HEADER_SIZE,
length
);

int result = udp.endPacket();

if (headerWritten != HEADER_SIZE ||
audioWritten != length ||
result != 1) {

Serial.printf(
"UDP send failed at packet %lu\n",
(unsigned long)sequenceNumber
);

return false;
}

sequenceNumber++;

return true;
}


// =====================================================
// RECORD AND TRANSMIT AUDIO
// =====================================================

void recordAndSendAudio() {

Serial.println("\n================================");
Serial.println("STARTING AUDIO TRANSMISSION");
Serial.println("================================");

Serial.printf(
"Recording duration: %d seconds\n",
RECORD_SECONDS
);

Serial.printf(
"Expected audio: %lu bytes\n",
(unsigned long)TOTAL_BYTES
);

size_t totalSent = 0;

uint32_t successfulPackets = 0;
uint32_t failedPackets = 0;

unsigned long startTime = millis();

while (totalSent < TOTAL_BYTES) {

size_t remaining = TOTAL_BYTES - totalSent;

size_t requestSize =
(remaining > BUFFER_SIZE)
? BUFFER_SIZE
: remaining;

// Read I2S audio
size_t bytesRead = i2s.readBytes(
audioBuffer,
requestSize
);

if (bytesRead == 0) {
delay(1);
continue;
}

// Preserve complete stereo frames
bytesRead -= bytesRead % FRAME_BYTES;

if (bytesRead == 0) {
continue;
}

// Send via UDP
if (sendAudioPacket(audioBuffer, bytesRead)) {

totalSent += bytesRead;

successfulPackets++;

} else {

failedPackets++;

// Do not advance totalSent.
// The same audio data will be retried.
}

static size_t lastProgress = 0;

if (totalSent - lastProgress >= BYTES_PER_SECOND) {

lastProgress = totalSent;

Serial.printf(
"Sent: %lu / %lu bytes (%.2f sec)\n",
(unsigned long)totalSent,
(unsigned long)TOTAL_BYTES,
(float)totalSent / BYTES_PER_SECOND
);
}
}

unsigned long elapsed = millis() - startTime;

Serial.println("\n================================");
Serial.println("TRANSMISSION COMPLETE");
Serial.println("================================");

Serial.printf(
"Total audio bytes: %lu\n",
(unsigned long)totalSent
);

Serial.printf(
"Successful packets: %lu\n",
(unsigned long)successfulPackets
);

Serial.printf(
"Failed packets: %lu\n",
(unsigned long)failedPackets
);

Serial.printf(
"Elapsed time: %.2f seconds\n",
elapsed / 1000.0
);

Serial.printf(
"Average data rate: %.2f KB/s\n",
elapsed > 0
? (float)totalSent / elapsed
: 0.0f
);

Serial.println("UDP transmission finished.");
}


// =====================================================
// SETUP
// =====================================================

void setup() {

Serial.begin(115200);

while (!Serial) {
delay(10);
}

AudioLogger::instance().begin(
Serial,
AudioLogger::Info
);

Serial.println("\nReSpeaker 44mm UDP Audio Test");

// 1. Connect WiFi
if (!connectWiFi()) {
while (true) delay(1000);
}

// 2. Initialize UDP
if (!udp.begin(0)) {
Serial.println("UDP initialization failed!");
while (true) delay(1000);
}

Serial.println("UDP initialized");

// 3. Initialize I2S
if (!setupI2SInput()) {
while (true) delay(1000);
}

delay(500);

// 4. Record and transmit
recordAndSendAudio();
}


// =====================================================
// LOOP
// =====================================================

void loop() {

// One-time recording test
delay(1000);
}

在 115200 波特率 下打开串口监视器,以确认 Wi-Fi 连接和流式传输进度。

数据包格式​

字节字段值
0–3MagicAUD0(ASCII)
4–7序列号小端 uint32,从 0 开始
8–1031音频负载1024 字节的原始 32 位立体声 PCM

在 48 kHz × 2 通道 × 4 字节的设置下,一秒是 384,000 字节;五秒是 1,920,000 字节,即 1,875 个 1024 字节的数据包。

Python 脚本(接收并保存音频)​

将以下内容保存为 udp_receiver.py,并在重置开发板之前在电脑上运行。

import socket
import struct
import wave
import time

# ==========================================
# UDP CONFIGURATION
# ==========================================

UDP_IP = "0.0.0.0"
UDP_PORT = 12345

PC_IP = "192.168.1.100"

# ==========================================
# AUDIO CONFIGURATION
# ==========================================

SAMPLE_RATE = 48000
CHANNELS = 2
SAMPLE_WIDTH = 4

RECORD_SECONDS = 5

BYTES_PER_SECOND = (
SAMPLE_RATE * CHANNELS * SAMPLE_WIDTH
)

EXPECTED_BYTES = BYTES_PER_SECOND * RECORD_SECONDS

# Arduino sends 1024-byte audio chunks
CHUNK_SIZE = 1024

EXPECTED_PACKETS = EXPECTED_BYTES // CHUNK_SIZE

# Packet header:
# 4 bytes magic + 4 bytes sequence number
HEADER_SIZE = 8

OUTPUT_FILE = "respeaker_recording.wav"

# ==========================================
# UDP SOCKET
# ==========================================

sock = socket.socket(
socket.AF_INET,
socket.SOCK_DGRAM
)

# Allow reuse of port
sock.setsockopt(
socket.SOL_SOCKET,
socket.SO_REUSEADDR,
1
)

sock.bind((UDP_IP, UDP_PORT))

sock.settimeout(5.0)

print("======================================")
print("ReSpeaker 44mm UDP Audio Receiver")
print("======================================")

print(f"Listening on: {UDP_IP}:{UDP_PORT}")
print(f"PC IP: {PC_IP}")
print(f"Sample rate: {SAMPLE_RATE}")
print(f"Channels: {CHANNELS}")
print(f"Bit depth: {SAMPLE_WIDTH * 8}")
print(f"Expected duration: {RECORD_SECONDS} seconds")
print(f"Expected packets: {EXPECTED_PACKETS}")

print("\nWaiting for ESP32 audio transmission...")

# ==========================================
# AUDIO STORAGE
# ==========================================

audio_data = bytearray()

expected_sequence = 0

received_packets = 0
missing_packets = 0
duplicate_packets = 0
invalid_packets = 0

end_received = False

last_packet_time = time.time()

# ==========================================
# RECEIVE UDP PACKETS
# ==========================================

try:

while True:

try:

data, addr = sock.recvfrom(2048)

last_packet_time = time.time()

# Check packet size
if len(data) < HEADER_SIZE:
invalid_packets += 1
continue

# Decode packet header
magic, sequence = struct.unpack(
"<4sI",
data[:HEADER_SIZE]
)

# End-of-transmission marker
if magic == b"END0":
print("\nEnd-of-transmission received.")
end_received = True
break

# Check packet identifier
if magic != b"AUD0":
invalid_packets += 1
print("Invalid packet identifier")
continue

payload = data[HEADER_SIZE:]

if len(payload) != CHUNK_SIZE:
invalid_packets += 1
print(
f"Unexpected payload size: {len(payload)}"
)
continue

# Handle missing packets
if sequence > expected_sequence:

lost = sequence - expected_sequence

missing_packets += lost

print(
f"Missing {lost} packet(s) before "
f"sequence {sequence}"
)

# Insert silence for missing audio
audio_data.extend(
bytes(lost * CHUNK_SIZE)
)

# Ignore duplicate or out-of-order packets
elif sequence < expected_sequence:

duplicate_packets += 1

print(
f"Duplicate/late packet: {sequence}"
)

continue

# Store audio payload
audio_data.extend(payload)

expected_sequence = sequence + 1

received_packets += 1

# Progress
if received_packets % 375 == 0:

duration = (
len(audio_data) / BYTES_PER_SECOND
)

print(
f"Received: {received_packets} packets | "
f"{duration:.2f} seconds"
)

except socket.timeout:

if received_packets > 0:

print("\nReceiver timeout.")

break

print("Still waiting for ESP32...")

except KeyboardInterrupt:

print("\nRecording stopped by user.")

finally:

sock.close()


# ==========================================
# SAVE WAV FILE
# ==========================================

print("\n======================================")
print("RECORDING STATISTICS")
print("======================================")

print(f"Received packets: {received_packets}")
print(f"Missing packets: {missing_packets}")
print(f"Duplicate packets: {duplicate_packets}")
print(f"Invalid packets: {invalid_packets}")
print(f"End marker received: {end_received}")

print(f"Total audio bytes: {len(audio_data)}")

print(
f"Audio duration: "
f"{len(audio_data) / BYTES_PER_SECOND:.2f} seconds"
)

if len(audio_data) > 0:

# Ensure complete stereo frames
audio_data = audio_data[
:len(audio_data) - len(audio_data) % 8
]

print(f"\nSaving WAV: {OUTPUT_FILE}")

with wave.open(OUTPUT_FILE, "wb") as wav:

wav.setnchannels(CHANNELS)
wav.setsampwidth(SAMPLE_WIDTH)
wav.setframerate(SAMPLE_RATE)

wav.writeframes(audio_data)

print("WAV saved successfully!")

else:

print("No audio received!")

print("\nReceiver finished.")

接收端在 5 秒的 socket 超时后结束,而不是通过结束标记结束,因为该示例程序没有发送可选的 END0 数据包。因此统计信息中的 End marker received: False 是正常的。

预期输出​

Arduino 串口监视器:

ReSpeaker 44mm UDP Audio Test
Connecting to WiFi: Your-SSID
....
WiFi connected!
ESP32 IP: 192.168.1.42
PC destination: 192.168.1.100
UDP port: 12345
UDP initialized

Initializing I2S...
I2S initialized successfully
Sample rate: 48000 Hz
Channels: 2
Bit depth: 32-bit

================================
STARTING AUDIO TRANSMISSION
================================
Recording duration: 5 seconds
Expected audio: 1920000 bytes
Sent: 384000 / 1920000 bytes (1.00 sec)
Sent: 768000 / 1920000 bytes (2.00 sec)
Sent: 1152000 / 1920000 bytes (3.00 sec)
Sent: 1536000 / 1920000 bytes (4.00 sec)
Sent: 1920000 / 1920000 bytes (5.00 sec)

================================
TRANSMISSION COMPLETE
================================
Total audio bytes: 1920000
Successful packets: 1875
Failed packets: 0
Elapsed time: 5.02 seconds
Average data rate: 382.47 KB/s
UDP transmission finished.

Python 接收端:

======================================
ReSpeaker 44mm UDP Audio Receiver
======================================
Listening on: 0.0.0.0:12345
PC IP: 192.168.1.100
Sample rate: 48000
Channels: 2
Bit depth: 32
Expected duration: 5 seconds
Expected packets: 1875

Waiting for ESP32 audio transmission...
Received: 375 packets | 1.00 seconds
Received: 750 packets | 2.00 seconds
Received: 1125 packets | 3.00 seconds
Received: 1500 packets | 4.00 seconds
Received: 1875 packets | 5.00 seconds

Receiver timeout.

======================================
RECORDING STATISTICS
======================================
Received packets: 1875
Missing packets: 0
Duplicate packets: 0
Invalid packets: 0
End marker received: False
Total audio bytes: 1920000
Audio duration: 5.00 seconds

Saving WAV: respeaker_recording.wav
WAV saved successfully!

Receiver finished.

收听音频​

在任意音频播放器中打开 respeaker_recording.wav——例如 VLC、Windows Media Player,或使用 Audacity 进行检查。该文件为 48 kHz、立体声、32 位 PCM。

技术支持与产品讨论​

感谢您选择我们的产品!我们将为您提供多种支持,以确保您在使用我们产品时拥有尽可能顺畅的体验。我们提供多种沟通渠道,以满足不同的偏好和需求。

Loading Comments...