Skip to main content

自定义:添加自定义 AT 命令

一个在 Clip 固件中添加新 AT 命令的具体端到端演练。我们添加一个简单但真实的命令 AT+ECHO=<msg>,它会回复:

{"ok":true,"data":{"echo":"<msg>"}}\n

同样的步骤可以扩展到真正会访问配置、存储、音频或事件系统的命令。

AI 提示词​

你可以将下面的提示词复制到一个 AI 编码代理中,在固件仓库中复现同样的自定义工作流:

You are working in the reSpeaker Clip firmware repository.

Use the repository Skill before editing:
1. Read `skills/clip-dev/SKILL.md` completely and follow it for firmware AT
command development, build, flash, and validation.
2. For AT protocol work, also read the referenced BLE/AT guidance from that
Skill when needed.
3. If the new command requires a Python SDK API or CLI support, read
`skills/clip-sdk/SKILL.md` and update `sdk/` plus `docs/protocol.md`
according to that Skill.

Task:
Add a new AT command named `ECHO` to the Clip firmware.

Expected behavior:
- `AT+ECHO=hello` returns `{"ok":true,"data":{"echo":"hello"}}`
- `AT+ECHO=` returns `{"ok":false,"msg":"Missing message"}`
- `AT+ECHO` returns `{"ok":false,"msg":"Use AT+ECHO=<msg>"}`

Implementation constraints:
- Modify `applications/clip/src/at_commands.c`.
- Add a `cmd_echo_handler(struct at_cmd_ctx *ctx, char *response, size_t len)`.
- Use `create_json_response(...)` so the response format matches existing
commands.
- Register the command in `at_commands_register()` with
`AT_CMD_SET | AT_CMD_EXEC`.
- Keep the example minimal. It may use `%s` for the demo response, but document
that real free-form string commands must validate or escape JSON-sensitive
input first.
- Do not change BLE, UDP, or USB transport code unless the source proves it is
necessary.

Validation:
- Build a pristine firmware image for `clip/nrf5340/cpuapp`.
- If hardware is available, flash the image and test `AT+ECHO=hello`,
`AT+ECHO=`, and bare `AT+ECHO` over at least one transport.
- Also check representative existing commands such as `AT+GSTAT`, `AT+MODE?`,
and `AT+VERSION`.
- Report exactly what was tested and do not claim hardware validation unless it
actually ran on a device.

1. 目标​

添加 AT+ECHO=<msg>,使其:

AT+ECHO=hello     -> {"ok":true,"data":{"echo":"hello"}}
AT+ECHO= -> {"ok":false,"msg":"Missing message"}
AT+ECHO -> {"ok":false,"msg":"Use AT+ECHO=<msg>"}

它是刻意保持最小化的:一个 SET 命令,带一个简短的 EXEC 用法提示,没有副作用,可以在三种传输方式上验证。ECHO 不会与任何已注册命令冲突(参见下面 at_commands_register() 中的注册表)。

2. 当前数据流​

一行入站 AT 命令会经过以下这些层(函数名都是真实的):

transport (BLE / UDP / USB CDC)
-> at_server_submit_cmd() applications/clip/src/at_server.c
-> at_server_thread_func() dequeues from its k_msgq
-> parse_command() splits name / args / type (SET|TEST|EXEC)
-> cmd->handler(&ctx, buf, len) matched in the cmd_registry
-> create_json_response(...) builds {"ok":..,"msg":..,"data":..}
-> SEND_RESPONSE() routes the buffer back to the
transport the command arrived on

对自定义开发者来说,有两点很重要:

  • 解析是共享的。 parse_command()(at_server.c)负责 AT+NAME=args 语法以及 =、? 类型检测。你永远不需要自己解析 AT+ 前缀——你的处理函数接收到的 ctx->args 已经被拆分好了。
  • 响应是自动路由的。 at_server.c 中的 SEND_RESPONSE() 宏会根据命令的来源传输类型进行分发:TRANSPORT_TYPE_USB -> usb_cdc_send_response(),TRANSPORT_TYPE_UDP -> transport_udp_send_response(),否则 -> transport_send_to(item->transport_type, ...)。你的处理函数只需要填充响应缓冲区;它不做任何传输相关的工作,同一份 JSON 会以完全相同的形式通过 BLE、UDP 和 USB 发出。

3. 扩展点:注册模式​

下面所有内容都摘自真实源码。约定定义在 applications/clip/include/at_server.h 中。

3.1 处理函数签名​

来自 at_server.h:

typedef int (*at_cmd_handler_t)(struct at_cmd_ctx *ctx, char *response, size_t len);

你的处理函数接收到的上下文(at_server.h):

struct at_cmd_ctx {
const char *name; /* Command name (e.g., "ECHO") */
uint8_t type; /* Command type (SET/QUERY/EXEC) */
const char *args; /* Arguments string */
uint8_t transport_type; /* Transport type for response */
};

ctx->type 取值为 AT_CMD_TYPE_TEST (0)、AT_CMD_TYPE_SET (1)、AT_CMD_TYPE_EXEC (2) 之一——还有 AT_CMD_TYPE_READ (3,与 TEST 相同)。参数位于 ctx->args 中(已经越过了 =)。一个使用完全相同形状的真实处理函数是 cmd_mode_handler(at_commands.c:422):

static int cmd_mode_handler(struct at_cmd_ctx *ctx, char *response, size_t len)
{
if (ctx->type == AT_CMD_TYPE_SET) {
if (!ctx->args || strlen(ctx->args) == 0) {
return create_json_response(false, "Missing mode value", NULL, response, len);
}
/* ...validate, mutate state... */
char data[32];
snprintf(data, sizeof(data), "{\"mode\":\"%s\"}", mode_str);
return create_json_response(true, NULL, data, response, len);
} else {
/* AT+MODE? */
char data[32];
snprintf(data, sizeof(data), "{\"mode\":\"%s\"}", mode_str);
return create_json_response(true, NULL, data, response, len);
}
}

3.2 create_json_response 辅助函数​

来自 at_commands.c(每个处理函数都会使用的静态辅助函数):

static int create_json_response(bool success, const char *message,
const char *data, char *response, size_t len);

行为(从其函数体中读出):

  • 输出 {"ok":true 或 {"ok":false。
  • 如果 message 非 NULL,则追加 ,"msg":"<message>"。
  • 如果 data 非 NULL,则原样追加 ,"data":<data> —— data 必须是你自己格式化好的完整 JSON 对象(例如 {"echo":"hello"}),不能是裸值或格式化字符串。这是最常见的坑。
  • 以 }\n 结尾并返回总长度;在截断时返回 AT_ERR_NOMEM。服务器线程将 ret < 0 视为错误,并用 at_server_err_msg(-ret) 进行替换。

因此响应结构是固定的:成功 -> {"ok":true,...,"data":{...}},失败 -> {"ok":false,...,"msg":"..."}。没有数字错误码,也没有 error 字段(参见 protocol.md)。

3.3 命令结构体与注册​

来自 at_server.h:

struct at_command {
const char *name; /* Command name */
uint8_t flags; /* Supported operations */
at_cmd_handler_t handler; /* Command handler */
};

标志位(位掩码;at_server.h):

#define AT_CMD_SET    (1 << 0)  /* Supports AT+CMD=... */
#define AT_CMD_QUERY (1 << 1) /* Supports AT+CMD? */
#define AT_CMD_EXEC (1 << 2) /* Supports AT+CMD */

注册(at_server.c)——注意注册表最多只能容纳 32 个命令:

int at_server_register_cmd(const struct at_command *cmd);

一个真实的注册代码块,与 at_commands.c:1769 中完全一致:

/* GSTAT - Get device status */
static const struct at_command gstat_cmd = {
.name = "GSTAT",
.flags = AT_CMD_EXEC,
.handler = cmd_gstat_handler,
};
err = at_server_register_cmd(&gstat_cmd);
if (err) return err;

4. 需要修改的文件​

只有一个源文件:applications/clip/src/at_commands.c。

4.1 添加处理函数​

把它放在其他 static int cmd_*_handler(...) 定义之间(现有处理函数位于 at_commands_register() 之上)。以 cmd_mode_handler 为模板:

/* ECHO Command Handler - customization example.
* AT+ECHO=<msg> -> {"ok":true,"data":{"echo":"<msg>"}} */
static int cmd_echo_handler(struct at_cmd_ctx *ctx, char *response, size_t len)
{
if (ctx->type != AT_CMD_TYPE_SET) {
return create_json_response(false, "Use AT+ECHO=<msg>", NULL, response, len);
}
if (!ctx->args || strlen(ctx->args) == 0) {
return create_json_response(false, "Missing message", NULL, response, len);
}

char data[160];
int n = snprintf(data, sizeof(data), "{\"echo\":\"%s\"}", ctx->args);
if (n < 0 || n >= (int)sizeof(data)) {
return AT_ERR_NOMEM;
}
return create_json_response(true, NULL, data, response, len);
}

针对真实命令的注意事项: ctx->args 是原始用户输入。像这个简单示例那样用 %s 进行插值,会让消息中的 " 破坏 JSON。对于任何接受自由文本字符串的命令,都要先校验/转义输入。已发布的使用 %s 的命令(例如 MODE、LOG)只会针对它们已经检查过的固定枚举值这样做。

4.2 注册它​

在 at_commands_register(void)(at_commands.c:1761)内部——这是唯一一个注册所有命令的初始化函数,它本身只会从 main.c 中被调用一次(main.c:286 的 at_commands_register())。把该代码块与其他命令一起添加(例如紧跟在 at_commands.c:2030 附近的 LOG 代码块之后):

/* ECHO - echo a message back (customization example) */
static const struct at_command echo_cmd = {
.name = "ECHO",
.flags = AT_CMD_SET | AT_CMD_EXEC,
.handler = cmd_echo_handler,
};
err = at_server_register_cmd(&echo_cmd);
if (err) return err;

需要 AT_CMD_EXEC,因为处理函数在裸 AT+ECHO 时会有意返回一个友好的用法提示。如果注册时只使用 AT_CMD_SET,分发器会在处理函数运行前就拒绝 AT+ECHO。由于服务器会自动路由响应(第 2 节),因此不需要对 BLE/UDP/USB 代码做任何修改。

5. 兼容性影响​

添加命令是增量式的——现有命令及其 JSON 结构保持不变。请保持响应约定不变:

  • 成功:{"ok":true,"data":{...}}
  • 失败:{"ok":false,"msg":"..."}
  • 没有数字错误码、没有请求 ID、没有 error 字段。(参见 protocol.md。)

如果新命令也需要通过主机工具访问,你需要的是Python SDK 一致性,而不仅仅是固件。根据 skills/clip-sdk/ 规则,在修改 SDK 之前先阅读当前的 at_commands.c 注册内容,并将 docs/protocol.md 加上固件源码视为协议契约——当固件契约发生变化时,同时更新 SDK(位于 sdk/)和 protocol.md。不要模拟已移除的旧版命令(BITRATE、COMPLEXITY、NOISE、AGC、DEREVERB、PURGE)。

6. 构建​

加载 NCS v3.3.0 环境,将模块路径设置为环境变量(Kconfig 发现阶段在 CMake 之前运行),然后进行构建:

source ~/ncs/v3.3.0/zephyr/zephyr-env.sh
export ZEPHYR_EXTRA_MODULES=$(pwd)

west build --build-dir build-clip --pristine --board clip/nrf5340/cpuapp applications/clip

根据 CLAUDE.md,项目构建时必须零警告——在提交之前修复任何编译器警告。(上面的处理程序不会引入任何警告。)

7. 设备端验证​

烧录(注意:west flash --reset 在此开发板上无效——需要单独复位):

west flash --build-dir build-clip && nrfutil device reset
minicom -D /dev/ttyACM0 -b 921600

然后在每种传输方式上测试该命令,并确认 JSON 完全一致:

BLE(交互式 shell——clip-cli.py terminal 会通过 BLE 打开一个 AT 提示符):

python applications/clip/tests/tools/clip-cli.py terminal
# at the prompt:
AT+ECHO=hello -> {"ok":true,"data":{"echo":"hello"}}
AT+ECHO -> {"ok":false,"msg":"Use AT+ECHO=<msg>"}
AT+ECHO= -> {"ok":false,"msg":"Missing message"}

UDP(WiFi AP 模式——先通过 BLE 发送 AT+WIFI=on,然后加入返回的 SSID/密码,并以 192.168.4.1:8089 为目标):

python applications/clip/tests/tools/udp_terminal.py
AT+ECHO=hello

USB CDC(打开 CDC-ACM 串口;必须先通过 BLE 发送 AT+USB=on 启用 USB,或者在插入时按住用户按键):

AT+ECHO=hello

三个通道上的响应字符串必须逐字节完全一致。同时确认现有命令没有回退——例如 AT+GSTAT、AT+MODE?、AT+VERSION。

8. 恢复​

如果新构建行为异常,可通过 USB 串口 DFU 恢复(1200 波特触发进入 MCUboot 恢复模式,PID 为 0x8069)、BLE OTA 或编程器——参见 usb_dfu.md。引导加载程序分区不会被应用 OTA 覆盖;其签名由 MCUboot 验证。

相关文档​

技术支持与产品讨论​

感谢您选择我们的产品!我们将为您提供多种支持,确保您在使用我们产品的过程中尽可能顺畅。我们提供多种沟通渠道,以满足不同的偏好和需求。

Loading Comments...