Skip to main content

使用 Xiao ESP32S3 通过 MQTT 传输 reSpeaker Flex 音频流

概述​

本项目演示如何将嵌入 XIAO ESP32S3 开发板的 reSpeaker Flex 麦克风阵列采集到的音频进行流式传输,并以 .wav 文件的形式发送到 MQTT broker。音频通过 I2S 采集,编码为 WAV 格式,并通过 MQTT 发布。

reSpeaker Flex XVF3800 线性阵列搭配 XIAO ESP32S3 reSpeaker Flex XVF3800 环形阵列搭配 XIAO ESP32S3

库​

Arduino MQTT Client

功能概览​

此示例程序将完成以下工作:

  • 连接到指定的 WiFi 网络。
  • 连接到 MQTT broker(例如 test.mosquitto.org)。
  • 使用 I2S 从搭配 XIAO ESP32S3 的 reSpeaker Flex XVF3800 采集实时音频
  • 将音频编码为 WAV 格式。
  • 将音频作为单条 MQTT 消息发布。
  • 使用 poll() 保持 MQTT 连接处于活动状态。

Arduino 代码​

在上传前请先更新以下字段:

const char* ssid = "your-SSID";
const char* password = "your-WIFI-password";
const char* broker = "test.mosquitto.org";
const char* topic = "flex/audio.wav";
int port = 1883;

完整代码(约传输 3 秒音频)​

#include "WiFi.h"                // For WiFi connectivity
#include "ArduinoMqttClient.h" // For MQTT communication
#include "AudioTools.h" // For handling I2S audio and WAV encoding

// Define how much audio data to send
#define MQTT_PACKET_SIZE 1024 // Size of each MQTT data packet (in bytes)
#define NUM_PACKETS 375 // Number of packets to send (~3 seconds of audio at 16kHz)

// WiFi network credentials
const char* ssid = "your-SSID"; // Replace with your WiFi SSID
const char* password = "your-WIFI-password"; // Replace with your WiFi password

// MQTT broker configuration
const char* broker = "test.mosquitto.org"; // Public test MQTT broker
const char* topic = "flex/audio.wav"; // Topic to publish audio to
int port = 1883; // Standard MQTT port

// Create MQTT and WiFi clients
WiFiClient wifiClient;
MqttClient mqttClient(wifiClient);

// Configure audio: 16kHz sample rate, stereo (2 channels), 32-bit per sample
AudioInfo info(16000, 2, 32);
I2SStream i2s_in; // I2S audio input stream
I2SConfig i2s_config; // I2S hardware configuration

// Stream that encodes audio in WAV format and sends it via MQTT
EncodedAudioStream out_stream(&mqttClient, new WAVEncoder());
StreamCopy copier(out_stream, i2s_in, MQTT_PACKET_SIZE); // Handles copying I2S data into the MQTT stream

// Connect to WiFi network
void connectWiFi() {
Serial.printf("Connecting to WiFi: %s\n", ssid);
WiFi.begin(ssid, password); // Start WiFi connection
while (WiFi.status() != WL_CONNECTED) { // Wait until connected
Serial.print(".");
delay(1000);
}
Serial.println("\nConnected to WiFi!");
}

// Connect to MQTT broker
void connectMQTT() {
mqttClient.setId("xvf3800_stream"); // Set MQTT client ID
Serial.printf("Connecting to MQTT broker: %s\n", broker);

if (!mqttClient.connect(broker, port)) { // Try to connect to MQTT
Serial.print("MQTT connection failed! Code: ");
Serial.println(mqttClient.connectError());
while (true); // Stop here if connection fails
}

Serial.println("Connected to MQTT broker!");
}

// Set up I2S audio input configuration
void setupI2SInput() {
i2s_config = i2s_in.defaultConfig(RX_MODE); // Set RX mode for audio input
i2s_config.copyFrom(info); // Apply audio format to config

// Assign correct GPIO pins for XVF3800
i2s_config.pin_bck = 8; // Bit clock
i2s_config.pin_ws = 7; // Word select (LR clock)
i2s_config.pin_data = 44; // Not used for RX, but required by lib
i2s_config.pin_data_rx = 43; // Data input pin from XVF3800
i2s_config.is_master = false; // XVF3800 provides clock, so this board acts as slave

i2s_in.begin(i2s_config); // Initialize I2S input with given config
Serial.println("I2S input started.");
}

void setup() {
Serial.begin(115200); // Start serial monitor
AudioLogger::instance().begin(Serial, AudioLogger::Info); // Enable audio debug logs

connectWiFi(); // Connect to WiFi
connectMQTT(); // Connect to MQTT
setupI2SInput(); // Configure and start I2S audio input

out_stream.begin(info); // Initialize WAV encoder with audio format

// Start a new MQTT message and reserve enough space for the full audio stream
mqttClient.beginMessage(topic, MQTT_PACKET_SIZE * NUM_PACKETS, true);

// Copy audio from microphone (I2S) into MQTT stream
copier.copyN(NUM_PACKETS); // Copies a fixed number of packets (3 seconds of audio)

mqttClient.endMessage(); // Finalize the MQTT message and send it
Serial.println("Audio stream sent via MQTT!");
}

void loop() {
mqttClient.poll(); // Keep MQTT connection alive (important if broker expects pings)
delay(5000); // Optional delay, useful if recording repeatedly
}

使用串口监视器(115200 波特率)确认连接和流式传输状态。

pir

Python 脚本(用于接收并保存音频)​

import paho.mqtt.client as mqtt

broker = "test.mosquitto.org"
port = 1883
topic = "flex/audio.wav"
output_file = "output.wav"
audio_data = bytearray()

def on_message(client, userdata, msg):
global audio_data
print("🔊 Received audio message")
audio_data.extend(msg.payload)

with open(output_file, "wb") as f:
f.write(audio_data)
print(f"✅ WAV file saved as: {output_file}")

client = mqtt.Client()
client.on_message = on_message

print(f"Connecting to MQTT broker {broker}...")
client.connect(broker, port, 60)

client.subscribe(topic)
print(f"📡 Subscribed to: {topic}")
client.loop_forever()

收听音频​

文件保存完成后(output.wav),只需使用任意音频播放器打开,例如:

  • VLC
  • Windows Media Player
  • Audacity(用于分析)

技术支持与产品讨论​

感谢您选择我们的产品!我们将为您提供多种支持,确保您在使用我们产品的过程中体验顺畅。我们提供多种沟通渠道,以满足不同的偏好和需求。

Loading Comments...