Seeed Studio XIAO MG24 引脚复用

XIAO MG24 具有多达 22 个常规引脚、18 个模拟引脚、18 个数字引脚、2 个 SPI、2 个 UART、2 个 I2C,并支持 所有 PWM。它提供了丰富多样的引脚供我们使用。在本教程中,我将教您如何驱动这些引脚,使我们能够有效地利用它们 😀!
数字引脚
硬件准备
| Seeed Studio XIAO MG24 Sense | Seeed Studio XIAO 扩展板配 Grove OLED | Grove - 继电器 |
|---|---|---|
![]() | ![]() | ![]() |
请将 XIAO MG24(Sense) 安装到扩展板上,并通过 Grove 线缆将继电器连接到扩展板的 A0/D0 接口。最后,通过 USB-C 线缆将 XIAO 连接到计算机。
软件实现
在这个示例中,我们将使用连接到 XIAO 扩展板的按钮来控制继电器的开关状态。当按钮被按下时,继电器打开;当按钮被释放时,继电器关闭。
const int buttonPin = D1; // the number of the pushbutton pin
int buttonState = 0; // variable for reading the pushbutton status
const int relayPin = D0;
void setup() {
// initialize the Relay pin as an output:
pinMode(relayPin, OUTPUT);
// initialize the pushbutton pin as an input:
pinMode(buttonPin, INPUT_PULLUP);
}
void loop() {
// read the state of the pushbutton value:
buttonState = digitalRead(buttonPin);
// check if the pushbutton is pressed. If it is, the buttonState is HIGH:
if (buttonState == HIGH) {
// turn Relay on:
digitalWrite(relayPin, HIGH);
} else {
// turn Relay off:
digitalWrite(relayPin, LOW);
}
}
结果图
如果一切顺利,上传程序后,您应该看到以下效果。

数字引脚作为PWM
XIAO MG24(Sense)上的所有GPIO引脚都支持PWM输出。因此,您可以使用任何引脚输出PWM来调节灯光亮度、控制舵机和其他功能。
硬件准备
| Seeed Studio XIAO MG24 Sense | Seeed Studio XIAO扩展板配Grove OLED | Grove - 可变色LED |
|---|---|---|
![]() | ![]() | ![]() |
请将XIAO MG24(Sense)安装到扩展板上,然后使用Grove线缆将可变色LED连接到扩展板的A0/D0接口。最后,通过USB-C线缆将XIAO连接到您的计算机。
软件实现
在这个示例中,我们将演示如何使用PWM输出来控制灯光的亮度。
int LED_pin = D0; // LED connected to digital pin 10
void setup() {
// declaring LED pin as output
pinMode(LED_pin, OUTPUT);
}
void loop() {
// fade in from min to max in increments of 5 points:
for (int fadeValue = 0 ; fadeValue <= 255; fadeValue += 3) {
// sets the value (range from 0 to 255):
analogWrite(LED_pin, fadeValue);
// wait for 30 milliseconds to see the dimming effect
delay(30);
}
// fade out from max to min in increments of 5 points:
for (int fadeValue = 255 ; fadeValue >= 0; fadeValue -= 3) {
// sets the value (range from 0 to 255):
analogWrite(LED_pin, fadeValue);
// wait for 30 milliseconds to see the dimming effect
delay(30);
}
}
结果图
如果程序运行成功,您将看到以下运行效果。

模拟
XIAO MG24(Sense) 开发板具有 12 位 ADC,可高分辨率读取模拟传感器值,它可以帮助我们读取更准确的值。
接下来,我们将选择两个传感器来体现 ADC 的特性。
硬件准备
| Seeed Studio XIAO MG24 Sense | Grove-可变色 LED | Grove-旋转角度传感器 | Seeed Studio Grove Base for XIAO |
|---|---|---|---|
![]() | ![]() | ![]() | ![]() |
软件实现
- analogRead 不使用 DMA
- analogRead With DMA
const int analogInPin = D1; // Analog input pin that the potentiometer is attached to
const int analogOutPin = 9; // Analog output pin that the LED is attached to
int sensorValue = 0; // value read from the pot
int outputValue = 0; // value output to the PWM (analog out)
void setup() {
Serial.begin(115200);
}
void loop() {
sensorValue = analogRead(analogInPin);
outputValue = map(sensorValue, 0, 4095, 0, 255);
analogWrite(analogOutPin, outputValue);
Serial.print("sensor = ");
Serial.print(sensorValue);
Serial.print("\t output = ");
Serial.println(outputValue);
delay(100);
}
#define ANALOG_VALUE_MIN 0 // Define the minimum analog value
#define ANALOG_VALUE_MAX 4095 // Define the maximum analog value for 12-bit ADC
#define NUM_SAMPLES 128 // Define the number of samples to collect each time
const int analogInPin = D1; // Analog input pin that the potentiometer is attached to
const int analogOutPin = LED_BUILTIN; // Analog output pin that the LED is attached to
// Buffers for storing samples
uint32_t analog_buffer[NUM_SAMPLES]; // Global buffer to store sampled values
uint32_t analog_buffer_local[NUM_SAMPLES]; // Local buffer to store sampled values for calculations
volatile bool data_ready_flag = false; // Data ready flag indicating new sample data is available
void analog_samples_ready_cb(); // Callback function called when samples are ready
void calculate_and_display_analog_level(); // Function to calculate and display the analog level
float getAverage(uint32_t *buffer, uint32_t buf_size); // Function to compute the average of the given buffer
void setup() {
Serial.begin(115200);
pinMode(analogOutPin, OUTPUT);
// Start DMA sampling, storing samples in analog_buffer, with callback on completion
analogReadDMA(analogInPin, analog_buffer, NUM_SAMPLES, analog_samples_ready_cb);
Serial.println("Sampling started...");
}
void loop() {
// If data is ready, process it
if (data_ready_flag) {
data_ready_flag = false;
calculate_and_display_analog_level();
}
}
void analog_samples_ready_cb() {
// Copy data to the local buffer in order to prevent it from overwriting
memcpy(analog_buffer_local, analog_buffer, NUM_SAMPLES * sizeof(uint32_t));
data_ready_flag = true;
}
void calculate_and_display_analog_level() {
// Rolling average for smoothing the analog level
static uint32_t rolling_average = 0u;
// Stop sampling in order to prevent overwriting the current data
ADC.scan_stop();
// Get the average of the sampled values
uint32_t analog_level = (uint32_t)getAverage(analog_buffer_local, NUM_SAMPLES);
// Adjust the analog level
analog_level = constrain(analog_level, ANALOG_VALUE_MIN, ANALOG_VALUE_MAX);
// Calculate the rolling average
rolling_average = (analog_level + rolling_average) / 2;
// Map the current average level to brightness
int brightness = map(rolling_average, ANALOG_VALUE_MIN, ANALOG_VALUE_MAX, 0, 255);
if (LED_BUILTIN_ACTIVE == LOW) {
analogWrite(analogOutPin, 255 - brightness);
} else {
analogWrite(analogOutPin, brightness);
}
// Print the average analog level and brightness output
Serial.print("sensor = ");
Serial.print(rolling_average);
Serial.print("\t output = ");
Serial.println(brightness);
// Restart sampling
analogReadDMA(analogInPin, analog_buffer, NUM_SAMPLES, analog_samples_ready_cb);
}
// Gets the average value of the provided samples
float getAverage(uint32_t *buffer, uint32_t buf_size) {
if (!buffer) {
return 0.0f;
}
float sum = 0.0f;
for (uint32_t i = 0u; i < buf_size; i++) {
sum += buffer[i];
}
return sum / buf_size;
}
需要注意的是,如果您想使用 DMA 读取模拟信号,您的库版本需要大于 2.2.0。目前,新版本尚未获得批准,您需要手动安装。
结果图
如果一切顺利,上传程序后,您应该看到以下效果。

UART
在使用 Arduino IDE 时,串行通信是许多项目的重要组成部分。要在 Arduino IDE 中使用串行通信,您需要首先打开串行监视器窗口。这可以通过点击工具栏中的串行监视器图标或按Ctrl+Shift+M快捷键来完成。
通用串行使用
一些常用的串行函数包括:
Serial.begin()-- 以指定的波特率初始化通信;Serial.print()-- 以可读格式向串行端口发送数据;Serial.write()-- 向串行端口发送二进制数据;Serial.available()-- 检查串行端口是否有可读取的数据;Serial.read()-- 从串行端口读取单个字节的数据;Serial.flush()-- 等待传出串行数据的传输完成。
通过使用这些串行函数,您可以在 Arduino 板和计算机之间发送和接收数据,这为创建交互式项目开辟了许多可能性。
以下是一个示例程序:
void setup() {
// initialize serial communication at 9600 bits per second:
Serial.begin(9600);
}
void loop() {
// send data to the serial port
Serial.println("Hello World!");
// read data from the serial port
if (Serial.available() > 0) {
// read the incoming byte:
char incomingByte = Serial.read();
// print the incoming byte to the serial monitor:
Serial.print("I received: ");
Serial.println(incomingByte);
}
// wait for a second before repeating the loop
delay(1000);
}
Serial1 的使用
根据上述 XIAO MG24(Sense) 引脚图的具体参数,我们可以观察到有 TX 引脚和 RX 引脚。 这与串行通信不同,但用法也非常相似,只是需要添加一些参数。 因此接下来,我们将使用芯片引出的引脚进行串行通信。
#define BAUD 115200
void setup() {
Serial1.begin(BAUD);
}
void loop() {
if(Serial1.available() > 0)
{
char incominByte = Serial1.read();
Serial1.print("I received : ");
Serial1.println(incominByte);
}
delay(1000);
}
I2C
XIAO MG24(Sense) 具有 I2C 接口,可用于许多传感器的数据传输和解析,以及使用一些 OLED 屏幕。
硬件准备
| Seeed Studio XIAO MG24 Sense | Seeed Studio XIAO 扩展底板配 Grove OLED |
|---|---|
![]() | ![]() |
扩展板上的OLED显示屏使用I2C协议,通过板上的I2C电路连接到XIAO的I2C接口。因此,我们可以直接将XIAO插入扩展板并对其进行编程,以在屏幕上显示内容。
软件实现
本示例介绍如何使用Seeed Studio Expansion Base for XIAO MG24(Sense)上的OLED显示屏。
步骤1. 将Seeed Studio XIAO MG24(Sense)安装到扩展板上,然后连接Type-C线缆。
步骤2. 安装u8g2库。
步骤3. 复制代码并粘贴到Arduino IDE中,然后上传。
- 下载下面的zip文件
📄 [ZIP] smiley_face Header
- 创建一个名为"smiley_face.h"的头文件,并将下载的zip文件内容复制到您创建的头文件中

#include <Arduino.h>
#include <U8g2lib.h>
#include <Wire.h>
#include "smiley_face.h"
U8G2_SSD1306_128X64_NONAME_F_HW_I2C u8g2(U8G2_R0, /* reset=*/ U8X8_PIN_NONE);
int xx = 20;
int yy = 10;
void setup() {
u8g2.begin();
}
void loop() {
smeil_display();
delay(500);
}
void smeil_display() {
const unsigned char* smileImages[] = {
semil1, semil2, semil3, semil4, semil5,
semil6, semil7, semil8, semil9, semil10,
semil11, semil12, semil13, semil14, semil15,
semil16, semil17, semil18, semil19, semil20,
semil21, semil22, semil23, semil24, semil25,
semil26, semil27
};
int delays[] = {
40, 50, 40, 40, 40,
40, 40, 50, 40, 40,
40, 40, 40, 50, 40,
40, 50, 40, 40, 50,
40, 50, 40, 40, 50,
50, 50, 40, 50
};
for (int i = 0; i < sizeof(smileImages) / sizeof(smileImages[0]); i++) {
u8g2.firstPage();
do {
u8g2.drawXBMP(xx, yy, 48, 48, smileImages[i]);
} while (u8g2.nextPage());
delay(delays[i]);
}
}
结果图

SPI
XIAO MG24(Sense) 芯片集成了多个外设,包括一个 SPI 接口,可用于连接外部 SPI 设备,如闪存、显示器、传感器等。
Arduino 库概述
基于 Waveshare 提供的 Arduino 示例程序,我们编写了一个适用于整个 XIAO 系列的 Arduino 库,您可以通过下面的按钮直接访问该库的 Github 页面。
硬件准备
引脚连接
按照上述方法准备好硬件后,使用跳线将 XIAO 和 OLED 的 SPI 接口连接起来。请参考以下图表进行接线。

安装
由于您已经下载了 zip 库文件,请打开您的 Arduino IDE,点击 Sketch > Include Library > Add .ZIP Library。选择您刚刚下载的 zip 文件,如果库安装正确,您将在通知窗口中看到 Library added to your libraries。这意味着库已成功安装。

软件实现
正确下载并安装库后,您可以在示例文件夹中找到两个名为 helloworld.ino 和 bgcolor.ino 的示例程序。bgcolor.ino 是一个显示背景颜色的示例,我们默认设置为红色。而 helloworld.ino 是一个显示我们公司徽标动画的示例,这个示例包含了 bgcolor 示例所具有的效果。
#include <st7789v2.h>
#include "SPI.h"
#include "seeed.h"
st7789v2 Display;
void setup() {
// put your setup code here, to run once:
Display.SetRotate(270);
Display.Init();
Display.SetBacklight(100);
Display.Clear(WHITE);
}
void loop() {
// put your main code here, to run repeatedly:
// Display.SetPixel(100, 100, RED);
// Display.DrawPoint(50, 50, YELLOW, DOT_PIXEL_8X8, DOT_FILL_AROUND);
Display.DrawImage(gImage_seeed, 20, 90, 240, 47);
Display.DrawLine(15, 65, 65, 65, MAGENTA, DOT_PIXEL_2X2, LINE_STYLE_SOLID);
Display.DrawLine(15, 70, 80, 70, MAGENTA, DOT_PIXEL_2X2, LINE_STYLE_SOLID);
Display.DrawRectangle(15, 80, 265, 150, GRAY, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(10, 10, 25, BLUE, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(10, 10, 20, BLACK, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(10, 10, 15, RED, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(10, 10, 10, GREEN, DOT_PIXEL_2X2, DRAW_FILL_FULL);
Display.DrawCircle(270, 10, 25, BLUE, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(270, 10, 20, BLACK, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(270, 10, 15, RED, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(270, 10, 10, GREEN, DOT_PIXEL_2X2, DRAW_FILL_FULL);
Display.DrawCircle(10, 230, 25, BLUE, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(10, 230, 20, BLACK, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(10, 230, 15, RED, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(10, 230, 10, GREEN, DOT_PIXEL_2X2, DRAW_FILL_FULL);
Display.DrawCircle(270, 230, 25, BLUE, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(270, 230, 20, BLACK, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(270, 230, 15, RED, DOT_PIXEL_2X2, DRAW_FILL_EMPTY);
Display.DrawCircle(270, 230, 10, GREEN, DOT_PIXEL_2X2, DRAW_FILL_FULL);
Display.DrawLine(200, 160, 265, 160, GRAYBLUE, DOT_PIXEL_2X2, LINE_STYLE_SOLID);
Display.DrawLine(215, 165, 265, 165, GRAYBLUE, DOT_PIXEL_2X2, LINE_STYLE_SOLID);
Display.DrawString_EN(20, 180, "By: Jason", &Font20, WHITE, BLACK);
// Display.DrawNum(100, 220, 123456, &Font24, RED, BRED);
Display.DrawFloatNum(100, 210, 1.00, 2, &Font16, WHITE, BLACK);
}
您会发现 Seeed Studio 的标志在显示屏上动态打印。

完成
您已经学习了 XIAO MG24 (Sense) 引脚的基本功能。现在,让我们进一步探索内置传感器。

技术支持与产品讨论
感谢您选择我们的产品!我们在这里为您提供不同的支持,以确保您使用我们产品的体验尽可能顺畅。我们提供多种沟通渠道,以满足不同的偏好和需求。