Control 6/7 DOF Robot Arm using NVIDIA Isaac GR00T N1.5
Introduction
This article demonstrates how NVIDIA's GR00T AI platform enables advanced, autonomous control of StarAI Robotic Arm. Combining real-time perception and adaptive decision-making, GR00T bridges AI and robotics for precision tasks in industrial and research applications.
Prerequisites
- StarAI Robotic Arm
- Orbbec Gemini 2
- NVIDIA GPU-accelerated Linux host
- ubuntu 20.04
- VRAM >32GB
While this demonstration uses StarAI + Gemini2, the tutorial remains fully applicable to SOArm 100 + standard USB cameras.
Getting Started
Setup Lerobot Env
The StarAI robotic arm can be driven using the lerobot project. Please refer to this wiki to configure your StarAI robotic arm operating environment. Once everything is ready, you can control the Follow Arm using the command below.
python lerobot/scripts/control_robot.py \
--robot.type=starai \
--robot.cameras='{}' \
--control.type=teleoperate
The program's runtime effect will be similar to the video below.
Setup Orbbec Camera SDK
Step1. 1.Clone OrbbecSDK.
cd ~/
git clone https://github.com/orbbec/pyorbbecsdk.git
cd pyorbbecsdk
Step2. 2.Install dependencies and compile pyOrbbecsdk.
conda activate lerobot
sudo apt-get install python3-dev python3-venv python3-pip python3-opencv
pip3 install -r requirements.txt
mkdir build
cd build
cmake -Dpybind11_DIR=`pybind11-config --cmakedir` ..
make -j4
make install
cd ~/pyorbbecsdk
pip install -e .
Setp3. Test if the depth camera works properly.
cd ~/pyorbbecsdk
pip install -e .
export PYTHONPATH=$PYTHONPATH:~/pyorbbecsdk/install/lib/
sudo bash ./scripts/install_udev_rules.sh
sudo udevadm control --reload-rules && sudo udevadm trigger
python3 examples/depth.py
If everything goes well, the depth information captured by the depth camera will be printed on the desktop.

Record the Dataset
We can run the following script to collect a new dataset:
python lerobot/scripts/control_robot.py \
--robot.type=so101 \
--control.type=record \
--control.fps=30 \
--control.single_task="Grasp a green block and put it in the bin." \
--control.repo_id=${HF_USER}/starai_test \
--control.tags='["starai","lerobot","tutorial"]' \
--control.warmup_time_s=5 \
--control.episode_time_s=30 \
--control.reset_time_s=30 \
--control.num_episodes=100 \
--control.display_data=true \
--control.push_to_hub=true
For training Isaac-GR00T, it is recommended to collect at least 50 data samples.
Here is the dataset we collected.
https://huggingface.co/datasets/youjiang97/starai02

Since we will be using the Isaac-GR00T project for model training, we need to add a dataset conversion configuration parameter to the dataset in accordance with the project's requirements. Specifically, this involves creating a file named modality.json in the meta folder with the following content:
{
"state": {
"single_arm": {
"start": 0,
"end": 6
},
"gripper": {
"start": 6,
"end": 7
}
},
"action": {
"single_arm": {
"start": 0,
"end": 6
},
"gripper": {
"start": 6,
"end": 7
}
},
"video": {
"webcam": {
"original_key": "observation.images.webcam"
}
},
"annotation": {
"human.task_description": {
"original_key": "task_index"
}
}
}
If you are using SOARM100 for testing, set the servo IDs of a single robotic arm to 0-5 and the gripper ID to 5-6.
Adjust the video parameters based on the camera naming convention in the dataset.
The organized dataset file structure is as follows:
├── data
│ └── chunk-000
│ ├── episode_000000.parquet
│ ├── ....
│ ├── episode_000099.parquet
│ └── episode_000100.parquet
├── meta
│ ├── episodes.jsonl
│ ├── episodes_stats.jsonl
│ ├── modality.json
│ ├── info.json
│ ├── so100__modality.json
│ ├── stats.json
│ └── tasks.jsonl
└── videos
└── chunk-000
├── observation.images.Orbbec
│ ├── episode_000000.mp4
│ ├── ....
│ ├── episode_000099.mp4
│ └── episode_000100.mp4
└── observation.images.laptop
├── episode_000000.mp4
├── ....
├── episode_000099.mp4
└── episode_000100.mp4
Setup Isaac-GR00T Env
First, we need to clone the Isaac-GR00T code repository:
git clone https://github.com/NVIDIA/Isaac-GR00T
cd Isaac-GR00T
Next, set up a Python runtime environment according to the project requirements:
conda create -n gr00t python=3.10
conda activate gr00t
pip install --upgrade setuptools
pip install -e .[base]
pip install --no-build-isolation flash-attn==2.7.1.post4
The installation of flash-attn involves package compilation, which can be extremely slow. It is recommended to download the precompiled package version matching your system environment and install it locally using the command: pip install ./<package_name>
Fine-tuning the Model
Now we can use the prepared dataset to fine-tune the GR00T N1.5 3B VLM model. NVIDIA has provided a dedicated Python script for fine-tuning—simply run the following command in your terminal:
python scripts/gr00t_finetune.py \
--dataset-path ~/Isaac-GR00T/demo_data/starai_test
--num-gpus 1
--output-dir ~/Isaac-GR00T/output_starai
--max-steps 20000
--data-config so100
--video-backend torchvision_av

You need to modify the dataset storage path according to your actual setup.
The training process requires approximately 33GB of GPU memory. If your local hardware has insufficient VRAM, consider using cloud computing resources to complete the training.
Deployment
The deployment architecture of Isaac-GR00T adopts a decoupled design between the inference endpoint and control endpoint:
- Inference Endpoint (Server): Dedicated solely to executing model inference tasks.
- Control Endpoint (Client): Responsible for acquiring robotic arm states and orchestrating motion control.
Server
python scripts/inference_service.py --server \
--model_path <PATH_TO_YOUR_CHECKPOINT> \
--embodiment-tag new_embodiment \
--data-config so100 \
--denoising-steps 4

Client
python getting_started/examples/eval_gr00t_so100.py --use_policy
If everything proceeds smoothly, Isaac-GR00T should now be controlling your robotic arm.
Since we are using a StarAI robotic arm, minor modifications to the client-side code are required to ensure compatibility with the new arm and camera. The updated code is as follows: eval_gr00t_so100.py
# SPDX-FileCopyrightText: Copyright (c) 2025 NVIDIA CORPORATION & AFFILIATES. All rights reserved.
# SPDX-License-Identifier: Apache-2.0
#
# Licensed under the Apache License, Version 2.0 (the "License");
# you may not use this file except in compliance with the License.
# You may obtain a copy of the License at
#
# http://www.apache.org/licenses/LICENSE-2.0
#
# Unless required by applicable law or agreed to in writing, software
# distributed under the License is distributed on an "AS IS" BASIS,
# WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
# See the License for the specific language governing permissions and
# limitations under the License.
# SO100 Real Robot
import time
from contextlib import contextmanager
import cv2
import matplotlib.pyplot as plt
import numpy as np
import torch
from lerobot.common.datasets.lerobot_dataset import LeRobotDataset
from lerobot.common.robot_devices.cameras.configs import OpenCVCameraConfig, OrbbecCameraConfig
from lerobot.common.robot_devices.motors.dynamixel import TorqueMode
from lerobot.common.robot_devices.robots.configs import So100RobotConfig, StaraiRobotConfig
from lerobot.common.robot_devices.robots.utils import make_robot_from_config
from lerobot.common.robot_devices.utils import RobotDeviceAlreadyConnectedError
# NOTE:
# Sometimes we would like to abstract different env, or run this on a separate machine
# User can just move this single python class method gr00t/eval/service.py
# to their code or do the following line below
import sys
import os
sys.path.append(os.path.expanduser("~/Isaac-GR00T/gr00t/eval/"))
from service import ExternalRobotInferenceClient
# Import tqdm for progress bar
from tqdm import tqdm
#################################################################################
class SO100Robot:
def __init__(self, calibrate=False, enable_camera=False, cam_idx=9):
# self.config = So100RobotConfig()
self.config = StaraiRobotConfig()
self.calibrate = calibrate
self.enable_camera = enable_camera
self.cam_idx = cam_idx
if not enable_camera:
self.config.cameras = {}
else:
# self.config.cameras = {"webcam": OpenCVCameraConfig(cam_idx, 30, 640, 480, "bgr")}
self.config.cameras = {"webcam": OrbbecCameraConfig(fps=30,use_depth=True,width = 640,Hi_resolution_mode = False)}
self.config.leader_arms = {}
# remove the .cache/calibration/so100 folder
if self.calibrate:
import os
import shutil
calibration_folder = os.path.join(os.getcwd(), ".cache", "calibration", "so100")
print("========> Deleting calibration_folder:", calibration_folder)
if os.path.exists(calibration_folder):
shutil.rmtree(calibration_folder)
# Create the robot
self.robot = make_robot_from_config(self.config)
print("<<<<<<<<<<<<<<<>>>>>>>>>>>>>>>>>>>")
print(self.robot.robot_type)
print("<<<<<<<<<<<<<<<>>>>>>>>>>>>>>>>>>>")
self.motor_bus = self.robot.follower_arms["main"]
@contextmanager
def activate(self):
try:
self.connect()
# self.move_to_initial_pose()
yield
finally:
self.disconnect()
def connect(self):
if self.robot.is_connected:
raise RobotDeviceAlreadyConnectedError(
"ManipulatorRobot is already connected. Do not run `robot.connect()` twice."
)
# Connect the arms
self.motor_bus.connect()
# We assume that at connection time, arms are in a rest position, and torque can
# be safely disabled to run calibration and/or set robot preset configurations.
self.motor_bus.write("Torque_Enable", TorqueMode.DISABLED.value)
# Calibrate the robot
# self.robot.activate_calibration()
# self.set_so100_robot_preset()
# Enable torque on all motors of the follower arms
self.motor_bus.write("Torque_Enable", TorqueMode.ENABLED.value)
print("robot present position:", self.motor_bus.read("Present_Position"))
self.robot.is_connected = True
self.camera = self.robot.cameras["webcam"] if self.enable_camera else None
if self.camera is not None:
self.camera.connect()
print("================> SO100 Robot is fully connected =================")
def set_so100_robot_preset(self):
# Mode=0 for Position Control
self.motor_bus.write("Mode", 0)
# Set P_Coefficient to lower value to avoid shakiness (Default is 32)
# self.motor_bus.write("P_Coefficient", 16)
self.motor_bus.write("P_Coefficient", 10)
# Set I_Coefficient and D_Coefficient to default value 0 and 32
self.motor_bus.write("I_Coefficient", 0)
self.motor_bus.write("D_Coefficient", 32)
# Close the write lock so that Maximum_Acceleration gets written to EPROM address,
# which is mandatory for Maximum_Acceleration to take effect after rebooting.
self.motor_bus.write("Lock", 0)
# Set Maximum_Acceleration to 254 to speedup acceleration and deceleration of
# the motors. Note: this configuration is not in the official STS3215 Memory Table
self.motor_bus.write("Maximum_Acceleration", 254)
self.motor_bus.write("Acceleration", 254)
def move_to_initial_pose(self):
current_state = self.robot.capture_observation()["observation.state"]
# print("current_state", current_state)
# print all keys of the observation
# print("observation keys:", self.robot.capture_observation().keys())
# current_state = torch.tensor([90, 90, 90, 90, -70, 30])
current_state = torch.tensor([90, 90, 90, 90, -70, 30, 40])
self.robot.send_action(current_state)
time.sleep(2)
print("-------------------------------- moving to initial pose")
def go_home(self):
# [ 88.0664, 156.7090, 135.6152, 83.7598, -89.1211, 16.5107]
print("-------------------------------- moving to home pose")
home_state = torch.tensor([88.0664, 156.7090, 135.6152, 83.7598, -89.1211, 16.5107])
self.set_target_state(home_state)
time.sleep(2)
def get_observation(self):
return self.robot.capture_observation()
def get_current_state(self):
state = self.get_observation()["observation.state"].data.numpy()
state[6] = -state[6]
return state
def get_current_img(self):
img = self.get_observation()["observation.images.webcam"].data.numpy()
# convert bgr to rgb
img = cv2.cvtColor(img, cv2.COLOR_BGR2RGB)
return img
def set_target_state(self, target_state: torch.Tensor):
temp = self.robot.send_action(target_state)
print(f">>>>>>>>>>>>>>>>>>>>>>>>{temp}<<<<<<<<<<<<<<<<<<<<")
def enable(self):
self.motor_bus.write("Torque_Enable", TorqueMode.ENABLED.value)
def disable(self):
self.motor_bus.write("Torque_Enable", TorqueMode.DISABLED.value)
def disconnect(self):
self.disable()
self.robot.disconnect()
self.robot.is_connected = False
print("================> SO100 Robot disconnected")
def __del__(self):
self.disconnect()
#################################################################################
class Gr00tRobotInferenceClient:
def __init__(
self,
host="localhost",
port=5555,
language_instruction="Pick up the fruits and place them on the plate.",
):
self.language_instruction = language_instruction
# 480, 640
self.img_size = (480, 640)
self.policy = ExternalRobotInferenceClient(host=host, port=port)
def get_action(self, img, state):
obs_dict = {
"video.webcam": img[np.newaxis, :, :, :],
"state.single_arm": state[:6][np.newaxis, :].astype(np.float64),
"state.gripper": state[6:7][np.newaxis, :].astype(np.float64),
"annotation.human.task_description": [self.language_instruction],
}
res = self.policy.get_action(obs_dict)
# print("Inference query time taken", time.time() - start_time)
return res
def sample_action(self):
obs_dict = {
"video.webcam": np.zeros((1, self.img_size[0], self.img_size[1], 3), dtype=np.uint8),
"state.single_arm": np.zeros((1, 5)),
"state.gripper": np.zeros((1, 1)),
"annotation.human.action.task_description": [self.language_instruction],
}
return self.policy.get_action(obs_dict)
def set_lang_instruction(self, lang_instruction):
self.language_instruction = lang_instruction
#################################################################################
def view_img(img, img2=None):
"""
This is a matplotlib viewer since cv2.imshow can be flaky in lerobot env
also able to overlay the image to ensure camera view is alligned to training settings
"""
plt.imshow(img)
if img2 is not None:
plt.imshow(img2, alpha=0.5)
plt.axis("off")
plt.pause(0.001) # Non-blocking show
plt.clf() # Clear the figure for the next frame
#################################################################################
if __name__ == "__main__":
import argparse
default_dataset_path = os.path.expanduser("/home/seeed/Isaac-GR00T/demo_data/starai01")
parser = argparse.ArgumentParser()
parser.add_argument(
"--use_policy", action="store_true"
) # default is to playback the provided dataset
parser.add_argument("--dataset_path", type=str, default=default_dataset_path)
# parser.add_argument("--host", type=str, default="192.168.1.78")
parser.add_argument("--host", type=str, default="127.0.0.1")
parser.add_argument("--port", type=int, default=5555)
parser.add_argument("--action_horizon", type=int, default=16)
parser.add_argument("--actions_to_execute", type=int, default=350)
parser.add_argument("--cam_idx", type=int, default=8) # 8和6
parser.add_argument(
"--lang_instruction", type=str, default="Pick up the fruits and place them on the plate."
)
parser.add_argument("--record_imgs", action="store_true")
args = parser.parse_args()
# print lang_instruction
print("lang_instruction: ", args.lang_instruction)
ACTIONS_TO_EXECUTE = args.actions_to_execute
USE_POLICY = args.use_policy
ACTION_HORIZON = (
args.action_horizon
) # we will execute only some actions from the action_chunk of 16
MODALITY_KEYS = ["single_arm", "gripper"]
if USE_POLICY:
client = Gr00tRobotInferenceClient(
host=args.host,
port=args.port,
language_instruction=args.lang_instruction,
)
if args.record_imgs:
# create a folder to save the images and delete all the images in the folder
os.makedirs("eval_images", exist_ok=True)
for file in os.listdir("eval_images"):
os.remove(os.path.join("eval_images", file))
robot = SO100Robot(calibrate=False, enable_camera=True, cam_idx=args.cam_idx)
image_count = 0
with robot.activate():
for i in tqdm(range(ACTIONS_TO_EXECUTE), desc="Executing actions"):
img = robot.get_current_img()
view_img(img)
state = robot.get_current_state()
# new_image = np.zeros((880, 640, 3), dtype=np.uint8)
# new_image[:480, :, :] = img
# print(">>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>><<<<<<<<<<<<<<<<<<<<<<<<<<<<")
# print(type(state))
# print(state.shape)
# print(">>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>><<<<<<<<<<<<<<<<<<<<<<<<<<<<")
# -70 ~ -10
action = client.get_action(img, state)
action["action.gripper"] = action["action.gripper"] * -1
# set_gripper = np.ones_like(action["action.gripper"]) * -10
# action["action.gripper"] = set_gripper
# # action = client.get_action(img, state)
# print(">>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>><<<<<<<<<<<<<<<<<<<<<<<<<<<<")
# print(type(action))
# print(action)
# print(">>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>><<<<<<<<<<<<<<<<<<<<<<<<<<<<")
start_time = time.time()
for i in range(ACTION_HORIZON):
concat_action = np.concatenate(
[np.atleast_1d(action[f"action.{key}"][i]) for key in MODALITY_KEYS],
axis=0,
)
# assert concat_action.shape == (6,), concat_action.shape
assert concat_action.shape == (7,), concat_action.shape
robot.set_target_state(torch.from_numpy(concat_action))
time.sleep(0.02)
# get the realtime image
img = robot.get_current_img()
view_img(img)
if args.record_imgs:
# resize the image to 320x240
img = cv2.resize(cv2.cvtColor(img, cv2.COLOR_RGB2BGR), (320, 240))
cv2.imwrite(f"eval_images/img_{image_count}.jpg", img)
image_count += 1
# 0.05*16 = 0.8 seconds
print("executing action", i, "time taken", time.time() - start_time)
print("Action chunk execution time taken", time.time() - start_time)
else:
# Test Dataset Source https://huggingface.co/datasets/youliangtan/so100_strawberry_grape
dataset = LeRobotDataset(
repo_id="",
root=args.dataset_path,
)
robot = SO100Robot(calibrate=False, enable_camera=True, cam_idx=args.cam_idx)
with robot.activate():
print("Run replay of the dataset")
actions = []
for i in tqdm(range(ACTIONS_TO_EXECUTE), desc="Loading actions"):
action = dataset[i]["action"]
img = dataset[i]["observation.images.webcam"].data.numpy()
# original shape (3, 480, 640) for image data
realtime_img = robot.get_current_img()
img = img.transpose(1, 2, 0)
view_img(img, realtime_img)
actions.append(action)
robot.set_target_state(action)
time.sleep(0.05)
# plot the actions
plt.plot(actions)
plt.show()
print("Done all actions")
robot.go_home()
print("Done home")
Effect Demonstration
Our inference tests were conducted on a laptop equipped with an RTX 4080 GPU. While the inference accuracy proved excellent, we observed noticeable arm movement jitter due to the large VLA model size. Nevertheless, the system successfully accomplishes all intended tasks.
References
- https://wiki.seeedstudio.com/lerobot_so100m/
- https://github.com/NVIDIA/Isaac-GR00T/tree/main
- https://github.com/huggingface/lerobot
- https://github.com/Dao-AILab/flash-attention
- https://huggingface.co/blog/nvidia/gr00t-n1-5-so101-tuning
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.